<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX8M Mini Power Sequencing in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-Power-Sequencing/m-p/953702#M142519</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the data sheet for the iMX8M Mini this table is given for the power up sequence:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/83688i024F05FE345E4174/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Does this mean that if all the power rails are brought up simultaneously (as the minimum time for all rails to rail delays is 0ms) and then RTC_RESET_B is released some time later full and proper operation can be expected?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Likewise if all the rails are shutdown simultaneously will there be any adverse effects?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Sep 2019 10:37:15 GMT</pubDate>
    <dc:creator>omar_wolfe-huss</dc:creator>
    <dc:date>2019-09-06T10:37:15Z</dc:date>
    <item>
      <title>iMX8M Mini Power Sequencing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-Power-Sequencing/m-p/953702#M142519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the data sheet for the iMX8M Mini this table is given for the power up sequence:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/83688i024F05FE345E4174/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Does this mean that if all the power rails are brought up simultaneously (as the minimum time for all rails to rail delays is 0ms) and then RTC_RESET_B is released some time later full and proper operation can be expected?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Likewise if all the rails are shutdown simultaneously will there be any adverse effects?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Sep 2019 10:37:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-Power-Sequencing/m-p/953702#M142519</guid>
      <dc:creator>omar_wolfe-huss</dc:creator>
      <dc:date>2019-09-06T10:37:15Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M Mini Power Sequencing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-Power-Sequencing/m-p/953703#M142520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Note, timings T1, T2, T3 are based on NVCC_SNVS_1P8 start moment,&lt;BR /&gt;but T4 - T13 are based on PMIC_ON_REQ, because t1 is uncertain period.&lt;/P&gt;&lt;P&gt;In both groups all voltages can start their rising simultaneously in the groups.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;-------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Note:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Sep 2019 06:59:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Mini-Power-Sequencing/m-p/953703#M142520</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2019-09-09T06:59:02Z</dc:date>
    </item>
  </channel>
</rss>