<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How can I stop enabling the i.MX6Q watchdog? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-stop-enabling-the-i-MX6Q-watchdog/m-p/953441#M142491</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I understood there is no way to clear the Watchdog Enable (WDE) bit of the Watchdog Control Register (WCR) in software once it is set. &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;https://community.nxp.com/thread/444082&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;https://community.nxp.com/thread/450037&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I would like to keep WDE bit clear from the beginning to the end.&lt;/P&gt;&lt;P&gt;Fortunately ROM and uboot seems do nothing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any way to ignore&amp;nbsp;the watchdog during linux configuration?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is nice to switch with setenv kernel variable or dts binding description without rebuild images.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone help me?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Aug 2019 08:21:10 GMT</pubDate>
    <dc:creator>torus1000</dc:creator>
    <dc:date>2019-08-22T08:21:10Z</dc:date>
    <item>
      <title>How can I stop enabling the i.MX6Q watchdog?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-stop-enabling-the-i-MX6Q-watchdog/m-p/953441#M142491</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I understood there is no way to clear the Watchdog Enable (WDE) bit of the Watchdog Control Register (WCR) in software once it is set. &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;https://community.nxp.com/thread/444082&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;https://community.nxp.com/thread/450037&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I would like to keep WDE bit clear from the beginning to the end.&lt;/P&gt;&lt;P&gt;Fortunately ROM and uboot seems do nothing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any way to ignore&amp;nbsp;the watchdog during linux configuration?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is nice to switch with setenv kernel variable or dts binding description without rebuild images.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone help me?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Aug 2019 08:21:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-I-stop-enabling-the-i-MX6Q-watchdog/m-p/953441#M142491</guid>
      <dc:creator>torus1000</dc:creator>
      <dc:date>2019-08-22T08:21:10Z</dc:date>
    </item>
    <item>
      <title>Re: How can I stop enabling the i.MX6Q watchdog?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-stop-enabling-the-i-MX6Q-watchdog/m-p/953442#M142492</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi torus1000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Is there any way to ignore&amp;nbsp;the watchdog during linux configuration?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check sect.2.11.7 Menu Configuration Options attached Linux Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;It is nice to switch with setenv kernel variable or dts binding description without rebuild images.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in dts wdog can be configured with status = "okay"; or "disabled" :&lt;/P&gt;&lt;P&gt;linux/arch/arm/boot/dts/imx6qdl-sabresd.dtsi&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6qdl-sabresd.dtsi?h=imx_4.14.98_2.1.0" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6qdl-sabresd.dtsi?h=imx_4.14.98_2.1.0"&gt;imx6qdl-sabresd.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Aug 2019 09:44:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-I-stop-enabling-the-i-MX6Q-watchdog/m-p/953442#M142492</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-08-22T09:44:03Z</dc:date>
    </item>
  </channel>
</rss>