<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 map network drive</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/map-network-drive/m-p/219154#M14242</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello everyone,&lt;/P&gt;&lt;P&gt;i have an issue while trying to map a network drive using the qsb.&lt;/P&gt;&lt;P&gt;my configuration is:&lt;/P&gt;&lt;P&gt;i compiled uboot,kernel and fs using ltib and installed samba (checked the start smbd nmbd).&lt;/P&gt;&lt;P&gt;i created a smb.conf file in /usr/lib as i understood from some manual.&lt;/P&gt;&lt;P&gt;the qsb is connecting to a laptop with eth.&lt;/P&gt;&lt;P&gt;everything is working well untill now.&lt;/P&gt;&lt;P&gt;i succeded to&amp;nbsp;map a sata drive connected to the qsb in the connected pc running win7 and accessed the files.&lt;/P&gt;&lt;P&gt;now i'm trien to do the oposite action. i'm trying to share a folder from windows and access it from the qsb.&lt;/P&gt;&lt;P&gt;i've tried using the command: mount -t cifs //x.x.x.x/sharename but i'm keep getting error says: "mount: mounting //x.x.x.x/Maps on /mnt/win failed: No such device"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;* the x.x.x.x is the windows machine ip number that i change here to x.x.x.x.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i also tried running that command on the linux host pc that i have ltib on but that finished succesfully, so something is wrong with the configuration on the qsb...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;did anyone had this problem or have an idea?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;snir.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Mar 2012 17:04:19 GMT</pubDate>
    <dc:creator>snirnisim</dc:creator>
    <dc:date>2012-03-15T17:04:19Z</dc:date>
    <item>
      <title>map network drive</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/map-network-drive/m-p/219154#M14242</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello everyone,&lt;/P&gt;&lt;P&gt;i have an issue while trying to map a network drive using the qsb.&lt;/P&gt;&lt;P&gt;my configuration is:&lt;/P&gt;&lt;P&gt;i compiled uboot,kernel and fs using ltib and installed samba (checked the start smbd nmbd).&lt;/P&gt;&lt;P&gt;i created a smb.conf file in /usr/lib as i understood from some manual.&lt;/P&gt;&lt;P&gt;the qsb is connecting to a laptop with eth.&lt;/P&gt;&lt;P&gt;everything is working well untill now.&lt;/P&gt;&lt;P&gt;i succeded to&amp;nbsp;map a sata drive connected to the qsb in the connected pc running win7 and accessed the files.&lt;/P&gt;&lt;P&gt;now i'm trien to do the oposite action. i'm trying to share a folder from windows and access it from the qsb.&lt;/P&gt;&lt;P&gt;i've tried using the command: mount -t cifs //x.x.x.x/sharename but i'm keep getting error says: "mount: mounting //x.x.x.x/Maps on /mnt/win failed: No such device"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;* the x.x.x.x is the windows machine ip number that i change here to x.x.x.x.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i also tried running that command on the linux host pc that i have ltib on but that finished succesfully, so something is wrong with the configuration on the qsb...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;did anyone had this problem or have an idea?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;snir.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Mar 2012 17:04:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/map-network-drive/m-p/219154#M14242</guid>
      <dc:creator>snirnisim</dc:creator>
      <dc:date>2012-03-15T17:04:19Z</dc:date>
    </item>
    <item>
      <title>Re: map network drive</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/map-network-drive/m-p/219155#M14243</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i tried running smbclient -L x.x.x.x and got all shares, i can see the folder i'm triend to mount but i also get this lines in the end:&lt;/P&gt;&lt;P&gt;session request to&amp;nbsp;x.x.x.x failed (Called name not present)&lt;/P&gt;&lt;P&gt;&amp;nbsp;session request to 10 failed (Called name not present)&lt;/P&gt;&lt;P&gt;session request to *SMBSERVER failed (Called name not present)&lt;/P&gt;&lt;P&gt;NetBIOS over TCP disabled -- no workgroup available&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(again the x.x.x.x is the ipnuber that i changed to that after pasting here)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;hope that will help someone to point the problem for me.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;htanks,&lt;/P&gt;&lt;P&gt;snir&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Mar 2012 17:22:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/map-network-drive/m-p/219155#M14243</guid>
      <dc:creator>snirnisim</dc:creator>
      <dc:date>2012-03-15T17:22:05Z</dc:date>
    </item>
    <item>
      <title>Re: map network drive</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/map-network-drive/m-p/219156#M14244</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;well problem solved... just forgot to check network filesystems in kernel build... for cifs and smbfs...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Mar 2012 14:15:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/map-network-drive/m-p/219156#M14244</guid>
      <dc:creator>snirnisim</dc:creator>
      <dc:date>2012-03-16T14:15:01Z</dc:date>
    </item>
  </channel>
</rss>