<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx6 camera input resolution?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6-camera-input-resolution/m-p/952673#M142395</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Camera sensors&lt;BR /&gt;• Up to three interfaces may be active at once&lt;BR /&gt;• Two parallel camera ports (up to 20-bit, up to 240MHz peak1 each).&lt;BR /&gt;• MIPI CSI-2 / Parallel port, supporting from 80 Mbps up to 1 Gbps speed per data&lt;BR /&gt;lane. The CSI-2 Receiver core can manage one clock lane and up to 4 data lanes.&lt;BR /&gt;There are 4 lanes in i.MX 6Dual/6Quad.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 Aug 2019 07:04:21 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2019-08-05T07:04:21Z</dc:date>
    <item>
      <title>imx6 camera input resolution?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-camera-input-resolution/m-p/952672#M142394</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;I am using the camera in IMX6Q.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;The camera resolution setting is used as follows.&lt;/P&gt;&lt;P&gt;1. 1920x1080@30&lt;/P&gt;&lt;P&gt;2. 1440x1080@30&lt;/P&gt;&lt;P&gt;3. &lt;A href="mailto:752x582@30"&gt;752x582@30&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;Resolution 1 and 2 work well from camera input to output. But 3 is output as if there is no input from the gstreamer.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;SPAN lang="en"&gt;Is there a range of resolutions for which IMX6Q can be input?&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV&gt;&lt;DIV class=""&gt;&lt;DIV&gt;&lt;DIV class=""&gt;&lt;DIV&gt;&lt;DIV data-ved="0ahUKEwiM0ZfY7sfjAhVa7mEKHRtMA6QQGggr"&gt;&lt;DIV data-async-context="query:%EB%B2%88%EC%97%AD"&gt;&lt;DIV class=""&gt;&lt;DIV class="" data-hveid="CAoQAA" data-md="77" data-ved="2ahUKEwiM0ZfY7sfjAhVa7mEKHRtMA6QQkCkwAHoECAoQAA"&gt;&lt;DIV data-hveid="CAoQAQ"&gt;&lt;DIV class="" data-cp="1" data-nnttsvi="1" data-nttsd="1" data-sm="1" data-sugg-time="500" data-sugg-url="https://clients1.google.com/complete/search" data-uilc="ko" data-ulf="1"&gt;&lt;DIV class=""&gt;&lt;DIV class="" data-rtid="iwl1GuJqdOBw"&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV&gt;&lt;DIV class=""&gt;&lt;DIV&gt;&lt;DIV class=""&gt;&lt;DIV&gt;&lt;DIV data-ved="0ahUKEwiM0ZfY7sfjAhVa7mEKHRtMA6QQGggr"&gt;&lt;DIV data-async-context="query:%EB%B2%88%EC%97%AD"&gt;&lt;DIV class=""&gt;&lt;DIV class="" data-hveid="CAoQAA" data-md="77" data-ved="2ahUKEwiM0ZfY7sfjAhVa7mEKHRtMA6QQkCkwAHoECAoQAA"&gt;&lt;DIV data-hveid="CAoQAQ"&gt;&lt;DIV class="" data-cp="1" data-nnttsvi="1" data-nttsd="1" data-sm="1" data-sugg-time="500" data-sugg-url="https://clients1.google.com/complete/search" data-uilc="ko" data-ulf="1"&gt;&lt;DIV class=""&gt;&lt;DIV class="" data-rtid="iwl1GuJqdOBw"&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;I thought I only needed to set act_sens_conf and sens_frm_size.&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV&gt;&lt;DIV class=""&gt;&lt;DIV&gt;&lt;DIV class=""&gt;&lt;DIV&gt;&lt;DIV data-ved="0ahUKEwiM0ZfY7sfjAhVa7mEKHRtMA6QQGggr"&gt;&lt;DIV data-async-context="query:%EB%B2%88%EC%97%AD"&gt;&lt;DIV class=""&gt;&lt;DIV class="" data-hveid="CAoQAA" data-md="77" data-ved="2ahUKEwiM0ZfY7sfjAhVa7mEKHRtMA6QQkCkwAHoECAoQAA"&gt;&lt;DIV data-hveid="CAoQAQ"&gt;&lt;DIV class="" data-cp="1" data-nnttsvi="1" data-nttsd="1" data-sm="1" data-sugg-time="500" data-sugg-url="https://clients1.google.com/complete/search" data-uilc="ko" data-ulf="1"&gt;&lt;DIV class=""&gt;&lt;DIV class="" data-rtid="iwl1GuJqdOBw"&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jul 2019 06:18:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-camera-input-resolution/m-p/952672#M142394</guid>
      <dc:creator>kangmw086</dc:creator>
      <dc:date>2019-07-22T06:18:10Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 camera input resolution?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-camera-input-resolution/m-p/952673#M142395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Camera sensors&lt;BR /&gt;• Up to three interfaces may be active at once&lt;BR /&gt;• Two parallel camera ports (up to 20-bit, up to 240MHz peak1 each).&lt;BR /&gt;• MIPI CSI-2 / Parallel port, supporting from 80 Mbps up to 1 Gbps speed per data&lt;BR /&gt;lane. The CSI-2 Receiver core can manage one clock lane and up to 4 data lanes.&lt;BR /&gt;There are 4 lanes in i.MX 6Dual/6Quad.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Aug 2019 07:04:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-camera-input-resolution/m-p/952673#M142395</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2019-08-05T07:04:21Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 camera input resolution?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-camera-input-resolution/m-p/952674#M142396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;Thank you for answer. But that's not the answer I want.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;SPAN lang="en"&gt;I proceeded to test each one.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;SPAN lang="en"&gt;However, I set the resolution for 752x582, but the gstreamer is not running. I want to know why.&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV&gt;&lt;DIV class=""&gt;&lt;DIV&gt;&lt;DIV class=""&gt;&lt;DIV&gt;&lt;DIV data-ved="0ahUKEwiY4fHnuevjAhUoyYsBHYQ5DDgQGggr"&gt;&lt;DIV data-async-context="query:%EB%B2%88%EC%97%AD"&gt;&lt;DIV class=""&gt;&lt;DIV class="" data-hveid="CAoQAA" data-md="77" data-ved="2ahUKEwiY4fHnuevjAhUoyYsBHYQ5DDgQkCkwAHoECAoQAA"&gt;&lt;DIV data-hveid="CAoQAQ"&gt;&lt;DIV class="" data-cp="1" data-nnttsvi="1" data-nttsd="1" data-sm="1" data-sugg-time="500" data-sugg-url="https://clients1.google.com/complete/search" data-uilc="ko" data-ulf="1"&gt;&lt;DIV class=""&gt;&lt;DIV class="" data-rtid="iZl1uJkRsdvA"&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Aug 2019 09:51:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-camera-input-resolution/m-p/952674#M142396</guid>
      <dc:creator>kangmw086</dc:creator>
      <dc:date>2019-08-05T09:51:09Z</dc:date>
    </item>
  </channel>
</rss>