<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Boot linux-imx 4.9.88 on phyflex-imx6-4 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Boot-linux-imx-4-9-88-on-phyflex-imx6-4/m-p/951713#M142273</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to boot the linux-imx kernel (for sabreauto for example) from freescale on the phyflex-imx6-4 board along with imx6q-phyflex-pbab01.dts devicetree.&lt;/P&gt;&lt;P&gt;Do you know if this is possible/easy ? Because this is not as straight forward as changing the device tree the kernel is using to boot.&lt;/P&gt;&lt;P&gt;I don't know in details the diffrence between linux-imx and linux-mainline ? Is there any documentation about it ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is because I want to use vpu encoders etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Quentin.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Jun 2019 09:09:49 GMT</pubDate>
    <dc:creator>quenreyn</dc:creator>
    <dc:date>2019-06-20T09:09:49Z</dc:date>
    <item>
      <title>Boot linux-imx 4.9.88 on phyflex-imx6-4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-linux-imx-4-9-88-on-phyflex-imx6-4/m-p/951713#M142273</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to boot the linux-imx kernel (for sabreauto for example) from freescale on the phyflex-imx6-4 board along with imx6q-phyflex-pbab01.dts devicetree.&lt;/P&gt;&lt;P&gt;Do you know if this is possible/easy ? Because this is not as straight forward as changing the device tree the kernel is using to boot.&lt;/P&gt;&lt;P&gt;I don't know in details the diffrence between linux-imx and linux-mainline ? Is there any documentation about it ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is because I want to use vpu encoders etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Quentin.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jun 2019 09:09:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-linux-imx-4-9-88-on-phyflex-imx6-4/m-p/951713#M142273</guid>
      <dc:creator>quenreyn</dc:creator>
      <dc:date>2019-06-20T09:09:49Z</dc:date>
    </item>
    <item>
      <title>Re: Boot linux-imx 4.9.88 on phyflex-imx6-4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-linux-imx-4-9-88-on-phyflex-imx6-4/m-p/951714#M142274</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Quentin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for phyflex-imx6-4 board software one can look at its vendor support portal&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://wiki.phytec.com/display/public/PRODUCTINFO/phyFLEX-i.MX+6#Landing-1383974343" title="https://wiki.phytec.com/display/public/PRODUCTINFO/phyFLEX-i.MX+6#Landing-1383974343"&gt;phyFLEX-i.MX 6 - Develop.phytec - PHYTEC Wiki&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As this is different board than NXP reference boards (SD, SabreAI)&lt;/P&gt;&lt;P&gt;seems it will not be easy to run NXP software on that board.&lt;/P&gt;&lt;P&gt;One can look on NXP Linux&amp;nbsp; Documentation, Porting Guide to get additional help:&lt;BR /&gt;&lt;A href="https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6series-i.mx-7series-software-and-development-tool-resources:IMX_SW" target="test_blank"&gt;https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6series-i.mx-7series-software-and-development-tool-resources:IMX_SW&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jun 2019 10:29:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-linux-imx-4-9-88-on-phyflex-imx6-4/m-p/951714#M142274</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-06-20T10:29:36Z</dc:date>
    </item>
    <item>
      <title>Re: Boot linux-imx 4.9.88 on phyflex-imx6-4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-linux-imx-4-9-88-on-phyflex-imx6-4/m-p/951715#M142275</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I come back to you if I found anything,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Quentin.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jun 2019 13:52:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-linux-imx-4-9-88-on-phyflex-imx6-4/m-p/951715#M142275</guid>
      <dc:creator>quenreyn</dc:creator>
      <dc:date>2019-06-20T13:52:54Z</dc:date>
    </item>
  </channel>
</rss>