<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 8M Mini 24MHz crystal load capacitance in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/8M-Mini-24MHz-crystal-load-capacitance/m-p/951210#M142217</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi adevries&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;I believe I can pick a crystal with any load capacitance value as long as its maximum drive level isn't exceeded&lt;/P&gt;&lt;P&gt;&amp;gt;and I choose the appropriate capacitors to accompany it. Would&amp;nbsp; agree with that statement?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;power calculator was designed to be used with the i.MX 6 series. Will it calculate an accurate&lt;/P&gt;&lt;P&gt;&amp;gt;drive level for the 8M Mini as well?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Sep 2019 00:17:08 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-09-12T00:17:08Z</dc:date>
    <item>
      <title>8M Mini 24MHz crystal load capacitance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8M-Mini-24MHz-crystal-load-capacitance/m-p/951205#M142212</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to choose a 24MHz crystal to use with the 8M Mini, but I am having difficultly determining which crystals would be acceptable to use. While the datasheet recommends a crystal with a typical Cload of 12pF, the eval kit uses a crystal with a Cload of 9pF. If I am interested in using a crystal with a Cload that isn't 12pF, how can I go about determining if it will work with the 8M Mini?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Additionally, when adding load capacitance, it's important to match the load capacitance listed on the crystal datasheet, correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/82801iBF46AC09F621DB62/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So, if the crystal CL&amp;nbsp;= 9pF, then I would pick C1 and C2 such that this equation:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/82756iB2539BE88BB3518D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&amp;nbsp;is satisfied, right? In this case, Cs is stray capacitance, Ci is the input capacitance, and Co is the output capacitance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If so, does anyone know what the&amp;nbsp;pin&amp;nbsp;capacitance is for pins 24M_XTALI and 24M_XTALO?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Sep 2019 22:46:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8M-Mini-24MHz-crystal-load-capacitance/m-p/951205#M142212</guid>
      <dc:creator>adevries</dc:creator>
      <dc:date>2019-09-04T22:46:06Z</dc:date>
    </item>
    <item>
      <title>Re: 8M Mini 24MHz crystal load capacitance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8M-Mini-24MHz-crystal-load-capacitance/m-p/951206#M142213</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &amp;nbsp;adevries&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;right, datasheet recommends Cload of 12pF as&amp;nbsp; typical, however other also&lt;BR /&gt;can be used. Examples of CL calculation can be found on&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://forum.digikey.com/t/crystal-oscillator-load-cap-selection/1915" title="https://forum.digikey.com/t/crystal-oscillator-load-cap-selection/1915"&gt;Crystal Oscillator Load Cap Selection - Tech Tips - Engineering and Component Solution Forum - TechForum │ Digi-Key&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://notes-application.abcelectronique.com/179/179-48215.pdf" title="http://notes-application.abcelectronique.com/179/179-48215.pdf"&gt;http://notes-application.abcelectronique.com/179/179-48215.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;crystal drive level calculator in EB830&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/engineering-bulletin/EB830.pdf" title="https://www.nxp.com/docs/en/engineering-bulletin/EB830.pdf"&gt;https://www.nxp.com/docs/en/engineering-bulletin/EB830.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Pin&amp;nbsp;capacitance can be found in ibis model.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Sep 2019 13:57:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8M-Mini-24MHz-crystal-load-capacitance/m-p/951206#M142213</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-09-07T13:57:35Z</dc:date>
    </item>
    <item>
      <title>Re: 8M Mini 24MHz crystal load capacitance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8M-Mini-24MHz-crystal-load-capacitance/m-p/951207#M142214</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the information. I understand how to calculate what capacitor to connect to the crystal, but I don't understand how to choose the proper Cload value for a crystal.&lt;/P&gt;&lt;P&gt;Table 19 in the 8M Mini datasheet recommends a typical Cload of 12pF, so obviously crystals that meet the other requirements and have a Cload of 12pF should work. The eval board uses a crystal with a Cload of 9pF, so that would imply crystals with a Cload of 9pF should work. But how large or small can the crystal Cload be before it will not work anymore? Can my crystal have a Cload of 100pF? or 1000pF? Why or why not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there really no minimum or maximum value for the crystal's Cload?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/66692iDE304E7E4F619BE1/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P.S. Due to a security update in Adobe Acrobat Reader, macro-enabled excel sheets embedded in PDF's cannot be opened anymore. So I cannot access the&amp;nbsp;crystal drive level calculator in EB830&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Sep 2019 19:15:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8M-Mini-24MHz-crystal-load-capacitance/m-p/951207#M142214</guid>
      <dc:creator>adevries</dc:creator>
      <dc:date>2019-09-10T19:15:16Z</dc:date>
    </item>
    <item>
      <title>Re: 8M Mini 24MHz crystal load capacitance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8M-Mini-24MHz-crystal-load-capacitance/m-p/951208#M142215</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi adevries&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;But how large or small can the crystal Cload be before it will not work anymore?&lt;/P&gt;&lt;P&gt;&amp;gt;Can my crystal have a Cload of 100pF? or 1000pF? Why or why not?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;to answer this question one needs to read how works Pierce oscillator - this is described&lt;/P&gt;&lt;P&gt;in common physics documentation, like &lt;A class="link-titled" href="https://www.electronics-tutorials.ws/oscillator/crystal.html" title="https://www.electronics-tutorials.ws/oscillator/crystal.html"&gt;https://www.electronics-tutorials.ws/oscillator/crystal.html&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;ftp://download.epson-europe.com/pub/electronics-de/quartz/applnotes/oscillation%20circuit%20design%20guide.pdf&lt;/P&gt;&lt;P&gt;and educational books for electronics.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Sep 2019 00:48:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8M-Mini-24MHz-crystal-load-capacitance/m-p/951208#M142215</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-09-11T00:48:51Z</dc:date>
    </item>
    <item>
      <title>Re: 8M Mini 24MHz crystal load capacitance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8M-Mini-24MHz-crystal-load-capacitance/m-p/951209#M142216</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for linking to those resources. I read the documents you linked and did some additional research, and this is the conclusion I've reached:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to this document by silabs (&lt;A href="https://www.silabs.com/documents/public/application-notes/an0016.0-efm32-series-0-oscillator-design-considerations.pdf"&gt;Link&lt;/A&gt;), "Crystals with small load capacitance would typically start faster than crystals requiring a large CL. Large load capacitors also increase power consumption". This statement is supported by the power calculator you provided.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can calculate the drive level of the crystal using the formula from Chrontel application note AN-06:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86777i0B38DBA05B69B9F9/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_9.png" alt="pastedImage_9.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But what is the voltage level that drives the crystal? Is it a 1.8V square wave at 50% duty cycle? Or something else?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, I believe I can pick a crystal with any load capacitance value as long as its maximum drive level isn't exceeded and I choose the appropriate capacitors to accompany it. Would&amp;nbsp; agree with that statement?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, the power calculator was designed to be used with the i.MX 6 series. Will it calculate an accurate drive level for the 8M Mini as well?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;adevries&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Sep 2019 18:07:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8M-Mini-24MHz-crystal-load-capacitance/m-p/951209#M142216</guid>
      <dc:creator>adevries</dc:creator>
      <dc:date>2019-09-11T18:07:39Z</dc:date>
    </item>
    <item>
      <title>Re: 8M Mini 24MHz crystal load capacitance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8M-Mini-24MHz-crystal-load-capacitance/m-p/951210#M142217</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi adevries&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;I believe I can pick a crystal with any load capacitance value as long as its maximum drive level isn't exceeded&lt;/P&gt;&lt;P&gt;&amp;gt;and I choose the appropriate capacitors to accompany it. Would&amp;nbsp; agree with that statement?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;power calculator was designed to be used with the i.MX 6 series. Will it calculate an accurate&lt;/P&gt;&lt;P&gt;&amp;gt;drive level for the 8M Mini as well?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Sep 2019 00:17:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8M-Mini-24MHz-crystal-load-capacitance/m-p/951210#M142217</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-09-12T00:17:08Z</dc:date>
    </item>
  </channel>
</rss>