<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX28 MfgTools 3.0 + Windows CE 6.0</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-MfgTools-3-0-Windows-CE-6-0/m-p/950399#M142112</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steve&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to develop own uuu script using sect.6 Migration from mfgtool ucl2.xml&lt;/P&gt;&lt;P&gt;in uuu.pdf manual :&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/NXPmicro/mfgtools/releases/download/uuu_1.2.0/UUU.pdf" title="https://github.com/NXPmicro/mfgtools/releases/download/uuu_1.2.0/UUU.pdf"&gt;https://github.com/NXPmicro/mfgtools/releases/download/uuu_1.2.0/UUU.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 Aug 2019 23:26:06 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-08-05T23:26:06Z</dc:date>
    <item>
      <title>i.MX28 MfgTools 3.0 + Windows CE 6.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-MfgTools-3-0-Windows-CE-6-0/m-p/950398#M142111</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a custom board with an i.MX28 processor. Would it be possible to write a Windows CE 6.0 image to the on-board NAND flash with&amp;nbsp;&lt;A href="https://github.com/NXPmicro/mfgtools" rel="nofollow noopener noreferrer" target="_blank"&gt;MfgTool 3.0&lt;/A&gt;. I have three files: uce_ivt.sb,&amp;nbsp;&lt;EM&gt;eboot_ivt.sb&lt;/EM&gt; and &lt;EM&gt;NK.nb0.&amp;nbsp;&lt;/EM&gt;I use ubuntu 18.04.2 LTS 64-bit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can boot the update client engine with command:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;./uuu uce_ivt.sb&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;, then I use this command to program the NAND flash, but it fails:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;./uuu -b NAND eboot_ivt.sb NK.nb0‍

Wait for Known USB Device Appear...
Error: Unknown Command:FB: nandbcd update $(fastboot_buffer) nandboot $(fastboot_bytes)&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the older version MfgTool V1 (on Windows) I have no problems.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Aug 2019 12:29:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-MfgTools-3-0-Windows-CE-6-0/m-p/950398#M142111</guid>
      <dc:creator>steve_vandenbus</dc:creator>
      <dc:date>2019-08-05T12:29:49Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX28 MfgTools 3.0 + Windows CE 6.0</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-MfgTools-3-0-Windows-CE-6-0/m-p/950399#M142112</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steve&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try to develop own uuu script using sect.6 Migration from mfgtool ucl2.xml&lt;/P&gt;&lt;P&gt;in uuu.pdf manual :&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/NXPmicro/mfgtools/releases/download/uuu_1.2.0/UUU.pdf" title="https://github.com/NXPmicro/mfgtools/releases/download/uuu_1.2.0/UUU.pdf"&gt;https://github.com/NXPmicro/mfgtools/releases/download/uuu_1.2.0/UUU.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Aug 2019 23:26:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-MfgTools-3-0-Windows-CE-6-0/m-p/950399#M142112</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-08-05T23:26:06Z</dc:date>
    </item>
  </channel>
</rss>