<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Network manager systemd in imx6ULL</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Network-manager-systemd-in-imx6ULL/m-p/950125#M142068</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Vasu,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You do not mention which board you are using. I would recommend making sure that the board has a MAC address so that an IP can be assigned. Would you please make sure that the MAC addressed is set? You can see this variable in uboot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Sep 2019 21:38:23 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2019-09-09T21:38:23Z</dc:date>
    <item>
      <title>Network manager systemd in imx6ULL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Network-manager-systemd-in-imx6ULL/m-p/950124#M142067</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Processor = imx6ull,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Yacto = L4.14.98-2.0.0_ga&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; We used default init manager systemd.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; u-boot set as emmc.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; After that bitbake-core-image-minimal.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; But systemd network manager not working ethernet also not detecting&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; lo&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Link encap:Local Loopback&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; inet addr:127.0.0.1&amp;nbsp; Mask:255.0.0.0 &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; inet6 addr: ::1%1996089040/128 Scope:Host &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; UP LOOPBACK RUNNING&amp;nbsp; MTU:65536&amp;nbsp; Metric:1 &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RX packets:320 errors:0 dropped:0 overruns:0 frame:0 &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; TX packets:320 errors:0 dropped:0 overruns:0 carrier:0 &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; collisions:0 txqueuelen:0 &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RX bytes:24320 (23.7 KiB)&amp;nbsp; TX bytes:24320 (23.7 KiB)&lt;/P&gt;&lt;P&gt;If i type manually&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&amp;nbsp;ifconfig eth1 up&lt;SPAN style="color: #1f4e79; font-family: Arial, sans-serif; "&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;udhcpc -i eth1 &amp;nbsp;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Now ethernet and dhcp working fine next poweroff again manually i need to type.&lt;/P&gt;&lt;P&gt;How to avoid error systemd network manager&amp;nbsp; (or) i need to use some other network manager ?&lt;/P&gt;&lt;P&gt;Please help me solve this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Vasu &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Sep 2019 06:08:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Network-manager-systemd-in-imx6ULL/m-p/950124#M142067</guid>
      <dc:creator>vasudhevan</dc:creator>
      <dc:date>2019-09-05T06:08:33Z</dc:date>
    </item>
    <item>
      <title>Re: Network manager systemd in imx6ULL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Network-manager-systemd-in-imx6ULL/m-p/950125#M142068</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Vasu,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You do not mention which board you are using. I would recommend making sure that the board has a MAC address so that an IP can be assigned. Would you please make sure that the MAC addressed is set? You can see this variable in uboot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Sep 2019 21:38:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Network-manager-systemd-in-imx6ULL/m-p/950125#M142068</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2019-09-09T21:38:23Z</dc:date>
    </item>
    <item>
      <title>Re: Network manager systemd in imx6ULL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Network-manager-systemd-in-imx6ULL/m-p/950126#M142069</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi gusarambula,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thank you for your reply,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; This issue resolved for me.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I followed this link &lt;A class="link-titled" href="https://developer.toradex.com/knowledge-base/ethernet-network-(linux)" title="https://developer.toradex.com/knowledge-base/ethernet-network-(linux)"&gt;Ethernet/Network (Linux)&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;Vasu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Sep 2019 03:31:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Network-manager-systemd-in-imx6ULL/m-p/950126#M142069</guid>
      <dc:creator>vasudhevan</dc:creator>
      <dc:date>2019-09-10T03:31:29Z</dc:date>
    </item>
  </channel>
</rss>