<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Qt OpenGL is too slow</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Qt-OpenGL-is-too-slow/m-p/949668#M142025</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi aither&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;according to sect.2.1 New features attached Release Notes:&lt;/P&gt;&lt;P&gt;"Qt 5 is not supported for SoCs without hardware graphics.&lt;/P&gt;&lt;P&gt;Qt 5 video is not supported on SoCs without a VPU."&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Aug 2019 23:14:21 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-08-21T23:14:21Z</dc:date>
    <item>
      <title>Qt OpenGL is too slow</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Qt-OpenGL-is-too-slow/m-p/949667#M142024</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, NXP and everyone&lt;/P&gt;&lt;P&gt;For IMX6ULL, I'm using fsl-imx-wayland(4.1.15-2.0.1).&lt;/P&gt;&lt;P&gt;I tested Qt example "Cube", in mainwidget.cpp, MainWidget::paintGL() function running of&amp;nbsp; consume 350ms, and MainWidget::timerEvent() interval was set with 12ms but actually is 4500ms (when MainWidget::paintGL() is empty, it is 11~14ms). So, the scene is drawn with 4.5s interval, too slow.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help me to solve this problem.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Thanks, aither&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Aug 2019 07:45:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Qt-OpenGL-is-too-slow/m-p/949667#M142024</guid>
      <dc:creator>3273977271</dc:creator>
      <dc:date>2019-08-21T07:45:56Z</dc:date>
    </item>
    <item>
      <title>Re: Qt OpenGL is too slow</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Qt-OpenGL-is-too-slow/m-p/949668#M142025</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi aither&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;according to sect.2.1 New features attached Release Notes:&lt;/P&gt;&lt;P&gt;"Qt 5 is not supported for SoCs without hardware graphics.&lt;/P&gt;&lt;P&gt;Qt 5 video is not supported on SoCs without a VPU."&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Aug 2019 23:14:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Qt-OpenGL-is-too-slow/m-p/949668#M142025</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-08-21T23:14:21Z</dc:date>
    </item>
  </channel>
</rss>