<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Rebuild kernel and not booting</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Rebuild-kernel-and-not-booting/m-p/948522#M141874</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi emmanuel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Your kernel is wrong, with the changes you are doing, try to make one by one to localize the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Sep 2019 14:29:39 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2019-09-05T14:29:39Z</dc:date>
    <item>
      <title>Rebuild kernel and not booting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Rebuild-kernel-and-not-booting/m-p/948520#M141872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working with an imx6 digi board. I builded a system with yocto 2.4 and 4.9 version kernel.&lt;/P&gt;&lt;P&gt;When I build al the system, with:&lt;/P&gt;&lt;P&gt;=&amp;gt; bitbake dey-image-qt&lt;/P&gt;&lt;P&gt;Kernel and dtb files are&amp;nbsp;&lt;SPAN style="color: rgba(0, 0, 0, 0.8); background-color: #ffffff;"&gt;packaged together in a single fil with .boot.vfat extension, and the root file system is packaged in rootfs.ext4 extension file. This worked and the system boot well, but I needed to make some changes in kernel, precisely change kernel logo, so I made the chenge and rebuild only the kernel.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: rgba(0, 0, 0, 0.8); background-color: #ffffff;"&gt;First to try if the chages works fine I mounted vfat an rootfs to boot from tftp, and replace .bin file. At fisrt the system botting well, the logo kernel is chenged, all ok, but when I&amp;nbsp; remounted vfat the system dont boot again, there is some error with kernel file (.bin).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: rgba(0, 0, 0, 0.8); background-color: #ffffff;"&gt;I need help with this.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Sep 2019 17:23:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Rebuild-kernel-and-not-booting/m-p/948520#M141872</guid>
      <dc:creator>emmanuelperea</dc:creator>
      <dc:date>2019-09-04T17:23:32Z</dc:date>
    </item>
    <item>
      <title>Re: Rebuild kernel and not booting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Rebuild-kernel-and-not-booting/m-p/948521#M141873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;&lt;SPAN style="font-size: 22px;"&gt;when the system bootin well this are the message&lt;/SPAN&gt;:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot dub-2015.04-r12.1+g5ea79be (Jun 27 2018 - 04:09:53)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6DL rev1.3 at 792MHz&lt;BR /&gt;CPU: Industrial temperature grade (-40C to 105C) at 42C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 512 MiB&lt;BR /&gt;MMC: FSL_SDHC: 0 (eMMC), FSL_SDHC: 1&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;ConnectCore 6 SOM variant 0x0C: Industrial DualLite-core 800MHz, 4GB eMMC, 512MB DDR3, -40/+85C&lt;BR /&gt;Board: ConnectCore 6 SBC&lt;BR /&gt; WARNING: Undefined board version!&lt;BR /&gt; WARNING: Undefined board ID!&lt;BR /&gt;Boot device: MMC4&lt;BR /&gt;PMIC: DA9063, Device: 0x61, Variant: 0x60, Customer: 0x00, Config: 0x56&lt;BR /&gt;Net: FEC [PRIME]&lt;BR /&gt;Hit any key to stop autoboot: 0 &lt;BR /&gt;=&amp;gt; dboot linux tftp&lt;BR /&gt;Using FEC device&lt;BR /&gt;TFTP from server 192.168.11.148; our IP address is 192.168.11.154&lt;BR /&gt;Filename 'zImage-ccimx6sbc.bin'.&lt;BR /&gt;Load address: 0x12000000&lt;BR /&gt;Loading: #################################################################&lt;BR /&gt; #################################################################&lt;BR /&gt; #################################################################&lt;BR /&gt; #################################################################&lt;BR /&gt; #################################################################&lt;BR /&gt; ###########################################################&lt;BR /&gt; 3.6 MiB/s&lt;BR /&gt;done&lt;BR /&gt;Bytes transferred = 5628240 (55e150 hex)&lt;BR /&gt;Using FEC device&lt;BR /&gt;TFTP from server 192.168.11.148; our IP address is 192.168.11.154&lt;BR /&gt;Filename 'zImage-imx6dl-ccimx6sbc.dtb'.&lt;BR /&gt;Load address: 0x18000000&lt;BR /&gt;Loading: ####&lt;BR /&gt; 979.5 KiB/s&lt;BR /&gt;done&lt;BR /&gt;Bytes transferred = 50162 (c3f2 hex)&lt;BR /&gt;Kernel image @ 0x12000000 [ 0x000000 - 0x55e150 ]&lt;BR /&gt;## Flattened Device Tree blob at 18000000&lt;BR /&gt; Booting using the fdt blob at 0x18000000&lt;BR /&gt; Using Device Tree in place at 18000000, end 1800f3f1&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 22px;"&gt;&lt;STRONG&gt;But when the system not booting this is the message:&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using FEC device&lt;BR /&gt;TFTP from server 192.168.11.148; our IP address is 192.168.11.154&lt;BR /&gt;Filename 'zImage-ccimx6sbc.bin'.&lt;BR /&gt;Load address: 0x12000000&lt;BR /&gt;Loading: ###############################&lt;BR /&gt; 681.6 KiB/s&lt;BR /&gt;done&lt;BR /&gt;Bytes transferred = 450560 (6e000 hex)&lt;BR /&gt;Using FEC device&lt;BR /&gt;TFTP from server 192.168.11.148; our IP address is 192.168.11.154&lt;BR /&gt;Filename 'zImage-imx6dl-ccimx6sbc.dtb'.&lt;BR /&gt;Load address: 0x18000000&lt;BR /&gt;Loading: ####&lt;BR /&gt; 194.3 KiB/s&lt;BR /&gt;done&lt;BR /&gt;Bytes transferred = 50162 (c3f2 hex)&lt;BR /&gt;Kernel image @ 0x12000000 [ 0x000000 - 0x55e150 ]&lt;BR /&gt;## Flattened Device Tree blob at 18000000&lt;BR /&gt; Booting using the fdt blob at 0x18000000&lt;BR /&gt; Using Device Tree in place at 18000000, end 1800f3f1&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I supose that It's not loading all bin file, but I don know why.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Sep 2019 17:56:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Rebuild-kernel-and-not-booting/m-p/948521#M141873</guid>
      <dc:creator>emmanuelperea</dc:creator>
      <dc:date>2019-09-04T17:56:26Z</dc:date>
    </item>
    <item>
      <title>Re: Rebuild kernel and not booting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Rebuild-kernel-and-not-booting/m-p/948522#M141874</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi emmanuel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Your kernel is wrong, with the changes you are doing, try to make one by one to localize the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Sep 2019 14:29:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Rebuild-kernel-and-not-booting/m-p/948522#M141874</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2019-09-05T14:29:39Z</dc:date>
    </item>
  </channel>
</rss>