<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックError while flashing custom linux image on emmc</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-flashing-custom-linux-image-on-emmc/m-p/948388#M141852</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have made custom linux image for custom board with iMX-6 processor through yocto for sd-card and for emmc; when I flashed image on sd-card through dd-command it is properly flashed and running.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, when I tried to flash the image on emmc through dd-command it is throwing the below error:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CPU: 2 PID: 94 Comm: mmcqd/3 Tainted: G O 3.14.61-fslc+g327d5c9 #4&lt;BR /&gt;task: a84f1b00 ti: a8524000 task.ti: a8524000&lt;BR /&gt;PC is at ext4_finish_bio+0xc0/0x230&lt;BR /&gt;LR is at ext4_finish_bio+0xec/0x230&lt;BR /&gt;pc : [&amp;lt;8016c9e8&amp;gt;] lr : [&amp;lt;8016ca14&amp;gt;] psr: a0010093&lt;BR /&gt;sp : a8525da8 ip : 00000000 fp : 0000004a&lt;BR /&gt;r10: ab814a40 r9 : 82069b84 r8 : 00001000&lt;BR /&gt;r7 : 00000000 r6 : 00000000 r5 : a75e9800 r4 : 00000000&lt;BR /&gt;r3 : 00000001 r2 : 00000001 r1 : a7009800 r0 : 00000000&lt;BR /&gt;Flags: NzCv IRQs off FIQs on Mode SVC_32 ISA ARM Segment kernel&lt;BR /&gt;Control: 10c53c7d Table: 389f004a DAC: 00000015&lt;BR /&gt;Process mmcqd/3 (pid: 94, stack limit = 0xa8524238)&lt;BR /&gt;Stack: (0xa8525da8 to 0xa8526000)&lt;BR /&gt;5da0: 00000001 00010013 a8524000 a982c280 80a13e04 800189f4&lt;BR /&gt;5dc0: ac060100 8001cca8 80a792c0 80ac9740 ac060100 a849ab60 00000037 a982c280&lt;BR /&gt;5de0: a97d1578 00080000 a97cc2a0 00000000 00000000 00000000 00000000 8016ceec&lt;BR /&gt;5e00: a849ab60 00000037 800194ac 80a15a18 a97cc2a0 00080000 122e8001 00000000&lt;BR /&gt;5e20: 00000000 a982c280 00080000 00080000 a97cc2a0 00000000 00000000 8027d268&lt;BR /&gt;5e40: a84d6950 804beba4 00000000 a97cc2a0 a97cc2a0 00000000 00000000 a84d694c&lt;BR /&gt;5e60: 00000000 a84d6810 a97cc380 8027d584 a97cc2a0 a97cc2a0 a84d7000 00000000&lt;BR /&gt;5e80: a84d694c 8027d8ec a84d6a58 a97cc2a0 a84d6808 a84d6400 a84d694c 804bb8e0&lt;BR /&gt;5ea0: a86f3be0 00000000 a84d6800 00000000 00000000 a86f3be0 a97cc380 a8520e00&lt;BR /&gt;5ec0: a84d7000 00000001 00000001 00000000 a9796b60 a84d6400 a84d6808 a97cc380&lt;BR /&gt;5ee0: a8524000 a84d6800 a84d6800 a84d6810 122e8001 804bbdc0 00080000 a84d7000&lt;BR /&gt;5f00: a84d7000 a829d800 a8524000 00000000 00000001 a84d6810 a84d7000 a84d6808&lt;BR /&gt;5f20: 122e8001 a84d7000 a8524000 00000000 00000001 a84d6810 a9796b60 804bd3dc&lt;BR /&gt;5f40: a84f1b00 00000000 a8553d00 a84d6808 804bd340 00000000 00000000 00000000&lt;BR /&gt;5f60: 00000000 8004de0c b7effaff 00000000 9be67def a84d6808 00000000 00000000&lt;BR /&gt;5f80: a8525f80 a8525f80 00000000 00000000 a8525f90 a8525f90 a8525fac a8553d00&lt;BR /&gt;5fa0: 8004dd40 00000000 00000000 8000e4c0 00000000 00000000 00000000 00000000&lt;BR /&gt;5fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000&lt;BR /&gt;5fe0: 00000000 00000000 00000000 00000000 00000013 00000000 fffdf3db 79ebedbc&lt;BR /&gt;[&amp;lt;8016c9e8&amp;gt;] (ext4_finish_bio) from [&amp;lt;8016ceec&amp;gt;] (ext4_end_bio+0x5c/0x12c)&lt;BR /&gt;[&amp;lt;8016ceec&amp;gt;] (ext4_end_bio) from [&amp;lt;8027d268&amp;gt;] (blk_update_request+0xa4/0x3ac)&lt;BR /&gt;[&amp;lt;8027d268&amp;gt;] (blk_update_request) from [&amp;lt;8027d584&amp;gt;] (blk_update_bidi_request+0x14/0x70)&lt;BR /&gt;[&amp;lt;8027d584&amp;gt;] (blk_update_bidi_request) from [&amp;lt;8027d8ec&amp;gt;] (blk_end_bidi_request+0x14/0x48)&lt;BR /&gt;[&amp;lt;8027d8ec&amp;gt;] (blk_end_bidi_request) from [&amp;lt;804bb8e0&amp;gt;] (mmc_blk_issue_rw_rq+0x798/0xa48)&lt;BR /&gt;[&amp;lt;804bb8e0&amp;gt;] (mmc_blk_issue_rw_rq) from [&amp;lt;804bbdc0&amp;gt;] (mmc_blk_issue_rq+0x230/0x514)&lt;BR /&gt;[&amp;lt;804bbdc0&amp;gt;] (mmc_blk_issue_rq) from [&amp;lt;804bd3dc&amp;gt;] (mmc_queue_thread+0x9c/0x150)&lt;BR /&gt;[&amp;lt;804bd3dc&amp;gt;] (mmc_queue_thread) from [&amp;lt;8004de0c&amp;gt;] (kthread+0xcc/0xe4)&lt;BR /&gt;[&amp;lt;8004de0c&amp;gt;] (kthread) from [&amp;lt;8000e4c0&amp;gt;] (ret_from_fork+0x14/0x34)&lt;BR /&gt;Code: 12877001 e5944004 e1550004 0a00001d (e594301c) &lt;BR /&gt;---[ end trace 67fd1f1b1a8f9c83 ]---&lt;BR /&gt;note: mmcqd/3[94] exited with preempt_count 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone tell me where could be the problem is !!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Oct 2019 10:39:02 GMT</pubDate>
    <dc:creator>purvi_billore1</dc:creator>
    <dc:date>2019-10-04T10:39:02Z</dc:date>
    <item>
      <title>Error while flashing custom linux image on emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-flashing-custom-linux-image-on-emmc/m-p/948388#M141852</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have made custom linux image for custom board with iMX-6 processor through yocto for sd-card and for emmc; when I flashed image on sd-card through dd-command it is properly flashed and running.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, when I tried to flash the image on emmc through dd-command it is throwing the below error:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CPU: 2 PID: 94 Comm: mmcqd/3 Tainted: G O 3.14.61-fslc+g327d5c9 #4&lt;BR /&gt;task: a84f1b00 ti: a8524000 task.ti: a8524000&lt;BR /&gt;PC is at ext4_finish_bio+0xc0/0x230&lt;BR /&gt;LR is at ext4_finish_bio+0xec/0x230&lt;BR /&gt;pc : [&amp;lt;8016c9e8&amp;gt;] lr : [&amp;lt;8016ca14&amp;gt;] psr: a0010093&lt;BR /&gt;sp : a8525da8 ip : 00000000 fp : 0000004a&lt;BR /&gt;r10: ab814a40 r9 : 82069b84 r8 : 00001000&lt;BR /&gt;r7 : 00000000 r6 : 00000000 r5 : a75e9800 r4 : 00000000&lt;BR /&gt;r3 : 00000001 r2 : 00000001 r1 : a7009800 r0 : 00000000&lt;BR /&gt;Flags: NzCv IRQs off FIQs on Mode SVC_32 ISA ARM Segment kernel&lt;BR /&gt;Control: 10c53c7d Table: 389f004a DAC: 00000015&lt;BR /&gt;Process mmcqd/3 (pid: 94, stack limit = 0xa8524238)&lt;BR /&gt;Stack: (0xa8525da8 to 0xa8526000)&lt;BR /&gt;5da0: 00000001 00010013 a8524000 a982c280 80a13e04 800189f4&lt;BR /&gt;5dc0: ac060100 8001cca8 80a792c0 80ac9740 ac060100 a849ab60 00000037 a982c280&lt;BR /&gt;5de0: a97d1578 00080000 a97cc2a0 00000000 00000000 00000000 00000000 8016ceec&lt;BR /&gt;5e00: a849ab60 00000037 800194ac 80a15a18 a97cc2a0 00080000 122e8001 00000000&lt;BR /&gt;5e20: 00000000 a982c280 00080000 00080000 a97cc2a0 00000000 00000000 8027d268&lt;BR /&gt;5e40: a84d6950 804beba4 00000000 a97cc2a0 a97cc2a0 00000000 00000000 a84d694c&lt;BR /&gt;5e60: 00000000 a84d6810 a97cc380 8027d584 a97cc2a0 a97cc2a0 a84d7000 00000000&lt;BR /&gt;5e80: a84d694c 8027d8ec a84d6a58 a97cc2a0 a84d6808 a84d6400 a84d694c 804bb8e0&lt;BR /&gt;5ea0: a86f3be0 00000000 a84d6800 00000000 00000000 a86f3be0 a97cc380 a8520e00&lt;BR /&gt;5ec0: a84d7000 00000001 00000001 00000000 a9796b60 a84d6400 a84d6808 a97cc380&lt;BR /&gt;5ee0: a8524000 a84d6800 a84d6800 a84d6810 122e8001 804bbdc0 00080000 a84d7000&lt;BR /&gt;5f00: a84d7000 a829d800 a8524000 00000000 00000001 a84d6810 a84d7000 a84d6808&lt;BR /&gt;5f20: 122e8001 a84d7000 a8524000 00000000 00000001 a84d6810 a9796b60 804bd3dc&lt;BR /&gt;5f40: a84f1b00 00000000 a8553d00 a84d6808 804bd340 00000000 00000000 00000000&lt;BR /&gt;5f60: 00000000 8004de0c b7effaff 00000000 9be67def a84d6808 00000000 00000000&lt;BR /&gt;5f80: a8525f80 a8525f80 00000000 00000000 a8525f90 a8525f90 a8525fac a8553d00&lt;BR /&gt;5fa0: 8004dd40 00000000 00000000 8000e4c0 00000000 00000000 00000000 00000000&lt;BR /&gt;5fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000&lt;BR /&gt;5fe0: 00000000 00000000 00000000 00000000 00000013 00000000 fffdf3db 79ebedbc&lt;BR /&gt;[&amp;lt;8016c9e8&amp;gt;] (ext4_finish_bio) from [&amp;lt;8016ceec&amp;gt;] (ext4_end_bio+0x5c/0x12c)&lt;BR /&gt;[&amp;lt;8016ceec&amp;gt;] (ext4_end_bio) from [&amp;lt;8027d268&amp;gt;] (blk_update_request+0xa4/0x3ac)&lt;BR /&gt;[&amp;lt;8027d268&amp;gt;] (blk_update_request) from [&amp;lt;8027d584&amp;gt;] (blk_update_bidi_request+0x14/0x70)&lt;BR /&gt;[&amp;lt;8027d584&amp;gt;] (blk_update_bidi_request) from [&amp;lt;8027d8ec&amp;gt;] (blk_end_bidi_request+0x14/0x48)&lt;BR /&gt;[&amp;lt;8027d8ec&amp;gt;] (blk_end_bidi_request) from [&amp;lt;804bb8e0&amp;gt;] (mmc_blk_issue_rw_rq+0x798/0xa48)&lt;BR /&gt;[&amp;lt;804bb8e0&amp;gt;] (mmc_blk_issue_rw_rq) from [&amp;lt;804bbdc0&amp;gt;] (mmc_blk_issue_rq+0x230/0x514)&lt;BR /&gt;[&amp;lt;804bbdc0&amp;gt;] (mmc_blk_issue_rq) from [&amp;lt;804bd3dc&amp;gt;] (mmc_queue_thread+0x9c/0x150)&lt;BR /&gt;[&amp;lt;804bd3dc&amp;gt;] (mmc_queue_thread) from [&amp;lt;8004de0c&amp;gt;] (kthread+0xcc/0xe4)&lt;BR /&gt;[&amp;lt;8004de0c&amp;gt;] (kthread) from [&amp;lt;8000e4c0&amp;gt;] (ret_from_fork+0x14/0x34)&lt;BR /&gt;Code: 12877001 e5944004 e1550004 0a00001d (e594301c) &lt;BR /&gt;---[ end trace 67fd1f1b1a8f9c83 ]---&lt;BR /&gt;note: mmcqd/3[94] exited with preempt_count 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone tell me where could be the problem is !!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Oct 2019 10:39:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-flashing-custom-linux-image-on-emmc/m-p/948388#M141852</guid>
      <dc:creator>purvi_billore1</dc:creator>
      <dc:date>2019-10-04T10:39:02Z</dc:date>
    </item>
    <item>
      <title>Re: Error while flashing custom linux image on emmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-while-flashing-custom-linux-image-on-emmc/m-p/948389#M141853</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Purvi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Apparently your eMMC is damage or Please try the DDR Stress Test : perhaps memory re-calibration is needed.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-105652"&gt;https://community.nxp.com/docs/DOC-105652&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Oct 2019 14:39:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-while-flashing-custom-linux-image-on-emmc/m-p/948389#M141853</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2019-10-08T14:39:40Z</dc:date>
    </item>
  </channel>
</rss>