<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX8M UUU flashing kernel error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-UUU-flashing-kernel-error/m-p/947403#M141727</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using the IMX8M mini evaluation kit.&lt;/P&gt;&lt;P&gt;I'm using the YOCTO BSP imx-4.14.98-2.0.0_ga and I'm able to build an image for the eMMC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to flash the eMMC (with UUU tool) using the script "example_kernel_emmc.uuu" (I found this script in the IMX8M eval kit prebuild image).&lt;/P&gt;&lt;P&gt;I edited the script to replace the kernel/dtb/rootfs file name with mine. The script is also expecting a initramfs file, which I don't have (YOCTO doesn't generate it) so I commented the line handling the initramfs.&lt;/P&gt;&lt;P&gt;The script start by loading the bootloader into the i.MX, then uboot start and download the kernel/dtb/rootfs and copy it in eMMC.&lt;/P&gt;&lt;P&gt;Unfortunately it doesn't work, I end up with an error during the flashing (right after the download of the image).&lt;/P&gt;&lt;P&gt;Here is the uboot log:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Wrong Ramdisk Image Format&lt;BR /&gt;Ramdisk image is corrupt or invalid&lt;/P&gt;&lt;P&gt;[ ... ]&lt;/P&gt;&lt;P&gt;## Loading ramdisk from FIT Image at 43000000 ...&lt;BR /&gt;Bad FIT ramdisk image format!&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Do you know what is going wrong ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NOTE: I attached the script "example_kernel_emmc.uuu" with some commentaries.&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Jul 2019 15:23:49 GMT</pubDate>
    <dc:creator>clement22</dc:creator>
    <dc:date>2019-07-05T15:23:49Z</dc:date>
    <item>
      <title>IMX8M UUU flashing kernel error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-UUU-flashing-kernel-error/m-p/947403#M141727</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using the IMX8M mini evaluation kit.&lt;/P&gt;&lt;P&gt;I'm using the YOCTO BSP imx-4.14.98-2.0.0_ga and I'm able to build an image for the eMMC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to flash the eMMC (with UUU tool) using the script "example_kernel_emmc.uuu" (I found this script in the IMX8M eval kit prebuild image).&lt;/P&gt;&lt;P&gt;I edited the script to replace the kernel/dtb/rootfs file name with mine. The script is also expecting a initramfs file, which I don't have (YOCTO doesn't generate it) so I commented the line handling the initramfs.&lt;/P&gt;&lt;P&gt;The script start by loading the bootloader into the i.MX, then uboot start and download the kernel/dtb/rootfs and copy it in eMMC.&lt;/P&gt;&lt;P&gt;Unfortunately it doesn't work, I end up with an error during the flashing (right after the download of the image).&lt;/P&gt;&lt;P&gt;Here is the uboot log:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Wrong Ramdisk Image Format&lt;BR /&gt;Ramdisk image is corrupt or invalid&lt;/P&gt;&lt;P&gt;[ ... ]&lt;/P&gt;&lt;P&gt;## Loading ramdisk from FIT Image at 43000000 ...&lt;BR /&gt;Bad FIT ramdisk image format!&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Do you know what is going wrong ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NOTE: I attached the script "example_kernel_emmc.uuu" with some commentaries.&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2019 15:23:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-UUU-flashing-kernel-error/m-p/947403#M141727</guid>
      <dc:creator>clement22</dc:creator>
      <dc:date>2019-07-05T15:23:49Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M UUU flashing kernel error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-UUU-flashing-kernel-error/m-p/947404#M141728</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Clement&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;initramfs is described in uuu documentation:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/NXPmicro/mfgtools/releases/download/uuu_1.2.0/UUU.pdf" title="https://github.com/NXPmicro/mfgtools/releases/download/uuu_1.2.0/UUU.pdf"&gt;https://github.com/NXPmicro/mfgtools/releases/download/uuu_1.2.0/UUU.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;for its generation one can try steps provided in sect.6.2 Manufacturing Tool, MFGTool&lt;/P&gt;&lt;P&gt;attached Yocto Guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2019 23:50:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-UUU-flashing-kernel-error/m-p/947404#M141728</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-07-05T23:50:04Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M UUU flashing kernel error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-UUU-flashing-kernel-error/m-p/947405#M141729</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the documentation, I'm going to try it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to flash the kernel + roofs without generating the initramfs ? For example just flashing the kernel using the UUU SDP command ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jul 2019 09:19:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-UUU-flashing-kernel-error/m-p/947405#M141729</guid>
      <dc:creator>clement22</dc:creator>
      <dc:date>2019-07-08T09:19:39Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8M UUU flashing kernel error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8M-UUU-flashing-kernel-error/m-p/947406#M141730</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;one can look at uuu.auto&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jul 2019 12:28:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8M-UUU-flashing-kernel-error/m-p/947406#M141730</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-07-08T12:28:45Z</dc:date>
    </item>
  </channel>
</rss>