<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Build fail at binutils_2.30</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Build-fail-at-binutils-2-30/m-p/947218#M141673</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you doesn't has enough host memory then also come. please try accommodate 100-150 GB for yocto.&amp;nbsp;&lt;/P&gt;&lt;P&gt;No where RAM will link to build. or is there any target configuration is changed.??????&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 13 Jul 2019 04:19:20 GMT</pubDate>
    <dc:creator>viswa_kondapall</dc:creator>
    <dc:date>2019-07-13T04:19:20Z</dc:date>
    <item>
      <title>Build fail at binutils_2.30</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Build-fail-at-binutils-2-30/m-p/947215#M141670</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am new to IMX8, I am trying to build yocto for iMX8DualX4 using kernel source imx-4.14.78-1.0.0.&lt;/P&gt;&lt;P&gt;It's almost done but then it fail at module binutils_2.30. The log file is attached.&lt;/P&gt;&lt;P&gt;Most of the error related to "Undefined reference to..", eg:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; powerpc.o:/usr/src/debug/binutils/2.30-r0/git/gold/powerpc.cc:3189: undefined reference to `.LASF12'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea from where I should start to check?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2019 08:16:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Build-fail-at-binutils-2-30/m-p/947215#M141670</guid>
      <dc:creator>tuanpham</dc:creator>
      <dc:date>2019-07-05T08:16:46Z</dc:date>
    </item>
    <item>
      <title>Re: Build fail at binutils_2.30</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Build-fail-at-binutils-2-30/m-p/947216#M141671</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;Please clean the built for the package. In download the package is broken.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bitbake -c cleanall -f binutils -- this will fix ur error&lt;/P&gt;&lt;P&gt;then run the build script.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Jul 2019 12:43:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Build-fail-at-binutils-2-30/m-p/947216#M141671</guid>
      <dc:creator>viswa_kondapall</dc:creator>
      <dc:date>2019-07-06T12:43:34Z</dc:date>
    </item>
    <item>
      <title>Re: Build fail at binutils_2.30</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Build-fail-at-binutils-2-30/m-p/947217#M141672</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Viswanath,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I noticed one error before that:&lt;/P&gt;&lt;P&gt;ERROR: ExpansionError during parsing /home/tuanpham/imx-yocto-bsp/sources/poky/meta/recipes-graphics/images/core-image-weston.bb&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;... [Errno 12] Cannot allocate memory&lt;/P&gt;&lt;P&gt;This is due to not enough RAM. But some how the build is still running and later it throws that error when compiling binutils_2.30.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not sure if they are linked together or not, but I discarded the build folder, increase RAM and started fresh build, it then completes with no error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 07 Jul 2019 10:57:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Build-fail-at-binutils-2-30/m-p/947217#M141672</guid>
      <dc:creator>tuanpham</dc:creator>
      <dc:date>2019-07-07T10:57:50Z</dc:date>
    </item>
    <item>
      <title>Re: Build fail at binutils_2.30</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Build-fail-at-binutils-2-30/m-p/947218#M141673</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you doesn't has enough host memory then also come. please try accommodate 100-150 GB for yocto.&amp;nbsp;&lt;/P&gt;&lt;P&gt;No where RAM will link to build. or is there any target configuration is changed.??????&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 13 Jul 2019 04:19:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Build-fail-at-binutils-2-30/m-p/947218#M141673</guid>
      <dc:creator>viswa_kondapall</dc:creator>
      <dc:date>2019-07-13T04:19:20Z</dc:date>
    </item>
  </channel>
</rss>