<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MC34708 on START-R Board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MC34708-on-START-R-Board/m-p/218864#M14158</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;thanks a lot for your fast reply.&lt;/P&gt;&lt;P&gt;In my application I have no battery.&lt;/P&gt;&lt;P&gt;I will leave that pins connected as per the Quick Start board schematics.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Filippo&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;BR /&gt; &lt;CITE&gt;Mark Middleton said:&lt;/CITE&gt;&lt;/P&gt;&lt;BLOCKQUOTE cite="http://imxcommunity.org/forum/topics/mc34708-on-start-r-board?groupUrl=imx53hardwaredesign&amp;amp;#4103961Comment62982"&gt;&lt;DIV&gt;&lt;DIV class="xg_user_generated"&gt;&lt;P&gt;Hi Filippo,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think the first thing you need to know is that the MC34708 PMIC was primarily designed to work in portable devices with a Li-ION battery. The Quick Start board, as a software development board, is designed primarily to run from a DC wall power source. The PMIC must be connected to either use an always conencted battery, or to operate without a battery. Since Freescale does not ship Li-ION batteries for liability reasons, we could not guarantee that customers would have a Li-ION battery, and therefore, the PMIC power structure on the Quick Start board is designed for only 5V wall power operations.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This means that U28 was required to simulate battery power, and is conencted to the PMIC like it was a battery. But since charging functions are disabled, there cannot be a 5V connection to either VBUSVIN or VAUXVIN.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So to answer your questions:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) ITRIC is a trickle charge pin used to provide an initial conditioning current to a dead battery. Because there is no real battery in this case, it is simple connected to the battery bus VCC_BP and left that way for this design.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) GBAT is a pin that controls a battery charging FET. Again, since there is no actual battery, there is no charging. Per the datasheet, this pin must be connected to ground.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this clears things up,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Mar 2012 16:22:35 GMT</pubDate>
    <dc:creator>Filippo</dc:creator>
    <dc:date>2012-03-12T16:22:35Z</dc:date>
    <item>
      <title>MC34708 on START-R Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MC34708-on-START-R-Board/m-p/218862#M14156</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I'm designing a board starting from START-R reference schematic. I'm planning to use the MC34708 PMIC, but I have two questions:&lt;/P&gt;&lt;P&gt;1) In my understanding, the ITRIC pin ( ball E8 on page 15 ) seems to me an output, but on the schematics I see this pin connected to VCC_BP. The VCC_BP is generated by U28 on page 3. Is this correct ?&lt;/P&gt;&lt;P&gt;2) The GBAT pin ( ball B6 on page 15 ) is tied to ground, but on the datasheet I see this is an output that drives the external mosfet for the battery charging section. Is this&amp;nbsp;correct ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are also some warnings detected by OrCad drc, but I think they are pin defines issues on the MC34708 symbol.&lt;/P&gt;&lt;P&gt;Thank you for your help&lt;/P&gt;&lt;P&gt;Filippo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Mar 2012 10:56:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MC34708-on-START-R-Board/m-p/218862#M14156</guid>
      <dc:creator>Filippo</dc:creator>
      <dc:date>2012-03-12T10:56:26Z</dc:date>
    </item>
    <item>
      <title>Re: MC34708 on START-R Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MC34708-on-START-R-Board/m-p/218863#M14157</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Filippo,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think the first thing you need to know is that the MC34708 PMIC was primarily designed to work in portable devices with a Li-ION battery. The Quick Start board, as a software development board, is designed primarily to run from a DC wall power source. The PMIC must be connected to either use an always conencted battery, or to operate without a battery. Since Freescale does not ship Li-ION batteries for liability reasons, we could not guarantee that customers would have a Li-ION battery, and therefore, the PMIC power structure on the Quick Start board is designed for only 5V wall power operations.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This means that U28 was required to simulate battery power, and is conencted to the PMIC like it was a battery. But since charging functions are disabled, there cannot be a 5V connection to either VBUSVIN or VAUXVIN.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So to answer your questions:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) ITRIC is a trickle charge pin used to provide an initial conditioning current to a dead battery. Because there is no real battery in this case, it is simple connected to the battery bus VCC_BP and left that way for this design.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) GBAT is a pin that controls a battery charging FET. Again, since there is no actual battery, there is no charging. Per the datasheet, this pin must be connected to ground.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this clears things up,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Mar 2012 16:03:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MC34708-on-START-R-Board/m-p/218863#M14157</guid>
      <dc:creator>TheAdmiral</dc:creator>
      <dc:date>2012-03-12T16:03:29Z</dc:date>
    </item>
    <item>
      <title>Re: MC34708 on START-R Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MC34708-on-START-R-Board/m-p/218864#M14158</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;thanks a lot for your fast reply.&lt;/P&gt;&lt;P&gt;In my application I have no battery.&lt;/P&gt;&lt;P&gt;I will leave that pins connected as per the Quick Start board schematics.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Filippo&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;BR /&gt; &lt;CITE&gt;Mark Middleton said:&lt;/CITE&gt;&lt;/P&gt;&lt;BLOCKQUOTE cite="http://imxcommunity.org/forum/topics/mc34708-on-start-r-board?groupUrl=imx53hardwaredesign&amp;amp;#4103961Comment62982"&gt;&lt;DIV&gt;&lt;DIV class="xg_user_generated"&gt;&lt;P&gt;Hi Filippo,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think the first thing you need to know is that the MC34708 PMIC was primarily designed to work in portable devices with a Li-ION battery. The Quick Start board, as a software development board, is designed primarily to run from a DC wall power source. The PMIC must be connected to either use an always conencted battery, or to operate without a battery. Since Freescale does not ship Li-ION batteries for liability reasons, we could not guarantee that customers would have a Li-ION battery, and therefore, the PMIC power structure on the Quick Start board is designed for only 5V wall power operations.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This means that U28 was required to simulate battery power, and is conencted to the PMIC like it was a battery. But since charging functions are disabled, there cannot be a 5V connection to either VBUSVIN or VAUXVIN.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So to answer your questions:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) ITRIC is a trickle charge pin used to provide an initial conditioning current to a dead battery. Because there is no real battery in this case, it is simple connected to the battery bus VCC_BP and left that way for this design.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) GBAT is a pin that controls a battery charging FET. Again, since there is no actual battery, there is no charging. Per the datasheet, this pin must be connected to ground.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this clears things up,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Mar 2012 16:22:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MC34708-on-START-R-Board/m-p/218864#M14158</guid>
      <dc:creator>Filippo</dc:creator>
      <dc:date>2012-03-12T16:22:35Z</dc:date>
    </item>
  </channel>
</rss>