<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Testing EMMC fastboot mode on IMX8QX MEK</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Testing-EMMC-fastboot-mode-on-IMX8QX-MEK/m-p/945363#M141431</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Komal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;your understanding is correct, eMMC fastboot can be activated only from fuse,&lt;/P&gt;&lt;P&gt;there is no way to test this mode without permanently programming efuses.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Jul 2019 10:31:37 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-07-05T10:31:37Z</dc:date>
    <item>
      <title>Testing EMMC fastboot mode on IMX8QX MEK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Testing-EMMC-fastboot-mode-on-IMX8QX-MEK/m-p/945362#M141430</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We would like to test various options from booting from EMMC&amp;nbsp;on IMX8QX MEK:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. EMMC fastboot mode&lt;/P&gt;&lt;P&gt;2. EMMC high speed&lt;/P&gt;&lt;P&gt;3. EMMC bus width selection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the Reference Manual (IMX8DQXPRM) section 5.8.2.1 (Boot Devices -&amp;gt; Expansion Device eFUSE configuration), I understand that the eFUSE needs to be programmed to select the above boot options. However, blowing eFUSE is a one time operation, which cannot be reverted.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to use the 'fuse override' command from u-boot, but it fails with the message 'Override fuse to i.MX8 in u-boot is forbidden'. Also, as I understand, the override setting will be lost on reset. However, the boot mode testing can only be done by resetting the board, so the override will not be useful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way to test the above modes without permanently programming eFUSE bits?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2019 09:12:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Testing-EMMC-fastboot-mode-on-IMX8QX-MEK/m-p/945362#M141430</guid>
      <dc:creator>komal_jpadia</dc:creator>
      <dc:date>2019-07-05T09:12:17Z</dc:date>
    </item>
    <item>
      <title>Re: Testing EMMC fastboot mode on IMX8QX MEK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Testing-EMMC-fastboot-mode-on-IMX8QX-MEK/m-p/945363#M141431</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Komal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;your understanding is correct, eMMC fastboot can be activated only from fuse,&lt;/P&gt;&lt;P&gt;there is no way to test this mode without permanently programming efuses.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2019 10:31:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Testing-EMMC-fastboot-mode-on-IMX8QX-MEK/m-p/945363#M141431</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-07-05T10:31:37Z</dc:date>
    </item>
    <item>
      <title>Re: Testing EMMC fastboot mode on IMX8QX MEK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Testing-EMMC-fastboot-mode-on-IMX8QX-MEK/m-p/945364#M141432</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Igor for your prompt reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So in that case, there is no way to change emmc rate and number of data lines for testing purpose only? Since these are also set in the eFUSE?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, since emmc fastboot cannot be tested without permanently setting the fuses, is there any experimental data available from NXP regarding boot performance of emmc fastboot vs emmc normal boot ?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2019 10:35:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Testing-EMMC-fastboot-mode-on-IMX8QX-MEK/m-p/945364#M141432</guid>
      <dc:creator>komal_jpadia</dc:creator>
      <dc:date>2019-07-05T10:35:53Z</dc:date>
    </item>
    <item>
      <title>Re: Testing EMMC fastboot mode on IMX8QX MEK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Testing-EMMC-fastboot-mode-on-IMX8QX-MEK/m-p/945365#M141433</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Komal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;your understanding is correct. Unfortunately I am not aware&lt;/P&gt;&lt;P&gt;of boot performance of emmc fastboot vs emmc normal boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2019 11:33:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Testing-EMMC-fastboot-mode-on-IMX8QX-MEK/m-p/945365#M141433</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-07-05T11:33:06Z</dc:date>
    </item>
    <item>
      <title>Re: Testing EMMC fastboot mode on IMX8QX MEK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Testing-EMMC-fastboot-mode-on-IMX8QX-MEK/m-p/945366#M141434</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Komal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am wondering if you did any benchmark testing after permanently setting the fuse.&amp;nbsp; I'm in the same situation, and I'd like to find out if you were able to provide any general results - maybe even percentages - before I proceed.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your time!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Lacy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Aug 2019 17:58:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Testing-EMMC-fastboot-mode-on-IMX8QX-MEK/m-p/945366#M141434</guid>
      <dc:creator>lsanvictores</dc:creator>
      <dc:date>2019-08-22T17:58:52Z</dc:date>
    </item>
  </channel>
</rss>