<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.mx53QSB available GPIO for testing</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx53QSB-available-GPIO-for-testing/m-p/218775#M14131</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tugrul,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The JTAG pins cannot be used as GPIO pins. They are for core diagnostics communications only, and do not connect to any higher level processor functions.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would probably recommend that you could use EIM_OE (V8) or EIM_RW (AB4). These two traces have resistor that you should be able to easily access. As long as you are not using them for VGA output, you can reconfigure them to GPIO pins. Another choice might&amp;nbsp;be to use any of the SD1 card pins. These traces can be reconfigured for GPIO use as well.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In reading your request, I do have one concern: Logic high levels will vary from GPIO pin depending on which module (EIM, PATA, SD) the pin is assigned. Voltage levels for the different modules are determined by the power applied to the NVCC_ pins. For example, on the Quick Start board, pins assigned to NANDF module will have a logic high of 1.8V, as well as pins assigned to CSI module. Most other modules will have a 3.3V logic high. If you are taking measurements to determine how a pin will act for a future hardware build, you need to make sure you are taking a measurement from a pin that will share the same module domain. Otherwise, you might find that the pin you actual use does not have the same characteristic as the one you measured.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helped,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Mar 2012 15:35:57 GMT</pubDate>
    <dc:creator>TheAdmiral</dc:creator>
    <dc:date>2012-03-12T15:35:57Z</dc:date>
    <item>
      <title>i.mx53QSB available GPIO for testing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx53QSB-available-GPIO-for-testing/m-p/218774#M14130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to measure some TTL level signals with oscilloscope therefore I need an output pin on the board I know that there is USER_LED but it's hard to connect ossilloscope on it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have seen the connector J15 has JTAG_TDO pin but as far as i know it's not connected to CPU. Is it possible to use it as GPIO ?&lt;/P&gt;&lt;P&gt;Do you know anything else that I can use an an output pin?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Tugrul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Mar 2012 09:33:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx53QSB-available-GPIO-for-testing/m-p/218774#M14130</guid>
      <dc:creator>TugrulGuclu</dc:creator>
      <dc:date>2012-03-12T09:33:53Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx53QSB available GPIO for testing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx53QSB-available-GPIO-for-testing/m-p/218775#M14131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tugrul,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The JTAG pins cannot be used as GPIO pins. They are for core diagnostics communications only, and do not connect to any higher level processor functions.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would probably recommend that you could use EIM_OE (V8) or EIM_RW (AB4). These two traces have resistor that you should be able to easily access. As long as you are not using them for VGA output, you can reconfigure them to GPIO pins. Another choice might&amp;nbsp;be to use any of the SD1 card pins. These traces can be reconfigured for GPIO use as well.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In reading your request, I do have one concern: Logic high levels will vary from GPIO pin depending on which module (EIM, PATA, SD) the pin is assigned. Voltage levels for the different modules are determined by the power applied to the NVCC_ pins. For example, on the Quick Start board, pins assigned to NANDF module will have a logic high of 1.8V, as well as pins assigned to CSI module. Most other modules will have a 3.3V logic high. If you are taking measurements to determine how a pin will act for a future hardware build, you need to make sure you are taking a measurement from a pin that will share the same module domain. Otherwise, you might find that the pin you actual use does not have the same characteristic as the one you measured.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helped,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Mar 2012 15:35:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx53QSB-available-GPIO-for-testing/m-p/218775#M14131</guid>
      <dc:creator>TheAdmiral</dc:creator>
      <dc:date>2012-03-12T15:35:57Z</dc:date>
    </item>
  </channel>
</rss>