<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Android9.0+imx8mini mipi to lvds issue?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943672#M141134</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Reply to @Linh Nguyen&lt;/P&gt;&lt;P&gt;&amp;gt; I also face the same problem with NT35596 based MIPI DSI LCD. Actually, the first 6 MIPI DSI commands work fine (after LCD panel reset signal),&lt;/P&gt;&lt;P&gt;&amp;gt; then "wait pkthdr tx done time out" error returned on all later MIPI commands.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;DIV class=""&gt;&lt;P&gt;I added a new display&amp;nbsp;(the ORIC ORC03003N-40) using the Sitronix ST7701 driver chip&amp;nbsp; to the iMX8MM EVK.&lt;/P&gt;&lt;P&gt;I patched the Raydium rm67191 driver by only changing the init sequence to the manufacturer command set of the new display, adjusted the pixel clock, and corrected the number of lanes in the corresponding dts and I immediately got colored stripes shown on the display.&lt;/P&gt;&lt;P&gt;One important observation is that the raydium driver uses&lt;/P&gt;&lt;P&gt;mipi_dsi_generic_write() to send mipi commands, which is working, while mipi_dsi_dcs_write_buffer() failed with "wait payload tx done time out" or ""wait pkthdr tx done time out" errors (in kernel log) after about four successful writes.&lt;/P&gt;&lt;P&gt;Find patches for i.MX8MM Android 10 sources below.&lt;/P&gt;&lt;P&gt;Apply with&lt;/P&gt;&lt;P&gt;cd imx-android-10/android_build/vendor/nxp-opensource/kernel_imx&lt;/P&gt;&lt;P&gt;git apply 0001-add-st7701-driver-shows-stripes-not-finished.patch&lt;/P&gt;&lt;P&gt;cd imx-android-10/android_build/device/fsl&lt;/P&gt;&lt;P&gt;git apply 0001-change-mipi-display-to-st7701.patch&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 12 Apr 2020 21:37:48 GMT</pubDate>
    <dc:creator>nxp31</dc:creator>
    <dc:date>2020-04-12T21:37:48Z</dc:date>
    <item>
      <title>Android9.0+imx8mini mipi to lvds issue?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943663#M141125</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community:&lt;/P&gt;&lt;P&gt;Someone passed the mipi output function on imx8mini? Using the official evk board, using "fsl-imx8mm-ddr4-evk-rm67191.dts", mipi reports the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any kind people come help?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;[ 1.629364] imx_sec_dsim_drv 32e10000.mipi_dsi: wait pkthdr tx done time out&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;[ 1.629370] panel-lt-lt9211 32e10000.mipi_dsi.0: [drm:lt9211_panel_enable] *ERROR* Failed to exit sleep mode (-16)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;[ 1.629375] panel-lt-lt9211 32e10000.mipi_dsi.0: [drm:lt9211_panel_enable] *ERROR* lt9211_panel_prepare failed (-16)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="color: #0000ff;"&gt;[ 1.629379] imx_sec_dsim_drv 32e10000.mipi_dsi: panel enable failed: -16&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Aug 2019 07:16:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943663#M141125</guid>
      <dc:creator>传策薛</dc:creator>
      <dc:date>2019-08-02T07:16:59Z</dc:date>
    </item>
    <item>
      <title>Re: Android9.0+imx8mini mipi to lvds issue?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943664#M141126</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;did you use hdmi though mipi dsi?rm67191 is for oled, if you want to use hdmi, try to use the default dtb, like fsl-imx8mm-evk.dtb&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Aug 2019 05:32:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943664#M141126</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2019-08-08T05:32:53Z</dc:date>
    </item>
    <item>
      <title>Re: Android9.0+imx8mini mipi to lvds issue?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943665#M141127</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Our design is mipi to lvds, so I want the mipi end to always output a stable signal to the chip processing, our chip is lt9211&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Aug 2019 05:30:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943665#M141127</guid>
      <dc:creator>传策薛</dc:creator>
      <dc:date>2019-08-12T05:30:58Z</dc:date>
    </item>
    <item>
      <title>Re: Android9.0+imx8mini mipi to lvds issue?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943666#M141128</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;as I mentioned, use fsl-imx8mm-evk.dtb, rm67191 is for oled&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Aug 2019 07:27:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943666#M141128</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2019-08-12T07:27:38Z</dc:date>
    </item>
    <item>
      <title>Re: Android9.0+imx8mini mipi to lvds issue?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943667#M141129</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello @&lt;A _jive_internal="true" data-content-finding="Community" data-userid="310064" data-username="传策薛" href="https://community.nxp.com/people/传策薛" style="color: #3d9ce7; background-color: #ffffff; border: 0px; font-weight: 200; text-decoration: underline; font-size: 1.286rem;"&gt;传策 薛&lt;/A&gt;&amp;nbsp;, 8mm Driver lt9211 display screen split screen jitter encountered ?&lt;span class="lia-inline-image-display-wrapper" image-alt="e2c36e543d2bd1db3380d478201b0f5.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/99584i99EDA54D1C1B524A/image-size/large?v=v2&amp;amp;px=999" role="button" title="e2c36e543d2bd1db3380d478201b0f5.jpg" alt="e2c36e543d2bd1db3380d478201b0f5.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Dec 2019 01:40:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943667#M141129</guid>
      <dc:creator>aber</dc:creator>
      <dc:date>2019-12-26T01:40:54Z</dc:date>
    </item>
    <item>
      <title>Re: Android9.0+imx8mini mipi to lvds issue?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943668#M141130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;maybe the config problem&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jan 2020 11:56:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943668#M141130</guid>
      <dc:creator>传策薛</dc:creator>
      <dc:date>2020-01-06T11:56:35Z</dc:date>
    </item>
    <item>
      <title>Re: Android9.0+imx8mini mipi to lvds issue?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943669#M141131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I also face the same problem with NT35596 based MIPI DSI LCD. Actually, the first 6 MIPI DSI commands work fine (after LCD panel reset signal), then "wait pkthdr tx done time out" error returned on all later MIPI commands.&lt;/P&gt;&lt;P&gt;But MIPI DSI commands work fine on other type of LCD driver IC.&lt;/P&gt;&lt;P&gt;I'm using iMX8M Mini.&lt;/P&gt;&lt;P&gt;Did you solved the error? or any idea? Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jan 2020 12:34:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943669#M141131</guid>
      <dc:creator>LinhNguyen</dc:creator>
      <dc:date>2020-01-06T12:34:48Z</dc:date>
    </item>
    <item>
      <title>Re: Android9.0+imx8mini mipi to lvds issue?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943670#M141132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;problem solved ! tks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jan 2020 08:56:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943670#M141132</guid>
      <dc:creator>aber</dc:creator>
      <dc:date>2020-01-07T08:56:07Z</dc:date>
    </item>
    <item>
      <title>Re: Android9.0+imx8mini mipi to lvds issue?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943671#M141133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;driver panel_enable method modifly:&lt;/P&gt;&lt;P&gt;ret = mipi_dsi_dcs_write(dsi, MIPI_DCS_WRITE_CONTROL_DISPLAY,&lt;BR /&gt; (u8[]){ 0x24 }, 1);&lt;BR /&gt; if (ret &amp;lt; 0) {&lt;BR /&gt; dev_err(dev, "failed to write control display: %d\n", ret);&lt;BR /&gt; return ret;&lt;BR /&gt; }&lt;/P&gt;&lt;P&gt;/* Set pixel format to RGB888 */&lt;BR /&gt; ret = mipi_dsi_dcs_set_pixel_format(dsi, 0x77);&lt;BR /&gt; if (ret &amp;lt; 0) {&lt;BR /&gt; DRM_DEV_ERROR(dev, "Failed to set pixel format (%d)\n", ret);&lt;BR /&gt; goto fail;&lt;BR /&gt; }&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jan 2020 09:01:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943671#M141133</guid>
      <dc:creator>aber</dc:creator>
      <dc:date>2020-01-07T09:01:06Z</dc:date>
    </item>
    <item>
      <title>Re: Android9.0+imx8mini mipi to lvds issue?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943672#M141134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Reply to @Linh Nguyen&lt;/P&gt;&lt;P&gt;&amp;gt; I also face the same problem with NT35596 based MIPI DSI LCD. Actually, the first 6 MIPI DSI commands work fine (after LCD panel reset signal),&lt;/P&gt;&lt;P&gt;&amp;gt; then "wait pkthdr tx done time out" error returned on all later MIPI commands.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;DIV class=""&gt;&lt;P&gt;I added a new display&amp;nbsp;(the ORIC ORC03003N-40) using the Sitronix ST7701 driver chip&amp;nbsp; to the iMX8MM EVK.&lt;/P&gt;&lt;P&gt;I patched the Raydium rm67191 driver by only changing the init sequence to the manufacturer command set of the new display, adjusted the pixel clock, and corrected the number of lanes in the corresponding dts and I immediately got colored stripes shown on the display.&lt;/P&gt;&lt;P&gt;One important observation is that the raydium driver uses&lt;/P&gt;&lt;P&gt;mipi_dsi_generic_write() to send mipi commands, which is working, while mipi_dsi_dcs_write_buffer() failed with "wait payload tx done time out" or ""wait pkthdr tx done time out" errors (in kernel log) after about four successful writes.&lt;/P&gt;&lt;P&gt;Find patches for i.MX8MM Android 10 sources below.&lt;/P&gt;&lt;P&gt;Apply with&lt;/P&gt;&lt;P&gt;cd imx-android-10/android_build/vendor/nxp-opensource/kernel_imx&lt;/P&gt;&lt;P&gt;git apply 0001-add-st7701-driver-shows-stripes-not-finished.patch&lt;/P&gt;&lt;P&gt;cd imx-android-10/android_build/device/fsl&lt;/P&gt;&lt;P&gt;git apply 0001-change-mipi-display-to-st7701.patch&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Apr 2020 21:37:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943672#M141134</guid>
      <dc:creator>nxp31</dc:creator>
      <dc:date>2020-04-12T21:37:48Z</dc:date>
    </item>
    <item>
      <title>Re: Android9.0+imx8mini mipi to lvds issue?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943673#M141135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;hello,&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;on our 8mm custom board , lt9211 driver output error log " LT9211 pcr unstable".&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;&lt;SPAN style="color: #666666; background-color: #ffffff; font-weight: normal; font-size: 13.600001335144043px;"&gt;I try to modify lt9211 drive&amp;nbsp;&lt;/SPAN&gt;Pcr_M&amp;nbsp;value&amp;nbsp; and check pcr_stable more times ,b&lt;SPAN style="color: #666666; background-color: #ffffff; font-weight: normal; font-size: 13.600001335144043px;"&gt;ut no use。&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;Have you seen the same problem?&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Apr 2020 05:35:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943673#M141135</guid>
      <dc:creator>daluotuo</dc:creator>
      <dc:date>2020-04-30T05:35:52Z</dc:date>
    </item>
    <item>
      <title>Re: Android9.0+imx8mini mipi to lvds issue?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943674#M141136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I am also debugging lt9211 recently, there is very little online information, you can share the driver of lt9211 to me？ thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 May 2020 08:07:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943674#M141136</guid>
      <dc:creator>jieh朱</dc:creator>
      <dc:date>2020-05-19T08:07:16Z</dc:date>
    </item>
    <item>
      <title>Re: Android9.0+imx8mini mipi to lvds issue?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943675#M141137</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you can write an i2c driver by referring to the microcontroller program, mainly to initialize the register.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 May 2020 08:20:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/943675#M141137</guid>
      <dc:creator>aber</dc:creator>
      <dc:date>2020-05-19T08:20:20Z</dc:date>
    </item>
    <item>
      <title>Re: Android9.0+imx8mini mipi to lvds issue?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/1294940#M175725</link>
      <description>&lt;P&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;Hello, I also encountered this problem, how did you solve it?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 19 Jun 2021 03:02:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/1294940#M175725</guid>
      <dc:creator>zhouyq</dc:creator>
      <dc:date>2021-06-19T03:02:17Z</dc:date>
    </item>
    <item>
      <title>Re: Android9.0+imx8mini mipi to lvds issue?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/1418861#M187452</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you have source code link?&lt;/P&gt;</description>
      <pubDate>Thu, 24 Feb 2022 07:15:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android9-0-imx8mini-mipi-to-lvds-issue/m-p/1418861#M187452</guid>
      <dc:creator>ziv_chen</dc:creator>
      <dc:date>2022-02-24T07:15:23Z</dc:date>
    </item>
  </channel>
</rss>