<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Device tree configuration for humidity sensor in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Device-tree-configuration-for-humidity-sensor/m-p/943515#M141115</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi devika&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at examples for sensors isl29023, mag3110 and sect.2.8 Sensors attached Linux Manual&lt;BR /&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6qdl-sabreauto.dtsi?h=imx_4.9.11_1.0.0_ga"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6qdl-sabreauto.dtsi?h=imx_4.9.11_1.0.0_ga&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Jun 2019 23:37:12 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-06-04T23:37:12Z</dc:date>
    <item>
      <title>Device tree configuration for humidity sensor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-tree-configuration-for-humidity-sensor/m-p/943514#M141114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have setup Yocto project 4.9.11_1.0.0 for imx6qpsabresd and need to add device tree configuration for temperature and humidity sensor(si7020).&lt;BR /&gt;We have added the following lines in imx6qdl-sabresd.dtsi file and also enabled si7020 as a module in kernel configuration.But it looks like the kernel module is not executing the functions after inserting it, as we are not seeing a print messages of "init/probe" functions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&amp;nbsp; adc: si7020@40 {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; compatible = "silabs,si7020";&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg = &amp;lt;0x40&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #io-channel-cells = &amp;lt;1&amp;gt;;&lt;BR /&gt;&amp;nbsp; };&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; iio-hwmon {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; compatible = "iio-hwmon";&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; io-channels = &amp;lt;&amp;amp;adc 0&amp;gt;, &amp;lt;&amp;amp;adc 1&amp;gt;, &amp;lt;&amp;amp;adc 2&amp;gt;;&lt;BR /&gt;&amp;nbsp; };&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Can you please let us know about if there is something wrong with this dts?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Devika&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Jun 2019 07:14:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-tree-configuration-for-humidity-sensor/m-p/943514#M141114</guid>
      <dc:creator>devikar</dc:creator>
      <dc:date>2019-06-04T07:14:35Z</dc:date>
    </item>
    <item>
      <title>Re: Device tree configuration for humidity sensor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-tree-configuration-for-humidity-sensor/m-p/943515#M141115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi devika&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at examples for sensors isl29023, mag3110 and sect.2.8 Sensors attached Linux Manual&lt;BR /&gt;&lt;A href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6qdl-sabreauto.dtsi?h=imx_4.9.11_1.0.0_ga"&gt;https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6qdl-sabreauto.dtsi?h=imx_4.9.11_1.0.0_ga&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Jun 2019 23:37:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-tree-configuration-for-humidity-sensor/m-p/943515#M141115</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-06-04T23:37:12Z</dc:date>
    </item>
    <item>
      <title>Re: Device tree configuration for humidity sensor</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-tree-configuration-for-humidity-sensor/m-p/943516#M141116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;Now we are able to get the print messages of probe functions as we have&amp;nbsp;enabled si7020 as built-in module in menuconfig.&lt;/P&gt;&lt;P&gt;It was not the problem with dts configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Devika&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jun 2019 10:56:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-tree-configuration-for-humidity-sensor/m-p/943516#M141116</guid>
      <dc:creator>devikar</dc:creator>
      <dc:date>2019-06-06T10:56:35Z</dc:date>
    </item>
  </channel>
</rss>