<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX6Q-SABREAUTO EVK board boot failed using Android 9</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SABREAUTO-EVK-board-boot-failed-using-Android-9/m-p/943382#M141077</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Platform: IMX6Q&lt;/P&gt;&lt;P&gt;OS: Android 9 (p9.0.0-2.2.0-ga)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As title, I tried the android 9 on IMX6Q-SABREAUTO EVK board but boot failed, it looks good before running into system, but it shows services failed when start running&amp;nbsp; zygote..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;log:&lt;/P&gt;&lt;P&gt;type=1400 audit(1562322318.470:10255): avc: denied { dac_read_search } for pid=1072 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0&lt;BR /&gt;type=1400 audit(1562322319.730:10256): avc: denied { dac_read_search } for pid=241 comm="Binder:241_4" capability=2 scontext=u:r:installd:s0 tcontext=u:r:installd:s0 tclass=capability permissive=0&lt;BR /&gt;init: Received control message 'interface_start' for 'android.hardware.sensors@1.0::ISensors/default' from pid: 190 (/system/bin/hwservicemanager)&lt;BR /&gt;init: &lt;STRONG&gt;Could not find service hosting interface android.hardware.sensors@1.0::ISensors/default&lt;/STRONG&gt;&lt;BR /&gt;init: Received control message 'interface_start' for 'android.hardware.sensors@1.0::ISensors/default' from pid: 190 (/system/bin/hwservicemanager)&lt;BR /&gt;init: Could not find service hosting interface android.hardware.sensors@1.0::ISensors/default&lt;BR /&gt;healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a&lt;BR /&gt;healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a&lt;/P&gt;&lt;P&gt;Seems the sensors service has some problem, but it also shows the same messages when I take out the sensors configuration from device/fsl/imx6dq/sabreauto_6q/sabreauto_6q.mk&lt;BR /&gt;&lt;BR /&gt;Any directions? I stocking almost one week... thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Jul 2019 10:38:36 GMT</pubDate>
    <dc:creator>mayqueen</dc:creator>
    <dc:date>2019-07-05T10:38:36Z</dc:date>
    <item>
      <title>IMX6Q-SABREAUTO EVK board boot failed using Android 9</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SABREAUTO-EVK-board-boot-failed-using-Android-9/m-p/943382#M141077</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Platform: IMX6Q&lt;/P&gt;&lt;P&gt;OS: Android 9 (p9.0.0-2.2.0-ga)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As title, I tried the android 9 on IMX6Q-SABREAUTO EVK board but boot failed, it looks good before running into system, but it shows services failed when start running&amp;nbsp; zygote..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;log:&lt;/P&gt;&lt;P&gt;type=1400 audit(1562322318.470:10255): avc: denied { dac_read_search } for pid=1072 comm="main" capability=2 scontext=u:r:zygote:s0 tcontext=u:r:zygote:s0 tclass=capability permissive=0&lt;BR /&gt;type=1400 audit(1562322319.730:10256): avc: denied { dac_read_search } for pid=241 comm="Binder:241_4" capability=2 scontext=u:r:installd:s0 tcontext=u:r:installd:s0 tclass=capability permissive=0&lt;BR /&gt;init: Received control message 'interface_start' for 'android.hardware.sensors@1.0::ISensors/default' from pid: 190 (/system/bin/hwservicemanager)&lt;BR /&gt;init: &lt;STRONG&gt;Could not find service hosting interface android.hardware.sensors@1.0::ISensors/default&lt;/STRONG&gt;&lt;BR /&gt;init: Received control message 'interface_start' for 'android.hardware.sensors@1.0::ISensors/default' from pid: 190 (/system/bin/hwservicemanager)&lt;BR /&gt;init: Could not find service hosting interface android.hardware.sensors@1.0::ISensors/default&lt;BR /&gt;healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a&lt;BR /&gt;healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a&lt;/P&gt;&lt;P&gt;Seems the sensors service has some problem, but it also shows the same messages when I take out the sensors configuration from device/fsl/imx6dq/sabreauto_6q/sabreauto_6q.mk&lt;BR /&gt;&lt;BR /&gt;Any directions? I stocking almost one week... thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2019 10:38:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SABREAUTO-EVK-board-boot-failed-using-Android-9/m-p/943382#M141077</guid>
      <dc:creator>mayqueen</dc:creator>
      <dc:date>2019-07-05T10:38:36Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6Q-SABREAUTO EVK board boot failed using Android 9</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SABREAUTO-EVK-board-boot-failed-using-Android-9/m-p/943383#M141078</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello May,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; For i.MX6Q, use android 8.0 BSP, please!&amp;nbsp;&amp;nbsp; Android 9.0 does't support i.MX6Q.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope above information can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;BR /&gt;BR,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jul 2019 07:56:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6Q-SABREAUTO-EVK-board-boot-failed-using-Android-9/m-p/943383#M141078</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2019-07-08T07:56:05Z</dc:date>
    </item>
  </channel>
</rss>