<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: CAN Communication</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/CAN-Communication/m-p/218456#M14094</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only reason the example asks you to modify the code is that, later, when you run the different binaries on the target you can verify that all methods work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the projects you mention&amp;nbsp;&lt;SPAN&gt;libsocketcan and canutils you can follow page 45 of the presentation to compile them.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Renato&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Apr 2012 18:54:33 GMT</pubDate>
    <dc:creator>Frias</dc:creator>
    <dc:date>2012-04-23T18:54:33Z</dc:date>
    <item>
      <title>CAN Communication</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CAN-Communication/m-p/218455#M14093</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;There are couple of questions about the building the can communications. I used the LTIBII method to build the helloworld, i tried doing the same thing for libsocketcan and canutils but i am missing the make file. in the ltib method, it says extract the source files to rpm/BUILD, the source files for the canutil and libsocketcan have .c and header files, do i move there all there? (the files that i got came from the /freescale/pkgs). and there is a line in there saying modify the code, which code are you refering to and what needs to be modified?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;UVic&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 10 Mar 2012 21:59:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CAN-Communication/m-p/218455#M14093</guid>
      <dc:creator>UVicEcoCar2</dc:creator>
      <dc:date>2012-03-10T21:59:09Z</dc:date>
    </item>
    <item>
      <title>Re: CAN Communication</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CAN-Communication/m-p/218456#M14094</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only reason the example asks you to modify the code is that, later, when you run the different binaries on the target you can verify that all methods work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the projects you mention&amp;nbsp;&lt;SPAN&gt;libsocketcan and canutils you can follow page 45 of the presentation to compile them.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Renato&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Apr 2012 18:54:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CAN-Communication/m-p/218456#M14094</guid>
      <dc:creator>Frias</dc:creator>
      <dc:date>2012-04-23T18:54:33Z</dc:date>
    </item>
  </channel>
</rss>