<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Connect USB 3.0 camera</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Connect-USB-3-0-camera/m-p/941382#M140859</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Hector,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The message&lt;/P&gt;&lt;PRE&gt;&lt;EM&gt;usb 2-1: new SuperSpeed USB device number 2 using xhci-hcd


&lt;/EM&gt;&lt;/PRE&gt;&lt;P&gt;Means that is recognized, just mount the USB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Oct 2019 14:42:19 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2019-10-08T14:42:19Z</dc:date>
    <item>
      <title>Connect USB 3.0 camera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Connect-USB-3-0-camera/m-p/941381#M140858</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to connect a USB camera to the&amp;nbsp;MCIMX8M-EVK, but it does not recognise it. The only thing that appears is:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE&gt;&lt;EM&gt;usb 2-1: new SuperSpeed USB device number 2 using xhci-hcd&lt;/EM&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But no further messages of detection are shown. Is there any specific Linux image I can use to make it work? I have tried with L4.9.88_2.0.0_images_MX8MQ.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank you in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Oct 2019 10:19:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Connect-USB-3-0-camera/m-p/941381#M140858</guid>
      <dc:creator>hmartinez</dc:creator>
      <dc:date>2019-10-03T10:19:05Z</dc:date>
    </item>
    <item>
      <title>Re: Connect USB 3.0 camera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Connect-USB-3-0-camera/m-p/941382#M140859</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Hector,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The message&lt;/P&gt;&lt;PRE&gt;&lt;EM&gt;usb 2-1: new SuperSpeed USB device number 2 using xhci-hcd


&lt;/EM&gt;&lt;/PRE&gt;&lt;P&gt;Means that is recognized, just mount the USB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Oct 2019 14:42:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Connect-USB-3-0-camera/m-p/941382#M140859</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2019-10-08T14:42:19Z</dc:date>
    </item>
  </channel>
</rss>