<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Change pins Drive strength runtime</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Change-pins-Drive-strength-runtime/m-p/940646#M140770</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nirmal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid it is not supported in nxp linux bsps, one can try to write to iomux&lt;/P&gt;&lt;P&gt;registers directly from application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Sep 2019 09:45:29 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-09-18T09:45:29Z</dc:date>
    <item>
      <title>Change pins Drive strength runtime</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Change-pins-Drive-strength-runtime/m-p/940645#M140769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Release: Yocto-Sumo (4.14.78_1.0.0_GA)&lt;/P&gt;&lt;P&gt;Board: i.MX8MQ based custom board&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to change pins drive strength runtime without board reboot.&lt;/P&gt;&lt;P&gt;Is it possible to do it? If yes, then what utility or steps I have to follow?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Nirmal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Sep 2019 08:50:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Change-pins-Drive-strength-runtime/m-p/940645#M140769</guid>
      <dc:creator>nirmalluhana</dc:creator>
      <dc:date>2019-09-18T08:50:13Z</dc:date>
    </item>
    <item>
      <title>Re: Change pins Drive strength runtime</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Change-pins-Drive-strength-runtime/m-p/940646#M140770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nirmal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid it is not supported in nxp linux bsps, one can try to write to iomux&lt;/P&gt;&lt;P&gt;registers directly from application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Sep 2019 09:45:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Change-pins-Drive-strength-runtime/m-p/940646#M140770</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-09-18T09:45:29Z</dc:date>
    </item>
    <item>
      <title>Re: Change pins Drive strength runtime</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Change-pins-Drive-strength-runtime/m-p/940647#M140771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV class=""&gt;&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your rapid response.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you please provide more information which application is used for it?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Nirmal&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Sep 2019 10:10:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Change-pins-Drive-strength-runtime/m-p/940647#M140771</guid>
      <dc:creator>nirmalluhana</dc:creator>
      <dc:date>2019-09-18T10:10:14Z</dc:date>
    </item>
    <item>
      <title>Re: Change pins Drive strength runtime</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Change-pins-Drive-strength-runtime/m-p/940648#M140772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nirmal&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;there is no special application for it. One can use for example&lt;/P&gt;&lt;P&gt;memtool for adding codes to custom application :&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/imx-test/tree/test/memtool?h=imx_4.14.98_2.1.0" title="https://source.codeaurora.org/external/imx/imx-test/tree/test/memtool?h=imx_4.14.98_2.1.0"&gt;memtool\test - imx-test - i.MX Driver Test Application Software&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Sep 2019 10:29:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Change-pins-Drive-strength-runtime/m-p/940648#M140772</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-09-18T10:29:14Z</dc:date>
    </item>
  </channel>
</rss>