<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX8 RNDIS USB Reset issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-RNDIS-USB-Reset-issue/m-p/940553#M140761</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Experts,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We tried to use the RNDIS mode device with iMX8 platform through USB port. The device is getting re-enumerated again and USB trace logs shows it that Reset is issued by USB host.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please suggest method to debug the same.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Sep 2019 06:43:46 GMT</pubDate>
    <dc:creator>lyfsci</dc:creator>
    <dc:date>2019-09-18T06:43:46Z</dc:date>
    <item>
      <title>iMX8 RNDIS USB Reset issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-RNDIS-USB-Reset-issue/m-p/940553#M140761</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Experts,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We tried to use the RNDIS mode device with iMX8 platform through USB port. The device is getting re-enumerated again and USB trace logs shows it that Reset is issued by USB host.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please suggest method to debug the same.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Sep 2019 06:43:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8-RNDIS-USB-Reset-issue/m-p/940553#M140761</guid>
      <dc:creator>lyfsci</dc:creator>
      <dc:date>2019-09-18T06:43:46Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8 RNDIS USB Reset issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-RNDIS-USB-Reset-issue/m-p/940554#M140762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lyf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try with usb unit tests&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_usb_test?h=imx_4.19.35_1.0.0" title="https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_usb_test?h=imx_4.19.35_1.0.0"&gt;mxc_usb_test\test - imx-test - i.MX Driver Test Application Software&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;for debugging, usb driver is described in &lt;A class="" href="https://www.nxp.com/webapp/Download?colCode=L4.19.35_1.0.0_LINUX_DOC" target="_blank"&gt;Documentation&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Sep 2019 07:32:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8-RNDIS-USB-Reset-issue/m-p/940554#M140762</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-09-18T07:32:54Z</dc:date>
    </item>
  </channel>
</rss>