<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Watchdog on imx</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Watchdog-on-imx/m-p/940176#M140740</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is safe also in u-boot ? Is it possible in u-boot to use the GPIO outpout from the watchdog ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 18 Oct 2019 11:51:13 GMT</pubDate>
    <dc:creator>matt67</dc:creator>
    <dc:date>2019-10-18T11:51:13Z</dc:date>
    <item>
      <title>Watchdog on imx</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Watchdog-on-imx/m-p/940174#M140738</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;What do you think of using the imx internal watchdog timer with&amp;nbsp;fsl,ext-reset-output dts property to output reset signal to PMIC ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it safe enough, and guaranteed that the&amp;nbsp;Low frequency reference clock feeding the WDOG block doesn't stop in case of hanging ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or perhaps should I use an hardware reset handler ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Oct 2019 08:30:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Watchdog-on-imx/m-p/940174#M140738</guid>
      <dc:creator>matt67</dc:creator>
      <dc:date>2019-10-18T08:30:53Z</dc:date>
    </item>
    <item>
      <title>Re: Watchdog on imx</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Watchdog-on-imx/m-p/940175#M140739</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi matt67&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes using internal watchdog to reset pmic is fine solution and it is safe.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Oct 2019 09:54:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Watchdog-on-imx/m-p/940175#M140739</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-10-18T09:54:31Z</dc:date>
    </item>
    <item>
      <title>Re: Watchdog on imx</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Watchdog-on-imx/m-p/940176#M140740</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is safe also in u-boot ? Is it possible in u-boot to use the GPIO outpout from the watchdog ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Oct 2019 11:51:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Watchdog-on-imx/m-p/940176#M140740</guid>
      <dc:creator>matt67</dc:creator>
      <dc:date>2019-10-18T11:51:13Z</dc:date>
    </item>
    <item>
      <title>Re: Watchdog on imx</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Watchdog-on-imx/m-p/940177#M140741</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi matt67&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;yes it is safe also in u-boot.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Oct 2019 13:16:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Watchdog-on-imx/m-p/940177#M140741</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-10-18T13:16:42Z</dc:date>
    </item>
  </channel>
</rss>