<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX8MQ: compatible LPDDR4 devices?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-compatible-LPDDR4-devices/m-p/939260#M140641</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm running into trouble finding Micron memory for an IMX8MQ design. I have used the same part ( MT53E768M32D4DT-053 WT:E ) which is on the IMX8MQ EVK board but this isn't available anywhere. The same goes for any LPDDR device from Micron with a similar capacity (2GB to 4GB; I don't care right now). Are there any alternatives out there which are available?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Oct 2019 11:48:31 GMT</pubDate>
    <dc:creator>N_Coesel</dc:creator>
    <dc:date>2019-10-02T11:48:31Z</dc:date>
    <item>
      <title>IMX8MQ: compatible LPDDR4 devices?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-compatible-LPDDR4-devices/m-p/939260#M140641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm running into trouble finding Micron memory for an IMX8MQ design. I have used the same part ( MT53E768M32D4DT-053 WT:E ) which is on the IMX8MQ EVK board but this isn't available anywhere. The same goes for any LPDDR device from Micron with a similar capacity (2GB to 4GB; I don't care right now). Are there any alternatives out there which are available?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Oct 2019 11:48:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-compatible-LPDDR4-devices/m-p/939260#M140641</guid>
      <dc:creator>N_Coesel</dc:creator>
      <dc:date>2019-10-02T11:48:31Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MQ: compatible LPDDR4 devices?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-compatible-LPDDR4-devices/m-p/939261#M140642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nico&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;file was sent via mail.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Oct 2019 23:20:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-compatible-LPDDR4-devices/m-p/939261#M140642</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-10-02T23:20:53Z</dc:date>
    </item>
  </channel>
</rss>