<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX 6,7,8 support USB device mode support to UVC in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-6-7-8-support-USB-device-mode-support-to-UVC/m-p/938705#M140594</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm checking the i.MX material and wants to know is i.MX 6,7,8 support USB device mode&amp;nbsp;support to&amp;nbsp;UVC and can connect to PC USB port as camera?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Jul 2019 10:13:52 GMT</pubDate>
    <dc:creator>sean4</dc:creator>
    <dc:date>2019-07-18T10:13:52Z</dc:date>
    <item>
      <title>i.MX 6,7,8 support USB device mode support to UVC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-6-7-8-support-USB-device-mode-support-to-UVC/m-p/938705#M140594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm checking the i.MX material and wants to know is i.MX 6,7,8 support USB device mode&amp;nbsp;support to&amp;nbsp;UVC and can connect to PC USB port as camera?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jul 2019 10:13:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-6-7-8-support-USB-device-mode-support-to-UVC/m-p/938705#M140594</guid>
      <dc:creator>sean4</dc:creator>
      <dc:date>2019-07-18T10:13:52Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 6,7,8 support USB device mode support to UVC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-6-7-8-support-USB-device-mode-support-to-UVC/m-p/938706#M140595</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Vencer,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Correct!!! all MX6, MX7 MX8 support UVC. Please read The USB certification:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-105609"&gt;I.MX6 series USB Certification Guides&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jul 2019 17:07:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-6-7-8-support-USB-device-mode-support-to-UVC/m-p/938706#M140595</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2019-07-18T17:07:39Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 6,7,8 support USB device mode support to UVC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-6-7-8-support-USB-device-mode-support-to-UVC/m-p/938707#M140596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your reply. I check the USB certification and only can find iMX6 as host and test with&amp;nbsp;Logitech QuickCam. Could you please teach me where to find the&amp;nbsp;&lt;STRONG&gt;iMX6 as&amp;nbsp;USB device&lt;/STRONG&gt; (Camera)&amp;nbsp;to connect with PC. Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vencer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jul 2019 01:31:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-6-7-8-support-USB-device-mode-support-to-UVC/m-p/938707#M140596</guid>
      <dc:creator>sean4</dc:creator>
      <dc:date>2019-07-19T01:31:25Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 6,7,8 support USB device mode support to UVC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-6-7-8-support-USB-device-mode-support-to-UVC/m-p/938708#M140597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For i.MX6 you need to enable the g_webcam driver in the kernel however, this gadget driver requires a user space application to finish the enumeration and attend the USB requests. You might need something like this in order to get it working on i.MX6:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://developer.ridgerun.com/wiki/index.php?title=USB_Video_Class_Gadget_Library_-_libguvc" title="https://developer.ridgerun.com/wiki/index.php?title=USB_Video_Class_Gadget_Library_-_libguvc"&gt;USB Video Class Gadget Library | UVC Driver Linux | UVC Linux&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.ridgerun.com"&gt;www.ridgerun.com&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jul 2019 19:43:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-6-7-8-support-USB-device-mode-support-to-UVC/m-p/938708#M140597</guid>
      <dc:creator>marcomadrigal</dc:creator>
      <dc:date>2019-07-23T19:43:39Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 6,7,8 support USB device mode support to UVC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-6-7-8-support-USB-device-mode-support-to-UVC/m-p/938709#M140598</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to do the same - attach a MIPI camera to an i.MX6 MCU, and present a UVC interface to the USB.&lt;/P&gt;&lt;P&gt;I looked for UVC within the MCUXpresso peripheral configuration for the USB Middleware, and was disappointed to find this is not a supported class.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I presume this is the same functionality provided by the Ridgerun UVC Gadget Library, but $2500 license fee means I'll be dropping the iMX6 as an option for this project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my opinion, it's pretty ludicrous to provide a device with heavy processing power, a camera interface ideal for streaming, and then ignore the obvious STANDARD defined to complete the stream.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Robb.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jun 2020 11:56:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-6-7-8-support-USB-device-mode-support-to-UVC/m-p/938709#M140598</guid>
      <dc:creator>rmain_mws</dc:creator>
      <dc:date>2020-06-03T11:56:43Z</dc:date>
    </item>
  </channel>
</rss>