<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Creating a bootable image in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Creating-a-bootable-image/m-p/938568#M140583</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am following the document &lt;A href="https://community.nxp.com/docs/DOC-343178"&gt;i.MX8 Boot process and creating a bootable image&lt;/A&gt; to create a bootable image for&amp;nbsp; MCIMX8M-EVK. I think I already have all I need to create one, but I am not sure which SCFW is suitable for my purpose because there are several variants in imx-sc-firmware.1.2 without any descriptions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/88095i2FDA5B51D7B41497/image-size/large?v=v2&amp;amp;px=999" title="Selection_441.png" alt="Selection_441.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could anyone tell me which one I should use?&lt;/P&gt;&lt;P&gt;Then I guess I also need&amp;nbsp; to rename it to scfw_tcm.bin to make the image. Is that correct procedure?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Jun 2019 08:52:34 GMT</pubDate>
    <dc:creator>ken1_saito</dc:creator>
    <dc:date>2019-06-18T08:52:34Z</dc:date>
    <item>
      <title>Creating a bootable image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Creating-a-bootable-image/m-p/938568#M140583</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am following the document &lt;A href="https://community.nxp.com/docs/DOC-343178"&gt;i.MX8 Boot process and creating a bootable image&lt;/A&gt; to create a bootable image for&amp;nbsp; MCIMX8M-EVK. I think I already have all I need to create one, but I am not sure which SCFW is suitable for my purpose because there are several variants in imx-sc-firmware.1.2 without any descriptions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/88095i2FDA5B51D7B41497/image-size/large?v=v2&amp;amp;px=999" title="Selection_441.png" alt="Selection_441.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could anyone tell me which one I should use?&lt;/P&gt;&lt;P&gt;Then I guess I also need&amp;nbsp; to rename it to scfw_tcm.bin to make the image. Is that correct procedure?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jun 2019 08:52:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Creating-a-bootable-image/m-p/938568#M140583</guid>
      <dc:creator>ken1_saito</dc:creator>
      <dc:date>2019-06-18T08:52:34Z</dc:date>
    </item>
    <item>
      <title>Re: Creating a bootable image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Creating-a-bootable-image/m-p/938569#M140584</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ken,&lt;/P&gt;&lt;P&gt;If you are using a MCIMX8M-EVK board, it includes a i.MX8&lt;STRONG&gt;M&lt;/STRONG&gt; processor (4x Cortex-A53), which does not have the SCU (so, no SCFW is required).&lt;/P&gt;&lt;P&gt;The SCU-SCFW is for i.MX8&lt;STRONG&gt;QM&lt;/STRONG&gt; (2x Cortex-A72 + 4x Cortex-A53) and i.MX&lt;STRONG&gt;8X&lt;/STRONG&gt; (4x Cortex-A35) processors &amp;nbsp;and their MEK boards.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jun 2019 02:08:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Creating-a-bootable-image/m-p/938569#M140584</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2019-06-19T02:08:34Z</dc:date>
    </item>
    <item>
      <title>Re: Creating a bootable image</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Creating-a-bootable-image/m-p/938570#M140585</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;Thanks for your help. Yes, you are right. I thought "Q" in i.MX8QM&amp;nbsp;stands for Quad. Now I understand they are totally different.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ken&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jun 2019 04:25:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Creating-a-bootable-image/m-p/938570#M140585</guid>
      <dc:creator>ken1_saito</dc:creator>
      <dc:date>2019-06-19T04:25:48Z</dc:date>
    </item>
  </channel>
</rss>