<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: PPP connection failed in yocto</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PPP-connection-failed-in-yocto/m-p/938310#M140555</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please ensure antenna is properly connected and your quectel_chat_connect file is as in the attachment below&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Sep 2019 07:23:19 GMT</pubDate>
    <dc:creator>sujay1</dc:creator>
    <dc:date>2019-09-04T07:23:19Z</dc:date>
    <item>
      <title>PPP connection failed in yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PPP-connection-failed-in-yocto/m-p/938308#M140553</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Currently, the yocto system needs to be run on imx6q, which needs to support 4g function and use the Quectel ec20 module. When dialing with PPPD, no matter how you modify it, it fails.&lt;/P&gt;&lt;P&gt;The module validates properly and the other attempt to integrate wvdial fails, both of which are successful on debian.&lt;/P&gt;&lt;P&gt;Is there any success at yocto? Or any idea. Thank you&lt;/P&gt;&lt;P&gt;Here is the dial script&lt;/P&gt;&lt;P&gt;====================================&lt;/P&gt;&lt;P&gt;debug&lt;/P&gt;&lt;P&gt;nodetach&lt;/P&gt;&lt;P&gt;/dev/ttyUSB2&lt;/P&gt;&lt;P&gt;115200&lt;/P&gt;&lt;P&gt;usepeerdns&lt;/P&gt;&lt;P&gt;noauth&lt;/P&gt;&lt;P&gt;local&lt;/P&gt;&lt;P&gt;novj&lt;/P&gt;&lt;P&gt;novjccomp&lt;/P&gt;&lt;P&gt;noccp&lt;/P&gt;&lt;P&gt;defaultroute&lt;/P&gt;&lt;P&gt;user "cmnet"&lt;/P&gt;&lt;P&gt;0.0.0.0:0.0.0.0&lt;/P&gt;&lt;P&gt;refuse-chap&lt;BR /&gt;refuse-mschap&lt;BR /&gt;refuse-mschap-v2&lt;/P&gt;&lt;P&gt;connect '/usr/bin/chat -s -v -f /etc/ppp/connect'&lt;/P&gt;&lt;P&gt;======================================&lt;/P&gt;&lt;P&gt;TIMEOUT 5&lt;/P&gt;&lt;P&gt;ABORT 'NO CARRIER'&lt;/P&gt;&lt;P&gt;ABORT 'ERROR'&lt;/P&gt;&lt;P&gt;ABORT 'NODIALTONE'&lt;/P&gt;&lt;P&gt;ABORT 'BUSY'&lt;/P&gt;&lt;P&gt;ABORT 'NO ANSWER'&lt;/P&gt;&lt;P&gt;'' \rAT&lt;/P&gt;&lt;P&gt;OK \rATZ&lt;/P&gt;&lt;P&gt;OK \rAT+CGDCONT=1,"IP","3GNET",,0,0&lt;/P&gt;&lt;P&gt;OK-AT-OK ATDT*99#&lt;/P&gt;&lt;P&gt;CONNECT \d\c&lt;/P&gt;&lt;P&gt;==================================================&lt;/P&gt;&lt;P&gt;result&amp;nbsp;&lt;/P&gt;&lt;P&gt;root@imx6qsabresd:~# pppd call wcdma &amp;amp;&lt;BR /&gt;[1] 702&lt;BR /&gt;root@imx6qsabresd:~# timeout set to 5 seconds&lt;BR /&gt;abort on (NO CARRIER)&lt;BR /&gt;abort on (ERROR)&lt;BR /&gt;abort on (NODIALTONE)&lt;BR /&gt;abort on (BUSY)&lt;BR /&gt;abort on (NO ANSWER)&lt;BR /&gt;send (^MAT^M)&lt;BR /&gt;expect (OK)&lt;BR /&gt;AT^M^M&lt;BR /&gt;OK&lt;BR /&gt; -- got it&lt;/P&gt;&lt;P&gt;send (^MATZ^M)&lt;BR /&gt;expect (OK)&lt;BR /&gt;^M&lt;BR /&gt;ATZ^M^M&lt;BR /&gt;OK&lt;BR /&gt; -- got it&lt;/P&gt;&lt;P&gt;send (^MAT+CGDCONT=1,"IP","3GNET",,0,0^M)&lt;BR /&gt;expect (OK)&lt;BR /&gt;^M&lt;BR /&gt;AT+CGDCONT=1,"IP","3GNET",,0,0^M^M&lt;BR /&gt;OK&lt;BR /&gt; -- got it&lt;/P&gt;&lt;P&gt;send (ATDT*99#^M)&lt;BR /&gt;expect (CONNECT)&lt;BR /&gt;^M&lt;BR /&gt;ATDT*99#^M^M&lt;BR /&gt;CONNECT&lt;BR /&gt; -- got it&lt;/P&gt;&lt;P&gt;send (\d)&lt;BR /&gt;Script /usr/bin/chat -s -v -f /etc/ppp/connect finished (pid 703), status = 0x0&lt;BR /&gt;Serial connection established.&lt;BR /&gt;using channel 4&lt;BR /&gt;Using interface ppp0&lt;BR /&gt;Connect: ppp0 &amp;lt;--&amp;gt; /dev/ttyUSB2&lt;BR /&gt;Warning - secret file /etc/ppp/pap-secrets has world and/or group access&lt;BR /&gt;sent [LCP ConfReq id=0x1 &amp;lt;asyncmap 0x0&amp;gt; &amp;lt;magic 0x934f19f6&amp;gt; &amp;lt;pcomp&amp;gt; &amp;lt;accomp&amp;gt;]&lt;BR /&gt;rcvd [LCP ConfReq id=0x9 &amp;lt;asyncmap 0x0&amp;gt; &amp;lt;auth chap MD5&amp;gt; &amp;lt;magic 0xd10c05a6&amp;gt; &amp;lt;pcomp&amp;gt; &amp;lt;accomp&amp;gt;]&lt;BR /&gt;sent [LCP ConfNak id=0x9 &amp;lt;auth pap&amp;gt;]&lt;BR /&gt;rcvd [LCP ConfAck id=0x1 &amp;lt;asyncmap 0x0&amp;gt; &amp;lt;magic 0x934f19f6&amp;gt; &amp;lt;pcomp&amp;gt; &amp;lt;accomp&amp;gt;]&lt;BR /&gt;rcvd [LCP ConfReq id=0xa &amp;lt;asyncmap 0x0&amp;gt; &amp;lt;auth pap&amp;gt; &amp;lt;magic 0xd10c05a6&amp;gt; &amp;lt;pcomp&amp;gt; &amp;lt;accomp&amp;gt;]&lt;BR /&gt;sent [LCP ConfAck id=0xa &amp;lt;asyncmap 0x0&amp;gt; &amp;lt;auth pap&amp;gt; &amp;lt;magic 0xd10c05a6&amp;gt; &amp;lt;pcomp&amp;gt; &amp;lt;accomp&amp;gt;]&lt;BR /&gt;sent [LCP EchoReq id=0x0 magic=0x934f19f6]&lt;BR /&gt;Warning - secret file /etc/ppp/pap-secrets has world and/or group access&lt;BR /&gt;sent [PAP AuthReq id=0x1 user="cmnet" password=&amp;lt;hidden&amp;gt;]&lt;BR /&gt;rcvd [LCP DiscReq id=0xb magic=0xd10c05a6]&lt;BR /&gt;rcvd [LCP EchoRep id=0x0 magic=0xd10c05a6 93 4f 19 f6]&lt;BR /&gt;rcvd [PAP AuthAck id=0x1 ""]&lt;BR /&gt;PAP authentication succeeded&lt;BR /&gt;sent [IPCP ConfReq id=0x1 &amp;lt;addr 0.0.0.0&amp;gt; &amp;lt;ms-dns1 0.0.0.0&amp;gt; &amp;lt;ms-dns2 0.0.0.0&amp;gt;]&lt;BR /&gt;sent [IPCP ConfReq id=0x1 &amp;lt;addr 0.0.0.0&amp;gt; &amp;lt;ms-dns1 0.0.0.0&amp;gt; &amp;lt;ms-dns2 0.0.0.0&amp;gt;]&lt;BR /&gt;sent [IPCP ConfReq id=0x1 &amp;lt;addr 0.0.0.0&amp;gt; &amp;lt;ms-dns1 0.0.0.0&amp;gt; &amp;lt;ms-dns2 0.0.0.0&amp;gt;]&lt;BR /&gt;sent [IPCP ConfReq id=0x1 &amp;lt;addr 0.0.0.0&amp;gt; &amp;lt;ms-dns1 0.0.0.0&amp;gt; &amp;lt;ms-dns2 0.0.0.0&amp;gt;]&lt;BR /&gt;sent [IPCP ConfReq id=0x1 &amp;lt;addr 0.0.0.0&amp;gt; &amp;lt;ms-dns1 0.0.0.0&amp;gt; &amp;lt;ms-dns2 0.0.0.0&amp;gt;]&lt;BR /&gt;sent [IPCP ConfReq id=0x1 &amp;lt;addr 0.0.0.0&amp;gt; &amp;lt;ms-dns1 0.0.0.0&amp;gt; &amp;lt;ms-dns2 0.0.0.0&amp;gt;]&lt;BR /&gt;sent [IPCP ConfReq id=0x1 &amp;lt;addr 0.0.0.0&amp;gt; &amp;lt;ms-dns1 0.0.0.0&amp;gt; &amp;lt;ms-dns2 0.0.0.0&amp;gt;]&lt;BR /&gt;sent [IPCP ConfReq id=0x1 &amp;lt;addr 0.0.0.0&amp;gt; &amp;lt;ms-dns1 0.0.0.0&amp;gt; &amp;lt;ms-dns2 0.0.0.0&amp;gt;]&lt;BR /&gt;sent [IPCP ConfReq id=0x1 &amp;lt;addr 0.0.0.0&amp;gt; &amp;lt;ms-dns1 0.0.0.0&amp;gt; &amp;lt;ms-dns2 0.0.0.0&amp;gt;]&lt;BR /&gt;sent [IPCP ConfReq id=0x1 &amp;lt;addr 0.0.0.0&amp;gt; &amp;lt;ms-dns1 0.0.0.0&amp;gt; &amp;lt;ms-dns2 0.0.0.0&amp;gt;]&lt;BR /&gt;sent [LCP EchoReq id=0x1 magic=0x934f19f6]&lt;BR /&gt;IPCP: timeout sending Config-Requests&lt;BR /&gt;sent [LCP TermReq id=0x2 "No network protocols running"]&lt;BR /&gt;sent [LCP TermReq id=0x3 "No network protocols running"]&lt;BR /&gt;Connection terminated.&lt;BR /&gt;Modem hangup&lt;/P&gt;&lt;P&gt;[1]+ Done(16) pppd call wcdma&lt;/P&gt;&lt;P&gt;================================================&lt;/P&gt;&lt;P&gt;Any Suggestions, thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Sep 2019 07:29:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PPP-connection-failed-in-yocto/m-p/938308#M140553</guid>
      <dc:creator>fu_qiang</dc:creator>
      <dc:date>2019-09-03T07:29:24Z</dc:date>
    </item>
    <item>
      <title>Re: PPP connection failed in yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PPP-connection-failed-in-yocto/m-p/938309#M140554</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually Config-Requests timeout usually means failed negotiation.&lt;BR /&gt;Please try to play with compression protocol and other configuration.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Sep 2019 05:13:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PPP-connection-failed-in-yocto/m-p/938309#M140554</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2019-09-04T05:13:58Z</dc:date>
    </item>
    <item>
      <title>Re: PPP connection failed in yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PPP-connection-failed-in-yocto/m-p/938310#M140555</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please ensure antenna is properly connected and your quectel_chat_connect file is as in the attachment below&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Sep 2019 07:23:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PPP-connection-failed-in-yocto/m-p/938310#M140555</guid>
      <dc:creator>sujay1</dc:creator>
      <dc:date>2019-09-04T07:23:19Z</dc:date>
    </item>
    <item>
      <title>Re: PPP connection failed in yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PPP-connection-failed-in-yocto/m-p/938311#M140556</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your answer, the method used before is to compile PPP source code into the system, I do not know what caused the error. Now add IMAGE_INSTALL_append = "PPP" in conf file, use the system to provide PPP service, can dial normally&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Sep 2019 09:54:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PPP-connection-failed-in-yocto/m-p/938311#M140556</guid>
      <dc:creator>fu_qiang</dc:creator>
      <dc:date>2019-09-25T09:54:39Z</dc:date>
    </item>
  </channel>
</rss>