<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: imx7ulpevk memory</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx7ulpevk-memory/m-p/937972#M140512</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ka-Yi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at i.MX7D example, without rpmsg_reserved :&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx7d.dtsi?h=imx_4.14.78_1.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx7d.dtsi?h=imx_4.14.78_1.0.0_ga"&gt;imx7d.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Oct 2019 10:14:32 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-10-02T10:14:32Z</dc:date>
    <item>
      <title>imx7ulpevk memory</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7ulpevk-memory/m-p/937969#M140509</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;I have a imx7ulpevk board. I changed the on board DRAM with a 4Gb LPDDR3.&amp;nbsp; I would like to test the memory as much as I can from the A7 CPU core. When I boot up the A7 core with Linux, I found there are some space seems to be reserved for the M4 or for A7/M4 communication . If this is true, is there any method to change? Will it work if I delete the rpmsg reserved memory in the dtsi file?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ka-Yi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Oct 2019 06:31:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7ulpevk-memory/m-p/937969#M140509</guid>
      <dc:creator>kayiyeh</dc:creator>
      <dc:date>2019-10-02T06:31:51Z</dc:date>
    </item>
    <item>
      <title>Re: imx7ulpevk memory</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7ulpevk-memory/m-p/937970#M140510</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ka-Yi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes one can try to delete reserved memory in dts file, it should work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Oct 2019 07:47:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7ulpevk-memory/m-p/937970#M140510</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-10-02T07:47:05Z</dc:date>
    </item>
    <item>
      <title>Re: imx7ulpevk memory</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7ulpevk-memory/m-p/937971#M140511</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Igor,&lt;/P&gt;&lt;P&gt;Thank you for your quick response. When I modified the imx7ulp.dtsi as attached then copy back to :&lt;/P&gt;&lt;P&gt;work/imx7ulpevk-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/arch/arm/dts/imx7ulp.dtsi&lt;/P&gt;&lt;P&gt;it seems fine to bitbake but the result turns out the same. Did I modify the wrong file?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ka-Yi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Oct 2019 08:40:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7ulpevk-memory/m-p/937971#M140511</guid>
      <dc:creator>kayiyeh</dc:creator>
      <dc:date>2019-10-02T08:40:46Z</dc:date>
    </item>
    <item>
      <title>Re: imx7ulpevk memory</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx7ulpevk-memory/m-p/937972#M140512</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ka-Yi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at i.MX7D example, without rpmsg_reserved :&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx7d.dtsi?h=imx_4.14.78_1.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx7d.dtsi?h=imx_4.14.78_1.0.0_ga"&gt;imx7d.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Oct 2019 10:14:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx7ulpevk-memory/m-p/937972#M140512</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-10-02T10:14:32Z</dc:date>
    </item>
  </channel>
</rss>