<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX6 failed DRAM address decode</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-failed-DRAM-address-decode/m-p/936671#M140342</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are making a product with i.MX6S. However, In rare case, we are encountering DDR accessing error.&lt;BR /&gt;therefore, we would like to identify failing point in DRAM chip for quality point of view.&lt;/P&gt;&lt;P&gt;It is need the failed address convert to ROW-COLUMN-BANK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to description from table 45-5 in reference manual rev 4, 07/2018.&lt;/P&gt;&lt;P&gt;Accessing address is able to decode by following&amp;nbsp;mapping table.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/84163iE9D07B3BC4CEC307/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If we encountered access error at 0x12001240, we can identify failing point as following table. Is it right?&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_4.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/83911iA6B13C49777A2159/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is our error log getting from DDR stress test tool.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;============================================&lt;BR /&gt; DDR configuration&lt;BR /&gt;BOOT_CFG3[5-4]: 0x00, Single DDR channel.&lt;BR /&gt;DDR type is DDR3&lt;BR /&gt;Data width: 32, bank num: 8&lt;BR /&gt;Row size: 13, col size: 10&lt;BR /&gt;Chip select CSD0 is used&lt;BR /&gt;Density per chip select: 256MB&lt;BR /&gt;============================================&lt;BR /&gt;DDR Stress Test Iteration 1&lt;BR /&gt;Current Temperature: 46&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;DDR Freq: 396 MHz&lt;BR /&gt;t0.1: data is addr test&lt;BR /&gt;&lt;STRONG&gt;Address of failure(step2): 0x12001240&lt;/STRONG&gt;&lt;BR /&gt;Data was: 0x52001240&lt;BR /&gt;But pattern should match address&lt;BR /&gt;Error: failed to run stress test!!!&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Kazuma Sasaki.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Aug 2019 01:27:06 GMT</pubDate>
    <dc:creator>Kazuma_Sasaki</dc:creator>
    <dc:date>2019-08-01T01:27:06Z</dc:date>
    <item>
      <title>i.MX6 failed DRAM address decode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-failed-DRAM-address-decode/m-p/936671#M140342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are making a product with i.MX6S. However, In rare case, we are encountering DDR accessing error.&lt;BR /&gt;therefore, we would like to identify failing point in DRAM chip for quality point of view.&lt;/P&gt;&lt;P&gt;It is need the failed address convert to ROW-COLUMN-BANK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to description from table 45-5 in reference manual rev 4, 07/2018.&lt;/P&gt;&lt;P&gt;Accessing address is able to decode by following&amp;nbsp;mapping table.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/84163iE9D07B3BC4CEC307/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If we encountered access error at 0x12001240, we can identify failing point as following table. Is it right?&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_4.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/83911iA6B13C49777A2159/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is our error log getting from DDR stress test tool.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;============================================&lt;BR /&gt; DDR configuration&lt;BR /&gt;BOOT_CFG3[5-4]: 0x00, Single DDR channel.&lt;BR /&gt;DDR type is DDR3&lt;BR /&gt;Data width: 32, bank num: 8&lt;BR /&gt;Row size: 13, col size: 10&lt;BR /&gt;Chip select CSD0 is used&lt;BR /&gt;Density per chip select: 256MB&lt;BR /&gt;============================================&lt;BR /&gt;DDR Stress Test Iteration 1&lt;BR /&gt;Current Temperature: 46&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;DDR Freq: 396 MHz&lt;BR /&gt;t0.1: data is addr test&lt;BR /&gt;&lt;STRONG&gt;Address of failure(step2): 0x12001240&lt;/STRONG&gt;&lt;BR /&gt;Data was: 0x52001240&lt;BR /&gt;But pattern should match address&lt;BR /&gt;Error: failed to run stress test!!!&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Kazuma Sasaki.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Aug 2019 01:27:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-failed-DRAM-address-decode/m-p/936671#M140342</guid>
      <dc:creator>Kazuma_Sasaki</dc:creator>
      <dc:date>2019-08-01T01:27:06Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 failed DRAM address decode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-failed-DRAM-address-decode/m-p/936672#M140343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kazuma&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;If we encountered access error at 0x12001240, we can identify failing point as following table. Is it right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes this decoding is correct.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Aug 2019 04:58:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-failed-DRAM-address-decode/m-p/936672#M140343</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-08-01T04:58:16Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 failed DRAM address decode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-failed-DRAM-address-decode/m-p/936673#M140344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I appreciate your quickly support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Kazuma Sasaki.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Aug 2019 05:02:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-failed-DRAM-address-decode/m-p/936673#M140344</guid>
      <dc:creator>Kazuma_Sasaki</dc:creator>
      <dc:date>2019-08-01T05:02:02Z</dc:date>
    </item>
  </channel>
</rss>