<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 SabreSD SDP BSP compatibility</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SabreSD-SDP-BSP-compatibility/m-p/218239#M14027</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Due to the fast update of hardware and software for these boards, I want to confirm the compatibilities between Reference Board revisions and their compatible BSP counterparts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I currently know based on the release notes:&lt;/P&gt;&lt;P&gt;Android BSP r13.3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SabreSD Rev B3 or 4 - Compiled and pre-built images OK (also stated in their release notes)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SabreSD Rev C1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - Compiled and pre-built, boot from eMMC and uSD - Would NOT Boot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Android BSP r13.4&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SabreSD Rev C1 - compiled and pre-built OK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the release notes of BSP 13.4, It says that the bsp is compatible with i.MX6Quad/Duallite boards, but it does not specify what revision, not like in r13.3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So can anyone confirm, what board revision is the current r13.4 BSPs compatible to? also what BSP versions are rev C boards compatible?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Dec 2012 07:38:48 GMT</pubDate>
    <dc:creator>Jon1z</dc:creator>
    <dc:date>2012-12-28T07:38:48Z</dc:date>
    <item>
      <title>SabreSD SDP BSP compatibility</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SabreSD-SDP-BSP-compatibility/m-p/218239#M14027</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Due to the fast update of hardware and software for these boards, I want to confirm the compatibilities between Reference Board revisions and their compatible BSP counterparts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I currently know based on the release notes:&lt;/P&gt;&lt;P&gt;Android BSP r13.3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SabreSD Rev B3 or 4 - Compiled and pre-built images OK (also stated in their release notes)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SabreSD Rev C1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - Compiled and pre-built, boot from eMMC and uSD - Would NOT Boot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Android BSP r13.4&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SabreSD Rev C1 - compiled and pre-built OK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the release notes of BSP 13.4, It says that the bsp is compatible with i.MX6Quad/Duallite boards, but it does not specify what revision, not like in r13.3.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So can anyone confirm, what board revision is the current r13.4 BSPs compatible to? also what BSP versions are rev C boards compatible?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Dec 2012 07:38:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SabreSD-SDP-BSP-compatibility/m-p/218239#M14027</guid>
      <dc:creator>Jon1z</dc:creator>
      <dc:date>2012-12-28T07:38:48Z</dc:date>
    </item>
  </channel>
</rss>