<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX8X Development tools</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8X-Development-tools/m-p/935726#M140143</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yuri&lt;/P&gt;&lt;P&gt;Thanks for the info. I did not know that the i.MX8X is the same as 8QuadXPlus. Why can't NXP use the same name everywhere.&lt;/P&gt;&lt;P&gt;I have build&amp;nbsp; and downloaded a SDK using this settings. The file is called SDK_2.5.2_MIMX8QX6xxxFZ. I am not sure if this is correct for my processor, as the name on the chip is PIMX8UX6AVLFZAB.&lt;/P&gt;&lt;P&gt;When I try to load it into the MCUXpresso IDE I get the following error:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/90457iD46F0822D3824E9D/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The message in the log is:&lt;/P&gt;&lt;P&gt;Error&lt;BR /&gt;Fri Jul 05 08:23:48 CEST 2019&lt;BR /&gt;The SDK 'SDK_2.x_MIMX8QX6xxxFZ' does not contain any MCUXpresso IDE compatible toolchain.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It would seem the NXP tools do not work together properly. In the SDK builder the only tool chain options are GCC and IAR, there is no MCUXpresso option.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Jul 2019 06:34:39 GMT</pubDate>
    <dc:creator>amanning</dc:creator>
    <dc:date>2019-07-05T06:34:39Z</dc:date>
    <item>
      <title>i.MX8X Development tools</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8X-Development-tools/m-p/935722#M140139</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We wish to use the i.MX8X processor in a new product and I am lokking for the correct tools for the development.&lt;/P&gt;&lt;P&gt;I cannot find the correct tools to download and debug the embedded Cortext-M core.&lt;/P&gt;&lt;P&gt;The chip has a JTAG connection. Can I use the Keil ULINKpro debugger with this port? I am not sure about the voltage levels as the core runs on 1V8.&lt;/P&gt;&lt;P&gt;The ARM Development tools (ARM-DS and ARM/KEIL MDK) do not have a support pack for the i.MX8X processor. Are there other tools that support the i.MX8X and the Keil ULINKpro debugger?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the standard method for the Cortex-M development? I have only seen descriptions of copying the code onto a SD card and then copying via UBOOT into the Flash. This does not sound like an effient development process.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help to get the debugging up and running would be appriciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jul 2019 08:56:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8X-Development-tools/m-p/935722#M140139</guid>
      <dc:creator>amanning</dc:creator>
      <dc:date>2019-07-03T08:56:29Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8X Development tools</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8X-Development-tools/m-p/935723#M140140</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; Use the following resource&amp;nbsp; to get M4 SDK for i.MX8X. The SDK sources &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;may be used as M4 examples and projects for IAR and GCC toolchains.&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp;&lt;A href="https://mcuxpresso.nxp.com/en/welcome"&gt;https://mcuxpresso.nxp.com/en/welcome&lt;/A&gt; &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; As for JTAG debugger - look at section 3.1 (Compiler/Debugger) of "Getting Started with &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;MCUXpresso SDK for i.MX 8QuadXPlus.pdf" in SDK documentation.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp; Note, also Lauterbach supports i.MX8X. &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;-------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Note:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jul 2019 09:10:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8X-Development-tools/m-p/935723#M140140</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2019-07-04T09:10:46Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8X Development tools</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8X-Development-tools/m-p/935724#M140141</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have looked at and downloaded the MCUXpresso SDK and IDE, but I cannot find any support for the i.MX8X processor. The SDK builder does not include this processor.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jul 2019 13:58:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8X-Development-tools/m-p/935724#M140141</guid>
      <dc:creator>amanning</dc:creator>
      <dc:date>2019-07-04T13:58:45Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8X Development tools</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8X-Development-tools/m-p/935725#M140142</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; On the Web&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuxpresso.nxp.com/en/select" title="https://mcuxpresso.nxp.com/en/select"&gt;https://mcuxpresso.nxp.com/en/select&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/90433i4B4DC0AFB52EB18D/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2019 03:51:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8X-Development-tools/m-p/935725#M140142</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2019-07-05T03:51:52Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8X Development tools</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8X-Development-tools/m-p/935726#M140143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yuri&lt;/P&gt;&lt;P&gt;Thanks for the info. I did not know that the i.MX8X is the same as 8QuadXPlus. Why can't NXP use the same name everywhere.&lt;/P&gt;&lt;P&gt;I have build&amp;nbsp; and downloaded a SDK using this settings. The file is called SDK_2.5.2_MIMX8QX6xxxFZ. I am not sure if this is correct for my processor, as the name on the chip is PIMX8UX6AVLFZAB.&lt;/P&gt;&lt;P&gt;When I try to load it into the MCUXpresso IDE I get the following error:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/90457iD46F0822D3824E9D/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The message in the log is:&lt;/P&gt;&lt;P&gt;Error&lt;BR /&gt;Fri Jul 05 08:23:48 CEST 2019&lt;BR /&gt;The SDK 'SDK_2.x_MIMX8QX6xxxFZ' does not contain any MCUXpresso IDE compatible toolchain.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It would seem the NXP tools do not work together properly. In the SDK builder the only tool chain options are GCC and IAR, there is no MCUXpresso option.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2019 06:34:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8X-Development-tools/m-p/935726#M140143</guid>
      <dc:creator>amanning</dc:creator>
      <dc:date>2019-07-05T06:34:39Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8X Development tools</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8X-Development-tools/m-p/935727#M140144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; please try to follow section 5 (Run a demo using ARM® GCC) of Getting Started with MCUXpresso&lt;/P&gt;&lt;P&gt;SDK for i.MX 8QuadXPlus, Rev. 1, 04/2019.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jul 2019 08:47:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8X-Development-tools/m-p/935727#M140144</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2019-07-08T08:47:51Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8X Development tools</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8X-Development-tools/m-p/935728#M140145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have had a closer look at the MCUXpresso documentation, especially the chapter 5 you mentioned.&lt;/P&gt;&lt;P&gt;It is now clear that the MCUXpresso SDK produces files that cannot be used with the MCUXpresso IDE. This seems to be very strange to me. I assumed as the names of the 2 products are the same, they would work hand in hand.&lt;/P&gt;&lt;P&gt;As I do not have a Linux machine (MCUXpresso IDE runs on windows), I cannot use the files generated by MCUXpresso SDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This brings me back to the original question: When will NXP supply a support pack for the ARM-DS toolchain?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian Manning&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Software Engineer&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hamilton Medical AG&lt;/P&gt;&lt;P&gt;Via Crusch 8&lt;/P&gt;&lt;P&gt;7402 Bonaduz&lt;/P&gt;&lt;P&gt;Switzerland&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Phone:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;+41 58 610 13 82&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fax:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;+41 58 610 00 20&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mail:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;amanning@hamilton-medical.com&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Web:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/www.hamilton-medical.com" target="test_blank"&gt;www.hamilton-medical.com&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;https://www.hamilton-medical.com/News/Newsletter-sign-up.html&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This message is confidential. It may also be privileged or otherwise protected by work product immunity or other legal rules. If you have received it by mistake, please let us know by e-mail reply and delete it from your system; you may not copy this message or disclose its contents to anyone. The integrity and security of this message cannot be guaranteed on the Internet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Von: Yuri &amp;lt;admin@community.nxp.com&amp;gt;&lt;/P&gt;&lt;P&gt;Gesendet: Montag, 8. Juli 2019 10:49&lt;/P&gt;&lt;P&gt;An: Manning Adrian &amp;lt;amanning@hamilton-medical.com&amp;gt;&lt;/P&gt;&lt;P&gt;Betreff: Re:  - Re: i.MX8X Development tools&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP Community &amp;lt;https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Re: i.MX8X Development tools&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reply from Yuri Muhin&amp;lt;https://community.nxp.com/people/Yuri?et=watches.email.thread&amp;gt; in i.MX Processors - View the full discussion&amp;lt;https://community.nxp.com/message/1174697?commentID=1174697&amp;amp;et=watches.email.thread#comment-1174697&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jul 2019 12:03:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8X-Development-tools/m-p/935728#M140145</guid>
      <dc:creator>amanning</dc:creator>
      <dc:date>2019-07-09T12:03:08Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8X Development tools</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8X-Development-tools/m-p/935729#M140146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Generally customers can use virtual machine technology, supported in VMware and Virtual Box,&lt;BR /&gt;to run Linux toolchains, recommended for the SDK, under Windows OS. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Also, customers can try using the Windows versions of the toolchains.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jul 2019 04:20:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8X-Development-tools/m-p/935729#M140146</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2019-07-10T04:20:23Z</dc:date>
    </item>
  </channel>
</rss>