<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Yocto Rocko: etc/network/interfaces file missing in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Rocko-etc-network-interfaces-file-missing/m-p/935662#M140123</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You may have NetworkManager or connman installed instead of ifupdown. In that case you can use nmcli/nmtui or connmanctl to configure network interfaces.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Jul 2019 06:29:38 GMT</pubDate>
    <dc:creator>turker</dc:creator>
    <dc:date>2019-07-04T06:29:38Z</dc:date>
    <item>
      <title>Yocto Rocko: etc/network/interfaces file missing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Rocko-etc-network-interfaces-file-missing/m-p/935661#M140122</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;I have built NXP's Yocto (4.9.88 rocko) following the Yocto Project User's Guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My board is based on iMX6ULL EVK and it has Ethernet interface, but in &lt;STRONG&gt;/et&lt;/STRONG&gt;&lt;STRONG&gt;c/network/&lt;/STRONG&gt; there is no "interfaces" file so i can't set up static IP and wifi.&lt;BR /&gt;&lt;BR /&gt;How can I enable networking in yocto environment?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thank you very much.&lt;BR /&gt;&lt;BR /&gt;Andrea&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jul 2019 06:52:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Rocko-etc-network-interfaces-file-missing/m-p/935661#M140122</guid>
      <dc:creator>acompagni</dc:creator>
      <dc:date>2019-07-03T06:52:40Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Rocko: etc/network/interfaces file missing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Rocko-etc-network-interfaces-file-missing/m-p/935662#M140123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You may have NetworkManager or connman installed instead of ifupdown. In that case you can use nmcli/nmtui or connmanctl to configure network interfaces.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jul 2019 06:29:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Rocko-etc-network-interfaces-file-missing/m-p/935662#M140123</guid>
      <dc:creator>turker</dc:creator>
      <dc:date>2019-07-04T06:29:38Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Rocko: etc/network/interfaces file missing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Rocko-etc-network-interfaces-file-missing/m-p/935663#M140124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;BR /&gt;thank you for your answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've checked, I have installed only ifupdown.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have also included in /mylayer/recipes-core/init-ifupdown/init-ifupdown-1.0.bbappend which should modify interfaces file through /mylayer/&lt;SPAN&gt;recipes-core/init-ifupdown/init-ifupdown-1.0/interfaces, but nothing happens.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Still no /etc/network/interfaces file&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I install NetworkManager packet and I follow your suggestion this is what I get:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;nmcli device show
GENERAL.DEVICE:                         eth1
GENERAL.TYPE:                           ethernet
GENERAL.HWADDR:                         6E:6F:A6:5B:07:8C
GENERAL.MTU:                            1500
GENERAL.STATE:                          20 (unavailable)
GENERAL.CONNECTION:                     --
GENERAL.CON-PATH:                       --
WIRED-PROPERTIES.CARRIER:               off

GENERAL.DEVICE:                         can0
GENERAL.TYPE:                           can
GENERAL.HWADDR:                         
GENERAL.MTU:                            16
GENERAL.STATE:                          10 (unmanaged)
GENERAL.CONNECTION:                     --
GENERAL.CON-PATH:                       --
IP4.GATEWAY:                            
IP6.GATEWAY:                            

GENERAL.DEVICE:                         can1
GENERAL.TYPE:                           can
GENERAL.HWADDR:                         
GENERAL.MTU:                            16
GENERAL.STATE:                          10 (unmanaged)
GENERAL.CONNECTION:                     --
GENERAL.CON-PATH:                       --
IP4.GATEWAY:                            
IP6.GATEWAY:                            

GENERAL.DEVICE:                         eth0
GENERAL.TYPE:                           ethernet
GENERAL.HWADDR:                         92:02:94:A6:2C:43
GENERAL.MTU:                            1500
GENERAL.STATE:                          10 (unmanaged)
GENERAL.CONNECTION:                     --
GENERAL.CON-PATH:                       --
WIRED-PROPERTIES.CARRIER:               off
IP4.GATEWAY:                            
IP6.GATEWAY:                            

GENERAL.DEVICE:                         sit0
GENERAL.TYPE:                           iptunnel
GENERAL.HWADDR:                         (unknown)
GENERAL.MTU:                            1480
GENERAL.STATE:                          10 (unmanaged)
GENERAL.CONNECTION:                     --
GENERAL.CON-PATH:                       --
IP4.GATEWAY:                            
IP6.GATEWAY:                            

GENERAL.DEVICE:                         lo
GENERAL.TYPE:                           loopback
GENERAL.HWADDR:                         00:00:00:00:00:00
GENERAL.MTU:                            65536
GENERAL.STATE:                          10 (unmanaged)
GENERAL.CONNECTION:                     --
GENERAL.CON-PATH:                       --
IP4.ADDRESS[1]:                         127.0.0.1/8
IP4.GATEWAY:                            
IP6.ADDRESS[1]:                         ::1/128
&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;BR /&gt;I really can't understand...&lt;BR /&gt;&lt;BR /&gt;Thank you&lt;BR /&gt;&lt;BR /&gt;Andrea&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jul 2019 09:08:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Rocko-etc-network-interfaces-file-missing/m-p/935663#M140124</guid>
      <dc:creator>acompagni</dc:creator>
      <dc:date>2019-07-04T09:08:37Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Rocko: etc/network/interfaces file missing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Rocko-etc-network-interfaces-file-missing/m-p/935664#M140125</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That is weird. Does your network interface work when you assign ip address using ifconfig? For example:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;ifconfig eth0 up&lt;/P&gt;&lt;P&gt;ifconfig eth0 192.168.1.100 netmask 255.255.255.0&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;You could also try manually copying the interfaces file in the following link under /etc/network/ and see if it works: &lt;A class="link-titled" href="https://git.yoctoproject.org/cgit.cgi/poky/plain/meta/recipes-core/init-ifupdown/init-ifupdown-1.0/interfaces" title="https://git.yoctoproject.org/cgit.cgi/poky/plain/meta/recipes-core/init-ifupdown/init-ifupdown-1.0/interfaces"&gt;https://git.yoctoproject.org/cgit.cgi/poky/plain/meta/recipes-core/init-ifupdown/init-ifupdown-1.0/interfaces&lt;/A&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jul 2019 16:46:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Rocko-etc-network-interfaces-file-missing/m-p/935664#M140125</guid>
      <dc:creator>turker</dc:creator>
      <dc:date>2019-07-04T16:46:29Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Rocko: etc/network/interfaces file missing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Rocko-etc-network-interfaces-file-missing/m-p/935665#M140126</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="342409" data-username="acompagni@lifeelettronica.com" href="https://community.nxp.com/people/acompagni@lifeelettronica.com"&gt;Andrea Compagni&lt;/A&gt;,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;One can follow these steps to assign Static IP. Follow below commands in your Board's Console.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;ifconfig -a&amp;nbsp;&amp;nbsp; (To check that ip address is provided or not).&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;udhcpc -i eth0&amp;nbsp;&amp;nbsp; ( command to get ip for ethernet port 0)&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;ifconfig -a&amp;nbsp;&amp;nbsp;&amp;nbsp; (to check the ip address of eth0 and Mask)&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;route -n&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;&lt;STRONG style="text-decoration: underline; "&gt;OR&lt;/STRONG&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;netstat -r&lt;/SPAN&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; (to find gateway and Mask)&lt;BR /&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;Create file named wireless.network in path "&lt;STRONG&gt;/etc/systemd/network/"&lt;/STRONG&gt;&amp;nbsp; with below data.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; [match]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;Name=eth0&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;[Network]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;Address=&amp;lt;ip address/mask&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;Gateway=&amp;lt;gateway address&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;&amp;nbsp;Let us know if you still do not get static ip after following above steps.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial, helvetica, sans-serif;"&gt;Radhika Somaiya.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jul 2019 06:14:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Rocko-etc-network-interfaces-file-missing/m-p/935665#M140126</guid>
      <dc:creator>radhikasomaiya</dc:creator>
      <dc:date>2019-07-09T06:14:31Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Rocko: etc/network/interfaces file missing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Rocko-etc-network-interfaces-file-missing/m-p/935666#M140127</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible to do the same for usb configured as cdc? what changes should be made in that .network file?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Oct 2019 05:25:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Rocko-etc-network-interfaces-file-missing/m-p/935666#M140127</guid>
      <dc:creator>sujay1</dc:creator>
      <dc:date>2019-10-29T05:25:16Z</dc:date>
    </item>
  </channel>
</rss>