<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Configure both csi0 and csi1</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Configure-both-csi0-and-csi1/m-p/934439#M140029</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guozhen&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes they can be used in the same time, one can try&lt;/P&gt;&lt;P&gt;with fsl-imx8qm-mek-mipi-two-ov5640.dts:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/fsl-imx8qm-mek-mipi-two-ov5640.dts?h=imx_4.14.78_1.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/fsl-imx8qm-mek-mipi-two-ov5640.dts?h=imx_4.14.78_1.0.0_ga"&gt;fsl-imx8qm-mek-mipi-two-ov5640.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Jun 2019 23:19:23 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-06-18T23:19:23Z</dc:date>
    <item>
      <title>Configure both csi0 and csi1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configure-both-csi0-and-csi1/m-p/934438#M140028</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #333333; background-color: #f7f8fa; font-size: 14px;"&gt;In imx8qm, csi0 and csi1 need to be used at the same time. In addition to being configured in DTS, is it necessary to configure elsewhere? I set the status attribute in the nodes of csi0 and csi1 to okay, but only csi0 is loaded&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jun 2019 03:56:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configure-both-csi0-and-csi1/m-p/934438#M140028</guid>
      <dc:creator>dengguozhen</dc:creator>
      <dc:date>2019-06-18T03:56:58Z</dc:date>
    </item>
    <item>
      <title>Re: Configure both csi0 and csi1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configure-both-csi0-and-csi1/m-p/934439#M140029</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guozhen&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes they can be used in the same time, one can try&lt;/P&gt;&lt;P&gt;with fsl-imx8qm-mek-mipi-two-ov5640.dts:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/fsl-imx8qm-mek-mipi-two-ov5640.dts?h=imx_4.14.78_1.0.0_ga" title="https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/fsl-imx8qm-mek-mipi-two-ov5640.dts?h=imx_4.14.78_1.0.0_ga"&gt;fsl-imx8qm-mek-mipi-two-ov5640.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jun 2019 23:19:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configure-both-csi0-and-csi1/m-p/934439#M140029</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-06-18T23:19:23Z</dc:date>
    </item>
  </channel>
</rss>