<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX6 Solo DDR3 Calibration Script Aid in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Solo-DDR3-Calibration-Script-Aid/m-p/933960#M139990</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Bruno,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The updated Programming Aid for i.MX6Solo and Dual Lite is the following:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-105964"&gt;i.MX6DL SABRE SDP/B DDR3 Register Programming Aid&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The programming aids were separated by versions of the i.MX6 processor so they are no longer all supported in a single programming aid.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-236354"&gt;https://community.nxp.com/docs/DOC-236354&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Jul 2019 14:33:55 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2019-07-09T14:33:55Z</dc:date>
    <item>
      <title>iMX6 Solo DDR3 Calibration Script Aid</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Solo-DDR3-Calibration-Script-Aid/m-p/933958#M139988</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I pulled down a script aid for imx6 DDR3 Calibration in Nov 2018. I was looking for a script that supported the iMX6 Solo/DualLite.The file I downloaded was "i.MX6DQSDL DDR3 Script Aid V0.11.xlsx" and this has support for a number iMX6 processors, including the iMX6 Solo, via a drop down menu.&lt;/P&gt;&lt;P&gt;However I went back to the NXP website and it looks like this script has been removed. In its place is a file MX6Q_SabreSD_DDR3_register_programming_aid_v2.3.xlsx&lt;/P&gt;&lt;P&gt;However this looks quite old and does not seem to support the iMX6Solo and now I can't find one that does.&lt;/P&gt;&lt;P&gt;Also the document "imx6 DRAM Port Application Guide - DD3" on the NXP website does not match this script aid.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This has prompted me to wonder which script aid I should use for the iMX6 Solo. Is the original one (i.MX6DQSDL DDR3 Script Aid V0.11.xlsx) still valid ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 May 2019 15:55:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Solo-DDR3-Calibration-Script-Aid/m-p/933958#M139988</guid>
      <dc:creator>bdp42</dc:creator>
      <dc:date>2019-05-31T15:55:11Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Solo DDR3 Calibration Script Aid</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Solo-DDR3-Calibration-Script-Aid/m-p/933959#M139989</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Bruno,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would recommend using the newest version. The previous one should also work as it was supported for a while and the hardware remains the same, but I’m trying to find out what are the differences on the output these two tools generate. Perhaps the newer version output may be better optimized.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I’ll let you know of my findings.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jun 2019 12:49:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Solo-DDR3-Calibration-Script-Aid/m-p/933959#M139989</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2019-06-06T12:49:24Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6 Solo DDR3 Calibration Script Aid</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6-Solo-DDR3-Calibration-Script-Aid/m-p/933960#M139990</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Bruno,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The updated Programming Aid for i.MX6Solo and Dual Lite is the following:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-105964"&gt;i.MX6DL SABRE SDP/B DDR3 Register Programming Aid&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The programming aids were separated by versions of the i.MX6 processor so they are no longer all supported in a single programming aid.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-236354"&gt;https://community.nxp.com/docs/DOC-236354&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jul 2019 14:33:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6-Solo-DDR3-Calibration-Script-Aid/m-p/933960#M139990</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2019-07-09T14:33:55Z</dc:date>
    </item>
  </channel>
</rss>