<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックEnabling Mobile_network &amp; RIL related Settings support for iMX6 based on Android 8.0 or 7.0 etc</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-Mobile-network-RIL-related-Settings-support-for-iMX6/m-p/933908#M139977</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="text-align: justify;"&gt;I was trying to integrate 4G Modem on iMX6dl running Android Oreo 8.0. but surprisingly the default BSP from nxp comes with WiFi-Only Device settings, which will not show any UI related settings for Mobile_Networks in status-bar also as well as Settings application also. When I added RIL source code,&amp;nbsp; device was not even trying to Send AT commands. I have debugged for some time and found the solution for the same. Many people have queried about this on nxp community So i thought of sharing my work as below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="text-align: justify;"&gt;&lt;BR /&gt;To enable Mobile_Network settings in Android UI two files have to changed namely&lt;/P&gt;&lt;P style="text-align: justify;"&gt;&lt;/P&gt;&lt;P style="text-align: justify;"&gt;1. device/fsl/imx6/imx6.mk --&amp;gt; used to mention device has RIL support&lt;/P&gt;&lt;P style="text-align: justify;"&gt;&lt;/P&gt;&lt;P style="text-align: justify;"&gt;2. device/fsl/sabresd_6dq/overlay/frameworks//base/core/res/res/values/config.xml --&amp;gt; used to Override the default config settings present is android frameworks. Android Frameworks, frameworks/base/core/res/res/values/config.xml file is superset of all settings which has support for everything. So when I commented overridden settings from overlay config.xml Mobile_networks settings re-appeared in Android UI and Device started to send AT commands to modem subsequently device got registered to Network also. I Have attached the patch and S.shots here.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Jul 2019 09:04:30 GMT</pubDate>
    <dc:creator>prasannakulkarni</dc:creator>
    <dc:date>2019-07-17T09:04:30Z</dc:date>
    <item>
      <title>Enabling Mobile_network &amp; RIL related Settings support for iMX6 based on Android 8.0 or 7.0 etc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-Mobile-network-RIL-related-Settings-support-for-iMX6/m-p/933908#M139977</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="text-align: justify;"&gt;I was trying to integrate 4G Modem on iMX6dl running Android Oreo 8.0. but surprisingly the default BSP from nxp comes with WiFi-Only Device settings, which will not show any UI related settings for Mobile_Networks in status-bar also as well as Settings application also. When I added RIL source code,&amp;nbsp; device was not even trying to Send AT commands. I have debugged for some time and found the solution for the same. Many people have queried about this on nxp community So i thought of sharing my work as below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="text-align: justify;"&gt;&lt;BR /&gt;To enable Mobile_Network settings in Android UI two files have to changed namely&lt;/P&gt;&lt;P style="text-align: justify;"&gt;&lt;/P&gt;&lt;P style="text-align: justify;"&gt;1. device/fsl/imx6/imx6.mk --&amp;gt; used to mention device has RIL support&lt;/P&gt;&lt;P style="text-align: justify;"&gt;&lt;/P&gt;&lt;P style="text-align: justify;"&gt;2. device/fsl/sabresd_6dq/overlay/frameworks//base/core/res/res/values/config.xml --&amp;gt; used to Override the default config settings present is android frameworks. Android Frameworks, frameworks/base/core/res/res/values/config.xml file is superset of all settings which has support for everything. So when I commented overridden settings from overlay config.xml Mobile_networks settings re-appeared in Android UI and Device started to send AT commands to modem subsequently device got registered to Network also. I Have attached the patch and S.shots here.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jul 2019 09:04:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-Mobile-network-RIL-related-Settings-support-for-iMX6/m-p/933908#M139977</guid>
      <dc:creator>prasannakulkarni</dc:creator>
      <dc:date>2019-07-17T09:04:30Z</dc:date>
    </item>
    <item>
      <title>Re: Enabling Mobile_network &amp; RIL related Settings support for iMX6 based on Android 8.0 or 7.0 etc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-Mobile-network-RIL-related-Settings-support-for-iMX6/m-p/933909#M139978</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;THanks for the sharing!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jul 2019 14:30:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-Mobile-network-RIL-related-Settings-support-for-iMX6/m-p/933909#M139978</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2019-07-17T14:30:23Z</dc:date>
    </item>
  </channel>
</rss>