<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Using MFG Tool on Linux to flash iMX6ULL EVK</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-MFG-Tool-on-Linux-to-flash-iMX6ULL-EVK/m-p/931743#M139739</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;BR /&gt;&lt;BR /&gt;I am using Linux kernel version 4.9.88. Is UUU supported for this kernel version?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Meetali Patel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Sep 2019 06:41:30 GMT</pubDate>
    <dc:creator>meetalipatel</dc:creator>
    <dc:date>2019-09-03T06:41:30Z</dc:date>
    <item>
      <title>Using MFG Tool on Linux to flash iMX6ULL EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-MFG-Tool-on-Linux-to-flash-iMX6ULL-EVK/m-p/931741#M139737</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to flash a binary on iMX6ULL EVK Board using MFG Tool. When running mfgtools on Windows, there is no issue and I am able to flash successfully. However, when I trying running mfgtools on Linux, I am unable to do so (I am using Ubuntu 14.04).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To run the mfgtoolcli application I executed the following command:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;$&amp;nbsp;./mfgtoolcli -l eMMC -s lite=l -s 6uluboot=14x14evk -s 6uldtb=14x14-evk&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The output is:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Your Options:&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;lite: l&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;6uluboot: 14x14evk&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;6uldtb: 14x14-evk&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Ready to flash.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;init op Failed code# 24&lt;/EM&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The logs in&amp;nbsp;MfgToolLibLog.txt file are:&lt;/P&gt;&lt;P&gt;&lt;EM&gt; Start new logging&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ModuleID[2] LevelID[1]: Error: Invalid device name: MX6ULL&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ModuleID[2] LevelID[1]: Parse ucl script failed, error code: 24&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please guide me on how can I successfully flash using the mfgtools on Linux machine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Meetali Patel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Sep 2019 07:00:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-MFG-Tool-on-Linux-to-flash-iMX6ULL-EVK/m-p/931741#M139737</guid>
      <dc:creator>meetalipatel</dc:creator>
      <dc:date>2019-09-02T07:00:50Z</dc:date>
    </item>
    <item>
      <title>Re: Using MFG Tool on Linux to flash iMX6ULL EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-MFG-Tool-on-Linux-to-flash-iMX6ULL-EVK/m-p/931742#M139738</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="border: none; padding: 0in;"&gt;Hi Patel,&lt;/P&gt;&lt;P style="border: none; padding: 0in;"&gt;For downloading images to i.MX using the Serial downloader mode, you could use the Universal Update Utility (UUU), available for Windows and Linux. Please take a look to the following Community thread, that provides additional UUU examples, and points to UUU documentation that could help you:&lt;/P&gt;&lt;P style="border: none; padding: 0in;"&gt;&lt;A href="https://community.nxp.com/thread/506805"&gt;IMX8M UUU flashing questions&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="border: none; padding: 0in;"&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Sep 2019 20:47:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-MFG-Tool-on-Linux-to-flash-iMX6ULL-EVK/m-p/931742#M139738</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2019-09-02T20:47:30Z</dc:date>
    </item>
    <item>
      <title>Re: Using MFG Tool on Linux to flash iMX6ULL EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-MFG-Tool-on-Linux-to-flash-iMX6ULL-EVK/m-p/931743#M139739</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;BR /&gt;&lt;BR /&gt;I am using Linux kernel version 4.9.88. Is UUU supported for this kernel version?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Meetali Patel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Sep 2019 06:41:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-MFG-Tool-on-Linux-to-flash-iMX6ULL-EVK/m-p/931743#M139739</guid>
      <dc:creator>meetalipatel</dc:creator>
      <dc:date>2019-09-03T06:41:30Z</dc:date>
    </item>
    <item>
      <title>Re: Using MFG Tool on Linux to flash iMX6ULL EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-MFG-Tool-on-Linux-to-flash-iMX6ULL-EVK/m-p/931744#M139740</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Patel,&lt;BR /&gt;Yes, it should be compatible, it just will need to manually specify the U-Boot and RootFS when launching the command, instead of using the “auto” script. You could take a look to the following link:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/NXPmicro/mfgtools/wiki/Example" title="https://github.com/NXPmicro/mfgtools/wiki/Example"&gt;Example · NXPmicro/mfgtools Wiki · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Sep 2019 21:39:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-MFG-Tool-on-Linux-to-flash-iMX6ULL-EVK/m-p/931744#M139740</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2019-09-03T21:39:51Z</dc:date>
    </item>
  </channel>
</rss>