<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Unstable HD output on iMX6 Quad Plus Board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Unstable-HD-output-on-iMX6-Quad-Plus-Board/m-p/929446#M139471</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Update: I have obtained a QuadPlus Wandboard, which has a very similar design, but it does not exhibit any fault using the same kernel, software, and a nearly identical device tree. However running my u-boot on the Wandboard show up the same fault, so it's probably a DDR setup issue with the version of u-boot I have.&amp;nbsp;&amp;nbsp; Will track down the working version that came with the wandboard and re-compile it for my board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Sep 2019 03:54:14 GMT</pubDate>
    <dc:creator>tonybryant</dc:creator>
    <dc:date>2019-09-13T03:54:14Z</dc:date>
    <item>
      <title>Unstable HD output on iMX6 Quad Plus Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unstable-HD-output-on-iMX6-Quad-Plus-Board/m-p/929444#M139469</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have upgraded our iMX6 based product from Quad to QuadPlus:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Everything works, BUT video output is unstable (i.e. flicks to all black randomly) at high resolutions, e.g. 1920x1080&lt;/P&gt;&lt;P&gt;- At 1024x768, output is 100% stable.&lt;/P&gt;&lt;P&gt;- Both Parallel RGB and HDMI outputs are affected identically&lt;/P&gt;&lt;P&gt;- Reducing pixclk down to 120MHz (from stock 138MHz) improves the situation a bit, but does not fix it.&lt;/P&gt;&lt;P&gt;- memtester is rock solid, as is every other type of software I have tried, including heavy multithreaded OpenCV ML stuff.&lt;/P&gt;&lt;P&gt;- Tried upping and lowering ARM/SOC &amp;amp; 2.5V supplies (via the standard PF0100 PMIC), without any change.&lt;/P&gt;&lt;P&gt;- Changing to LDO bypass mode doesn't make it better or worse&lt;/P&gt;&lt;P&gt;- Adding extra bypassing to SOC_CAP didn't help at all.&lt;/P&gt;&lt;P&gt;- Scoping all power rails shows clean and in-spec voltages.&lt;/P&gt;&lt;P&gt;- Adding extra bypassing to SOC_CAP didn't help at all.&lt;/P&gt;&lt;P&gt;- Loading up the system up, with either a memory tester or an OpenGL app, makes it&lt;/P&gt;&lt;P&gt;worse,&amp;nbsp; leading me to suspect memory bandwidth issue.&amp;nbsp; Raw CPU load that uses no memory doesn't affect the output.&lt;/P&gt;&lt;P&gt;- memtester seems to run at a slightly greater speed than the Quad boards, indicating greater memory bandwidth is available on the QuadPlus boards.&lt;/P&gt;&lt;P&gt;- AXI priorities in NoC and the GPR regs seem to be set up sensibly.&lt;/P&gt;&lt;P&gt;- Linux 4.9.128&amp;nbsp; Uboot 2018.07-32726, both derived from Boundaries Devices's Git.&lt;/P&gt;&lt;P&gt;- 64bit 1G DDR3 memory&lt;/P&gt;&lt;P&gt;- No kernel message during flicker events, though these messages are in the log:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x08800000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have I missed something important?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not sure if it's HW, or an IPU datapath setup issue, or something else?&amp;nbsp; I'm fishing for ideas for avenues to pursue at this point...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 31 Aug 2019 02:47:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unstable-HD-output-on-iMX6-Quad-Plus-Board/m-p/929444#M139469</guid>
      <dc:creator>tonybryant</dc:creator>
      <dc:date>2019-08-31T02:47:37Z</dc:date>
    </item>
    <item>
      <title>Re: Unstable HD output on iMX6 Quad Plus Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unstable-HD-output-on-iMX6-Quad-Plus-Board/m-p/929445#M139470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tony&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check EB828 MMDC &amp;amp; NoC Configuration for Optimal DDR3 Performance&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/engineering-bulletin/EB828.pdf" title="https://www.nxp.com/docs/en/engineering-bulletin/EB828.pdf"&gt;https://www.nxp.com/docs/en/engineering-bulletin/EB828.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and memory profile tool &lt;A href="https://community.nxp.com/thread/443828"&gt;About MMDC Profiling Tool for i.MX6&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/imx-test/tree/test/mmdc?h=imx_4.9.123_imx8mm_ga" title="https://source.codeaurora.org/external/imx/imx-test/tree/test/mmdc?h=imx_4.9.123_imx8mm_ga"&gt;mmdc\test - imx-test - i.MX Driver Test Application Software&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also try with nxp linux from &lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/linux-imx" title="https://source.codeaurora.org/external/imx/linux-imx"&gt;linux-imx - i.MX Linux kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Linux documentation&lt;BR /&gt;&lt;A class="link-titled" href="https://www.nxp.com/design/i.mx-developer-resources/i.mx-software-and-development-tool:IMX-SW" title="https://www.nxp.com/design/i.mx-developer-resources/i.mx-software-and-development-tool:IMX-SW"&gt;i.MX Software | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note, boundaries devices's software is supported by boundary devices directly&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://boundarydevices.com/software/" title="https://boundarydevices.com/software/"&gt;https://boundarydevices.com/software/&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Sep 2019 05:15:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unstable-HD-output-on-iMX6-Quad-Plus-Board/m-p/929445#M139470</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-09-02T05:15:12Z</dc:date>
    </item>
    <item>
      <title>Re: Unstable HD output on iMX6 Quad Plus Board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unstable-HD-output-on-iMX6-Quad-Plus-Board/m-p/929446#M139471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Update: I have obtained a QuadPlus Wandboard, which has a very similar design, but it does not exhibit any fault using the same kernel, software, and a nearly identical device tree. However running my u-boot on the Wandboard show up the same fault, so it's probably a DDR setup issue with the version of u-boot I have.&amp;nbsp;&amp;nbsp; Will track down the working version that came with the wandboard and re-compile it for my board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Sep 2019 03:54:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unstable-HD-output-on-iMX6-Quad-Plus-Board/m-p/929446#M139471</guid>
      <dc:creator>tonybryant</dc:creator>
      <dc:date>2019-09-13T03:54:14Z</dc:date>
    </item>
  </channel>
</rss>