<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックXIP boot  feature</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/XIP-boot-feature/m-p/927876#M139270</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello there!&lt;BR /&gt;I use MCIMX6SX4_A9.&lt;BR /&gt;I want to clarify some points when qspi boot mode implements.&lt;BR /&gt;I realaze that even if an uboot image is created with BOOT_FROM qspi and it will be set at right place on a flash device, there would not be XIP boot process while IVT data structure (entry) points to RAM.&lt;BR /&gt;(am i right? i suppose in case of xip, the entry have points to flash address)&lt;BR /&gt;i would to know how works the engine that swich load proccess to XIP and is it connected with uboot ld file?&lt;BR /&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Jul 2019 17:06:49 GMT</pubDate>
    <dc:creator>o_scherbinin</dc:creator>
    <dc:date>2019-07-16T17:06:49Z</dc:date>
    <item>
      <title>XIP boot  feature</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/XIP-boot-feature/m-p/927876#M139270</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello there!&lt;BR /&gt;I use MCIMX6SX4_A9.&lt;BR /&gt;I want to clarify some points when qspi boot mode implements.&lt;BR /&gt;I realaze that even if an uboot image is created with BOOT_FROM qspi and it will be set at right place on a flash device, there would not be XIP boot process while IVT data structure (entry) points to RAM.&lt;BR /&gt;(am i right? i suppose in case of xip, the entry have points to flash address)&lt;BR /&gt;i would to know how works the engine that swich load proccess to XIP and is it connected with uboot ld file?&lt;BR /&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jul 2019 17:06:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/XIP-boot-feature/m-p/927876#M139270</guid>
      <dc:creator>o_scherbinin</dc:creator>
      <dc:date>2019-07-16T17:06:49Z</dc:date>
    </item>
    <item>
      <title>Re: XIP boot  feature</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/XIP-boot-feature/m-p/927877#M139271</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Oleg&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes this understanding is correct and Reference Manual states&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/80205i9A8D8DEDE4C2BBCD/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.jpg" alt="pastedImage_1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jul 2019 23:32:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/XIP-boot-feature/m-p/927877#M139271</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-07-16T23:32:01Z</dc:date>
    </item>
    <item>
      <title>Re: XIP boot  feature</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/XIP-boot-feature/m-p/927878#M139272</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jul 2019 15:45:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/XIP-boot-feature/m-p/927878#M139272</guid>
      <dc:creator>o_scherbinin</dc:creator>
      <dc:date>2019-07-17T15:45:10Z</dc:date>
    </item>
  </channel>
</rss>