<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic WiFi Scan not working in Android Auto in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/WiFi-Scan-not-working-in-Android-Auto/m-p/926219#M139072</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on iMX8QXP-CPU MEK. And I have flashed following pre-built Android Auto image downloaded from NXP portal.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt; android_p9.0.0_1.0.2-auto-beta_image_8qmek&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I have ported my WLAN driver for this board, and able to install the module.&lt;/P&gt;&lt;P&gt;Using CLI, I am able to bring up my interface and connect to an AP. ping is also working fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, I have couple of questions :-&lt;/P&gt;&lt;P&gt;1. I tried setting following&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;setprop wifi.interface &amp;lt;interface_name&amp;gt; &amp;amp;&amp;amp; setprop wifi.direct.interface &amp;lt;interface_name&amp;gt;&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;still not able to scan available networks using &lt;STRONG&gt;GUI&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;Is there is anything else I need to do for making this work?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. I cannot find dhcp running in this image. Also do not know how to start this.&lt;/P&gt;&lt;P&gt;As a result, I have to assign ip manually.&lt;/P&gt;&lt;P&gt;Is there any command to start dhcp? To help resolving ip address automatically?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many Thanks,&lt;/P&gt;&lt;P&gt;Mayank&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 May 2019 12:46:34 GMT</pubDate>
    <dc:creator>mayanksirotiya</dc:creator>
    <dc:date>2019-05-30T12:46:34Z</dc:date>
    <item>
      <title>WiFi Scan not working in Android Auto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WiFi-Scan-not-working-in-Android-Auto/m-p/926219#M139072</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on iMX8QXP-CPU MEK. And I have flashed following pre-built Android Auto image downloaded from NXP portal.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt; android_p9.0.0_1.0.2-auto-beta_image_8qmek&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I have ported my WLAN driver for this board, and able to install the module.&lt;/P&gt;&lt;P&gt;Using CLI, I am able to bring up my interface and connect to an AP. ping is also working fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, I have couple of questions :-&lt;/P&gt;&lt;P&gt;1. I tried setting following&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;setprop wifi.interface &amp;lt;interface_name&amp;gt; &amp;amp;&amp;amp; setprop wifi.direct.interface &amp;lt;interface_name&amp;gt;&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;still not able to scan available networks using &lt;STRONG&gt;GUI&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;Is there is anything else I need to do for making this work?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. I cannot find dhcp running in this image. Also do not know how to start this.&lt;/P&gt;&lt;P&gt;As a result, I have to assign ip manually.&lt;/P&gt;&lt;P&gt;Is there any command to start dhcp? To help resolving ip address automatically?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many Thanks,&lt;/P&gt;&lt;P&gt;Mayank&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 May 2019 12:46:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WiFi-Scan-not-working-in-Android-Auto/m-p/926219#M139072</guid>
      <dc:creator>mayanksirotiya</dc:creator>
      <dc:date>2019-05-30T12:46:34Z</dc:date>
    </item>
    <item>
      <title>Re: WiFi Scan not working in Android Auto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/WiFi-Scan-not-working-in-Android-Auto/m-p/926220#M139073</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="border: none; padding: 0in;"&gt;Hi Mayank,&lt;/P&gt;&lt;P style="border: none; padding: 0in;"&gt;The i.MX8QX series is still on preproduction, so, no additional information/support could be provided yet. In case of having doubts, please refer with your Sales/FAE.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Jun 2019 00:22:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/WiFi-Scan-not-working-in-Android-Auto/m-p/926220#M139073</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2019-06-04T00:22:03Z</dc:date>
    </item>
  </channel>
</rss>