<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX 8M Mini Configuration Resistor Strength</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-Configuration-Resistor-Strength/m-p/925716#M139004</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For boot mode configuration pins on the 8M Mini like BOOT_MODE0, BOOT_MODE1, TEST_MODE, and JTAG_MOD, does it matter if I connect a very strong pull-up or pull-down resistor to these pins? Can I connect these pins directly to NVCC_JTAG or GND?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe these pins are always inputs, so I think it's acceptable to tie them directly to a power rail, but I want to ask and verify this before I accidentally blow up my 8M Mini.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Sep 2019 19:56:29 GMT</pubDate>
    <dc:creator>adevries</dc:creator>
    <dc:date>2019-09-27T19:56:29Z</dc:date>
    <item>
      <title>i.MX 8M Mini Configuration Resistor Strength</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-Configuration-Resistor-Strength/m-p/925716#M139004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For boot mode configuration pins on the 8M Mini like BOOT_MODE0, BOOT_MODE1, TEST_MODE, and JTAG_MOD, does it matter if I connect a very strong pull-up or pull-down resistor to these pins? Can I connect these pins directly to NVCC_JTAG or GND?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe these pins are always inputs, so I think it's acceptable to tie them directly to a power rail, but I want to ask and verify this before I accidentally blow up my 8M Mini.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Sep 2019 19:56:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-Configuration-Resistor-Strength/m-p/925716#M139004</guid>
      <dc:creator>adevries</dc:creator>
      <dc:date>2019-09-27T19:56:29Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini Configuration Resistor Strength</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-Configuration-Resistor-Strength/m-p/925717#M139005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Usually for pull-up resistors any value between 4.7k ~ 10k ohms, 4.7k ohm is preferred in high noise environments, for pull downs usually a 100k ohm is recommended.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Aldo.&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Oct 2019 23:12:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-Configuration-Resistor-Strength/m-p/925717#M139005</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2019-10-01T23:12:02Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini Configuration Resistor Strength</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-Configuration-Resistor-Strength/m-p/925718#M139006</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Aldo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the response. I know that the recommendation is for a 4.7-10k pull up and 100k pull down resistor. However, in my application, I'm looking to temporarily override&amp;nbsp;some pull-up and pull-down resistors. For example, if I have BOOT_MODE1 set to 1 by pulling it high with 4.7k ohms, and I need to set BOOT_MODE1 to 0 temporarily, can I just ground the pin?&amp;nbsp;&lt;/P&gt;&lt;P&gt;What if BOOT_MODE0 was set to 0 by pulling it low with 100k ohms, and I need to set it to 1. Can I connect the pin to NVCC_JTAG?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Oct 2019 23:29:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-Configuration-Resistor-Strength/m-p/925718#M139006</guid>
      <dc:creator>adevries</dc:creator>
      <dc:date>2019-10-01T23:29:15Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini Configuration Resistor Strength</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-Configuration-Resistor-Strength/m-p/925719#M139007</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For this case scenario we suggest to place a switch, just like in our EVK, if you plan to change the logic state of the BOOT_MODE.&lt;/P&gt;&lt;P&gt;Also, the connection you mentioned shouldn't be done, you can use one of these two options for the BOOT_MODE pins:&lt;/P&gt;&lt;UL type="disc"&gt;&lt;LI&gt;Pulled up or down using the resistor I previously mentioned&lt;/LI&gt;&lt;LI&gt;Connected directly to NVCC_JTAG or GND&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Pull-up regulate the amount of current it drives to the pin, if the power is not an issue it can be tied directly to VDD.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Aldo.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Oct 2019 21:39:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-Configuration-Resistor-Strength/m-p/925719#M139007</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2019-10-03T21:39:36Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Mini Configuration Resistor Strength</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-Configuration-Resistor-Strength/m-p/925720#M139008</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Aldo, that's good to know!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Oct 2019 18:29:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Mini-Configuration-Resistor-Strength/m-p/925720#M139008</guid>
      <dc:creator>adevries</dc:creator>
      <dc:date>2019-10-04T18:29:44Z</dc:date>
    </item>
  </channel>
</rss>