<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: bitbake fsl-image-gui errors out on do_configure</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-fsl-image-gui-errors-out-on-do-configure/m-p/924892#M138948</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Bill Goetz,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that you are using the Variscite yocto BSP. I would recommend not changing anything from the default setup and try baking the fsl-image-gui first jus to make sure that the default setup is working correctly. Then work on your changes. There is a lot of useful information and forums on the Yocto Project side.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Oct 2019 17:05:37 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2019-10-17T17:05:37Z</dc:date>
    <item>
      <title>bitbake fsl-image-gui errors out on do_configure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-fsl-image-gui-errors-out-on-do-configure/m-p/924891#M138947</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I'm trying to get 'bitback&amp;nbsp;fsl-image-gui' to work (attempting to create a build/cross-compiler environment) and&amp;nbsp;I'm getting stuck at:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;MAKEINFO='${SHELL} /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/missing --run makeinfo'&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here's the log file from the 'bitbake fsl-image-gui' command:&lt;/P&gt;&lt;P&gt;Any suggestions would be greatly appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;much thanks,&lt;/P&gt;&lt;P&gt;Bill&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bgoetz@volta18:~/unix$ cat /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/build/config.log&lt;BR /&gt;This file contains any messages produced by compilers while&lt;BR /&gt;running configure, to aid debugging if configure makes a mistake.&lt;/P&gt;&lt;P&gt;It was created by GNU Autoconf configure 2.69, which was&lt;BR /&gt;generated by GNU Autoconf 2.69. Invocation command line was&lt;/P&gt;&lt;P&gt;$ ../autoconf-2.69/configure --build=x86_64-linux --host=x86_64-linux --target=x86_64-linux --prefix=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr --exec_prefix=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr --bindir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/bin --sbindir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/sbin --libexecdir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/libexec --datadir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/share --sysconfdir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/etc --sharedstatedir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/com --localstatedir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/var --libdir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/lib --includedir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/include --oldincludedir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/include --infodir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/share/info --mandir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/share/man --disable-silent-rules --disable-dependency-tracking ac_cv_path_M4=m4 ac_cv_prog_TEST_EMACS=no&lt;/P&gt;&lt;P&gt;## --------- ##&lt;BR /&gt;## Platform. ##&lt;BR /&gt;## --------- ##&lt;/P&gt;&lt;P&gt;hostname = volta18&lt;BR /&gt;uname -m = x86_64&lt;BR /&gt;uname -r = 5.0.0-31-generic&lt;BR /&gt;uname -s = Linux&lt;BR /&gt;uname -v = #33~18.04.1-Ubuntu SMP Tue Oct 1 10:20:39 UTC 2019&lt;/P&gt;&lt;P&gt;/usr/bin/uname -p = unknown&lt;BR /&gt;/bin/uname -X = unknown&lt;/P&gt;&lt;P&gt;/bin/arch = unknown&lt;BR /&gt;/usr/bin/arch -k = unknown&lt;BR /&gt;/usr/convex/getsysinfo = unknown&lt;BR /&gt;/usr/bin/hostinfo = unknown&lt;BR /&gt;/bin/machine = unknown&lt;BR /&gt;/usr/bin/oslevel = unknown&lt;BR /&gt;/bin/universe = unknown&lt;/P&gt;&lt;P&gt;PATH: /export/users/bgoetz/var-fsl-yocto/sources/poky/scripts/native-intercept&lt;BR /&gt;PATH: /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/bin/texinfo-dummy-native&lt;BR /&gt;PATH: /export/users/bgoetz/var-fsl-yocto/sources/poky/scripts&lt;BR /&gt;PATH: /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/bin/x86_64-linux&lt;BR /&gt;PATH: /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/bin&lt;BR /&gt;PATH: /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/sbin&lt;BR /&gt;PATH: /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/bin&lt;BR /&gt;PATH: /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/sbin&lt;BR /&gt;PATH: /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/bin&lt;BR /&gt;PATH: /export/users/bgoetz/var-fsl-yocto/sources/poky/bitbake/bin&lt;BR /&gt;PATH: /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/hosttools&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;## ----------- ##&lt;BR /&gt;## Core tests. ##&lt;BR /&gt;## ----------- ##&lt;/P&gt;&lt;P&gt;configure:1796: checking for a BSD-compatible install&lt;BR /&gt;configure:1864: result: /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/hosttools/install -c&lt;BR /&gt;configure:1875: checking whether build environment is sane&lt;BR /&gt;configure:1925: result: yes&lt;BR /&gt;configure:2066: checking for a thread-safe mkdir -p&lt;BR /&gt;configure:2105: result: /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/hosttools/mkdir -p&lt;BR /&gt;configure:2118: checking for gawk&lt;BR /&gt;configure:2134: found /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/hosttools/gawk&lt;BR /&gt;configure:2145: result: gawk&lt;BR /&gt;configure:2156: checking whether make sets $(MAKE)&lt;BR /&gt;configure:2178: result: yes&lt;BR /&gt;&lt;STRONG&gt;configure:2261: error: cannot run /bin/bash ../autoconf-2.69/build-aux/config.sub&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;## ---------------- ##&lt;BR /&gt;## Cache variables. ##&lt;BR /&gt;## ---------------- ##&lt;/P&gt;&lt;P&gt;ac_cv_env_EMACSLOADPATH_set=&lt;BR /&gt;ac_cv_env_EMACSLOADPATH_value=&lt;BR /&gt;ac_cv_env_EMACS_set=&lt;BR /&gt;ac_cv_env_EMACS_value=&lt;BR /&gt;ac_cv_env_M4_set=&lt;BR /&gt;ac_cv_env_M4_value=&lt;BR /&gt;ac_cv_env_build_alias_set=set&lt;BR /&gt;ac_cv_env_build_alias_value=x86_64-linux&lt;BR /&gt;ac_cv_env_host_alias_set=set&lt;BR /&gt;ac_cv_env_host_alias_value=x86_64-linux&lt;BR /&gt;ac_cv_env_target_alias_set=set&lt;BR /&gt;ac_cv_env_target_alias_value=x86_64-linux&lt;BR /&gt;ac_cv_path_M4=m4&lt;BR /&gt;ac_cv_path_PERL='/usr/bin/env perl'&lt;BR /&gt;ac_cv_path_install='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/hosttools/install -c'&lt;BR /&gt;ac_cv_path_mkdir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/hosttools/mkdir&lt;BR /&gt;ac_cv_prog_AWK=gawk&lt;BR /&gt;ac_cv_prog_TEST_EMACS=no&lt;BR /&gt;ac_cv_prog_make_make_set=yes&lt;BR /&gt;lt_cv_sys_lib_dlsearch_path_spec='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/lib /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/lib /lib /lib64 /usr/lib /usr/lib64'&lt;/P&gt;&lt;P&gt;## ----------------- ##&lt;BR /&gt;## Output variables. ##&lt;BR /&gt;## ----------------- ##&lt;/P&gt;&lt;P&gt;ACLOCAL='${SHELL} /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/missing --run aclocal-1.11'&lt;BR /&gt;AMTAR='${SHELL} /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/missing --run tar'&lt;BR /&gt;AUTOCONF='${SHELL} /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/missing --run autoconf'&lt;BR /&gt;AUTOHEADER='${SHELL} /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/missing --run autoheader'&lt;BR /&gt;AUTOMAKE='${SHELL} /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/missing --run automake-1.11'&lt;BR /&gt;AWK='gawk'&lt;BR /&gt;CYGPATH_W='echo'&lt;BR /&gt;DEFS=''&lt;BR /&gt;ECHO_C=''&lt;BR /&gt;ECHO_N='-n'&lt;BR /&gt;ECHO_T=''&lt;BR /&gt;EGREP=''&lt;BR /&gt;EMACS=''&lt;BR /&gt;EMACSLOADPATH=''&lt;BR /&gt;EXPR=''&lt;BR /&gt;GREP=''&lt;BR /&gt;HELP2MAN=''&lt;BR /&gt;INSTALL_DATA='${INSTALL} -m 644'&lt;BR /&gt;INSTALL_PROGRAM='${INSTALL}'&lt;BR /&gt;INSTALL_SCRIPT='${INSTALL}'&lt;BR /&gt;INSTALL_STRIP_PROGRAM='$(install_sh) -c -s'&lt;BR /&gt;LIBOBJS=''&lt;BR /&gt;LIBS=''&lt;BR /&gt;LTLIBOBJS=''&lt;BR /&gt;M4=''&lt;BR /&gt;M4_DEBUGFILE=''&lt;BR /&gt;M4_GNU=''&lt;BR /&gt;&lt;STRONG&gt;MAKEINFO='${SHELL} /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/missing --run makeinfo'&lt;/STRONG&gt;&lt;BR /&gt;MAKE_CASE_SENSITIVE_FALSE=''&lt;BR /&gt;MAKE_CASE_SENSITIVE_TRUE=''&lt;BR /&gt;MKDIR_P='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/hosttools/mkdir -p'&lt;BR /&gt;PACKAGE='autoconf'&lt;BR /&gt;PACKAGE_BUGREPORT='bug-autoconf@gnu.org'&lt;BR /&gt;PACKAGE_NAME='GNU Autoconf'&lt;BR /&gt;PACKAGE_STRING='GNU Autoconf 2.69'&lt;BR /&gt;PACKAGE_TARNAME='autoconf'&lt;BR /&gt;PACKAGE_URL='http://www.gnu.org/software/autoconf/'&lt;BR /&gt;PACKAGE_VERSION='2.69'&lt;BR /&gt;PATH_SEPARATOR=':'&lt;BR /&gt;PERL=''&lt;BR /&gt;PERL_FLOCK=''&lt;BR /&gt;SED=''&lt;BR /&gt;SET_MAKE=''&lt;BR /&gt;SHELL='/bin/bash'&lt;BR /&gt;STRIP='strip'&lt;BR /&gt;TEST_EMACS=''&lt;BR /&gt;VERSION='2.69'&lt;BR /&gt;ac_cv_dir_trailing_space=''&lt;BR /&gt;ac_cv_sh_n_works=''&lt;BR /&gt;ac_cv_unsupported_fs_chars=''&lt;BR /&gt;am__isrc=' -I$(srcdir)'&lt;BR /&gt;am__leading_dot='.'&lt;BR /&gt;am__tar='${AMTAR} chof - "$$tardir"'&lt;BR /&gt;am__untar='${AMTAR} xf -'&lt;BR /&gt;bindir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/bin'&lt;BR /&gt;build='x86_64-linux'&lt;BR /&gt;build_alias='x86_64-linux'&lt;BR /&gt;build_cpu=''&lt;BR /&gt;build_os=''&lt;BR /&gt;build_vendor=''&lt;BR /&gt;datadir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/share'&lt;BR /&gt;datarootdir='${prefix}/share'&lt;BR /&gt;docdir='${datarootdir}/doc/${PACKAGE_TARNAME}'&lt;BR /&gt;dvidir='${docdir}'&lt;BR /&gt;exec_prefix='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr'&lt;BR /&gt;host='x86_64-linux'&lt;BR /&gt;host_alias='x86_64-linux'&lt;BR /&gt;host_cpu=''&lt;BR /&gt;host_os=''&lt;BR /&gt;host_vendor=''&lt;BR /&gt;htmldir='${docdir}'&lt;BR /&gt;includedir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/include'&lt;BR /&gt;infodir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/share/info'&lt;BR /&gt;install_sh='${SHELL} /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/install-sh'&lt;BR /&gt;libdir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/lib'&lt;BR /&gt;libexecdir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/libexec'&lt;BR /&gt;lispdir=''&lt;BR /&gt;localedir='${datarootdir}/locale'&lt;BR /&gt;localstatedir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/var'&lt;BR /&gt;mandir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/share/man'&lt;BR /&gt;mkdir_p='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/hosttools/mkdir -p'&lt;BR /&gt;oldincludedir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/include'&lt;BR /&gt;pdfdir='${docdir}'&lt;BR /&gt;prefix='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr'&lt;BR /&gt;program_transform_name='s,x,x,'&lt;BR /&gt;psdir='${docdir}'&lt;BR /&gt;sbindir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/sbin'&lt;BR /&gt;sharedstatedir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/com'&lt;BR /&gt;sysconfdir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/etc'&lt;BR /&gt;target_alias='x86_64-linux'&lt;/P&gt;&lt;P&gt;## ----------- ##&lt;BR /&gt;## confdefs.h. ##&lt;BR /&gt;## ----------- ##&lt;/P&gt;&lt;P&gt;/* confdefs.h */&lt;BR /&gt;#define PACKAGE_NAME "GNU Autoconf"&lt;BR /&gt;#define PACKAGE_TARNAME "autoconf"&lt;BR /&gt;#define PACKAGE_VERSION "2.69"&lt;BR /&gt;#define PACKAGE_STRING "GNU Autoconf 2.69"&lt;BR /&gt;#define PACKAGE_BUGREPORT "bug-autoconf@gnu.org"&lt;BR /&gt;#define PACKAGE_URL "http://www.gnu.org/software/autoconf/"&lt;BR /&gt;#define PACKAGE "autoconf"&lt;BR /&gt;#define VERSION "2.69"&lt;/P&gt;&lt;P&gt;configure: exit 2&lt;BR /&gt;bgoetz@volta18:~/unix$&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Oct 2019 00:49:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bitbake-fsl-image-gui-errors-out-on-do-configure/m-p/924891#M138947</guid>
      <dc:creator>bgoetz</dc:creator>
      <dc:date>2019-10-16T00:49:48Z</dc:date>
    </item>
    <item>
      <title>Re: bitbake fsl-image-gui errors out on do_configure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-fsl-image-gui-errors-out-on-do-configure/m-p/924892#M138948</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Bill Goetz,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that you are using the Variscite yocto BSP. I would recommend not changing anything from the default setup and try baking the fsl-image-gui first jus to make sure that the default setup is working correctly. Then work on your changes. There is a lot of useful information and forums on the Yocto Project side.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Oct 2019 17:05:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bitbake-fsl-image-gui-errors-out-on-do-configure/m-p/924892#M138948</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2019-10-17T17:05:37Z</dc:date>
    </item>
    <item>
      <title>Re: bitbake fsl-image-gui errors out on do_configure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bitbake-fsl-image-gui-errors-out-on-do-configure/m-p/924893#M138949</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, yes, thanks for the reply!&lt;/P&gt;&lt;P&gt;I’m working with the Variscite guys to get a build.&lt;/P&gt;&lt;P&gt;Thanks again!&lt;/P&gt;&lt;P&gt;Bill&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Oct 2019 22:44:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bitbake-fsl-image-gui-errors-out-on-do-configure/m-p/924893#M138949</guid>
      <dc:creator>bgoetz</dc:creator>
      <dc:date>2019-10-17T22:44:40Z</dc:date>
    </item>
  </channel>
</rss>