<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic I.MX6Q parallel camera input freeze (Oreo 8) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6Q-parallel-camera-input-freeze-Oreo-8/m-p/924448#M138899</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we're working on a board built around a Variscite Dart-Mx6q.&lt;/P&gt;&lt;P&gt;The board has an Analog Device ADV7181C to perform cvbs acquisition.&lt;/P&gt;&lt;P&gt;All works fine but if the analog input is switched to an empty one (no camera connected) the bt.656 video data stream&amp;nbsp; to imx6 parallel port stops and the camera application freeze.&lt;/P&gt;&lt;P&gt;The only way to get all working again is reboot the board.&lt;/P&gt;&lt;P&gt;Is there any workaround?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you, kind regards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Luca&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Sep 2019 09:22:19 GMT</pubDate>
    <dc:creator>l_bruni</dc:creator>
    <dc:date>2019-09-13T09:22:19Z</dc:date>
    <item>
      <title>I.MX6Q parallel camera input freeze (Oreo 8)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6Q-parallel-camera-input-freeze-Oreo-8/m-p/924448#M138899</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we're working on a board built around a Variscite Dart-Mx6q.&lt;/P&gt;&lt;P&gt;The board has an Analog Device ADV7181C to perform cvbs acquisition.&lt;/P&gt;&lt;P&gt;All works fine but if the analog input is switched to an empty one (no camera connected) the bt.656 video data stream&amp;nbsp; to imx6 parallel port stops and the camera application freeze.&lt;/P&gt;&lt;P&gt;The only way to get all working again is reboot the board.&lt;/P&gt;&lt;P&gt;Is there any workaround?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you, kind regards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Luca&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Sep 2019 09:22:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6Q-parallel-camera-input-freeze-Oreo-8/m-p/924448#M138899</guid>
      <dc:creator>l_bruni</dc:creator>
      <dc:date>2019-09-13T09:22:19Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6Q parallel camera input freeze (Oreo 8)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6Q-parallel-camera-input-freeze-Oreo-8/m-p/924449#M138900</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Luca&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;unfortunately I am not aware workaround for such case, probably one can add&lt;/P&gt;&lt;P&gt;some code to application which would exit when there are no several incoming camera frames.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Sep 2019 23:17:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6Q-parallel-camera-input-freeze-Oreo-8/m-p/924449#M138900</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-09-13T23:17:49Z</dc:date>
    </item>
  </channel>
</rss>