<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: camera interface performance? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/camera-interface-performance/m-p/923504#M138790</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello k,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One can use parallel CSI Interface,you can connect up to 4 cameras to the MIPI. for this you have to either use a MIPI CSI-2 hub or multiplexed the four streams in and FPGA.&lt;/P&gt;&lt;P&gt;The Parallel camera is limited to 10bits per camera.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Jul 2019 15:16:29 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2019-07-09T15:16:29Z</dc:date>
    <item>
      <title>camera interface performance?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/camera-interface-performance/m-p/923503#M138789</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;I want to know the performance difference between IMX6 parallel camera interface and MIPI interface.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;SPAN lang="en"&gt;Is there any comparison data such as parallel maximum operation speed and mipi maximum operation speed?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;SPAN lang="en"&gt;Is there a difference in gstreamer processing speed between when the camera input is parallel and when it is mipi?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;camera input ~ HDMI output.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;or&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;camera input ~ streaming output.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;regards!&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV&gt;&lt;DIV class=""&gt;&lt;DIV&gt;&lt;DIV class=""&gt;&lt;DIV&gt;&lt;DIV data-ved="0ahUKEwjnw-Dkr5PjAhUD6bwKHW7_CfwQGggq"&gt;&lt;DIV data-async-context="query:%EB%B2%88%EC%97%AD"&gt;&lt;DIV&gt;&lt;DIV class=""&gt;&lt;DIV class="" data-hveid="CAoQAA" data-md="77" data-ved="2ahUKEwjnw-Dkr5PjAhUD6bwKHW7_CfwQkCkwAHoECAoQAA"&gt;&lt;DIV data-hveid="CAoQAQ"&gt;&lt;DIV class="" data-cp="1" data-nnttsvi="1" data-nttsd="1" data-sm="1" data-sugg="1" data-sugg-time="500" data-sugg-url="https://clients1.google.com/complete/search" data-uilc="ko" data-ulf="1"&gt;&lt;DIV class=""&gt;&lt;DIV class="" data-rtid="izgMfccd_zc8"&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Jul 2019 09:16:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/camera-interface-performance/m-p/923503#M138789</guid>
      <dc:creator>kangmw086</dc:creator>
      <dc:date>2019-07-01T09:16:04Z</dc:date>
    </item>
    <item>
      <title>Re: camera interface performance?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/camera-interface-performance/m-p/923504#M138790</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello k,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One can use parallel CSI Interface,you can connect up to 4 cameras to the MIPI. for this you have to either use a MIPI CSI-2 hub or multiplexed the four streams in and FPGA.&lt;/P&gt;&lt;P&gt;The Parallel camera is limited to 10bits per camera.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jul 2019 15:16:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/camera-interface-performance/m-p/923504#M138790</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2019-07-09T15:16:29Z</dc:date>
    </item>
  </channel>
</rss>