<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic I.MX6 Parallel Video Capture Freeze on Oreo 8 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-Parallel-Video-Capture-Freeze-on-Oreo-8/m-p/922491#M138695</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we're working on a custom board built around a Variscite DART MX6Q.&lt;/P&gt;&lt;P&gt;On our carrier board we've an Analog Device ADV7280A used to capture and display an analog video source.&lt;/P&gt;&lt;P&gt;The ADV7280A has four input channel and we can switch between them writing commands through i2cset (there's a daemon with root privileges receiving commands from our Android Java application).&lt;/P&gt;&lt;P&gt;All is working fine but if we switch to a disconnected analog channel (or the camera connected is off) the camera display section of the application stop working and there's no way to get the video to stream again until&amp;nbsp;system reboot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way to reset the parallel video capture from Java application (or with a linux c program that can be launched through our daemon?)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you, kind regards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Luca&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Sep 2019 11:57:35 GMT</pubDate>
    <dc:creator>l_bruni</dc:creator>
    <dc:date>2019-09-13T11:57:35Z</dc:date>
    <item>
      <title>I.MX6 Parallel Video Capture Freeze on Oreo 8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-Parallel-Video-Capture-Freeze-on-Oreo-8/m-p/922491#M138695</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we're working on a custom board built around a Variscite DART MX6Q.&lt;/P&gt;&lt;P&gt;On our carrier board we've an Analog Device ADV7280A used to capture and display an analog video source.&lt;/P&gt;&lt;P&gt;The ADV7280A has four input channel and we can switch between them writing commands through i2cset (there's a daemon with root privileges receiving commands from our Android Java application).&lt;/P&gt;&lt;P&gt;All is working fine but if we switch to a disconnected analog channel (or the camera connected is off) the camera display section of the application stop working and there's no way to get the video to stream again until&amp;nbsp;system reboot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way to reset the parallel video capture from Java application (or with a linux c program that can be launched through our daemon?)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you, kind regards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Luca&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Sep 2019 11:57:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-Parallel-Video-Capture-Freeze-on-Oreo-8/m-p/922491#M138695</guid>
      <dc:creator>l_bruni</dc:creator>
      <dc:date>2019-09-13T11:57:35Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6 Parallel Video Capture Freeze on Oreo 8</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-Parallel-Video-Capture-Freeze-on-Oreo-8/m-p/922492#M138696</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;Is there a way to reset the parallel video capture from Java application (or with a linux c program that can be launched through our daemon?)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;---Java:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; please look into android SDK on camera operations, which should provide STREAM_ON &amp;amp; STREAM OFF interface.&lt;/P&gt;&lt;P&gt;---Linux C&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Use V4L2 API to do stream off / on operations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope abvoe information is helpful for you .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have&amp;nbsp; a nice day!&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Sep 2019 07:26:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-Parallel-Video-Capture-Freeze-on-Oreo-8/m-p/922492#M138696</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2019-09-17T07:26:18Z</dc:date>
    </item>
  </channel>
</rss>