<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Linux DTB compilation failed - imx6ull in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Linux-DTB-compilation-failed-imx6ull/m-p/920332#M138403</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Pankaj Joshi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did Kunal’s suggestions worked? These are a good starting point if you are not making changes to the BSP Release.&lt;/P&gt;&lt;P&gt;If you are porting or editing the device tree it would be good to make sure that the required files can be located, for example in this case the iomux_snvs include.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Sep 2019 14:47:39 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2019-09-17T14:47:39Z</dc:date>
    <item>
      <title>Linux DTB compilation failed - imx6ull</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-DTB-compilation-failed-imx6ull/m-p/920330#M138401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;While I do the Linux build using Yocto for imx6ull, I get the following error while Device Tree is built.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Error: /home/lem/kernel_silex_migration/tb-lem-release/linux-fslc/arch/arm/boot/dts/mackinac.dts:477.1-13 Label or path iomuxc_snvs not found&lt;BR /&gt;| FATAL ERROR: Syntax error parsing input tree&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However the same Label is present in old Linux kernel and building fine. Is it because of DTC version? Any pointer is helpful.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Sep 2019 12:40:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-DTB-compilation-failed-imx6ull/m-p/920330#M138401</guid>
      <dc:creator>pankajjoshi</dc:creator>
      <dc:date>2019-09-12T12:40:25Z</dc:date>
    </item>
    <item>
      <title>Re: Linux DTB compilation failed - imx6ull</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-DTB-compilation-failed-imx6ull/m-p/920331#M138402</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/pankajjoshi"&gt;pankajjoshi&lt;/A&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please follow "i.MX Yocto Project User's Guide" to compile various components. To compile device tree for linux you can&amp;nbsp;use below two commands:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;bitbake -c compile linux-imx -f&lt;/LI&gt;&lt;LI&gt;bitbake -c deploy linux-imx&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please&amp;nbsp;download&amp;nbsp;the&amp;nbsp;&lt;SPAN&gt;"i.MX Yocto Project User's Guide" from this &lt;A href="https://www.nxp.com/design/i.mx-developer-resources/i.mx-software-and-development-tool:IMX-SW"&gt;link&lt;/A&gt;.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kunal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Sep 2019 07:18:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-DTB-compilation-failed-imx6ull/m-p/920331#M138402</guid>
      <dc:creator>kunalkotecha1</dc:creator>
      <dc:date>2019-09-17T07:18:24Z</dc:date>
    </item>
    <item>
      <title>Re: Linux DTB compilation failed - imx6ull</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-DTB-compilation-failed-imx6ull/m-p/920332#M138403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Pankaj Joshi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did Kunal’s suggestions worked? These are a good starting point if you are not making changes to the BSP Release.&lt;/P&gt;&lt;P&gt;If you are porting or editing the device tree it would be good to make sure that the required files can be located, for example in this case the iomux_snvs include.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Sep 2019 14:47:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-DTB-compilation-failed-imx6ull/m-p/920332#M138403</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2019-09-17T14:47:39Z</dc:date>
    </item>
  </channel>
</rss>