<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using DMA in imx6ul SPI client driver in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-DMA-in-imx6ul-SPI-client-driver/m-p/920305#M138395</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right, there &lt;SPAN&gt;is no&amp;nbsp;extra configuration needed other than calling standard SPI API&lt;/SPAN&gt;s.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Jun 2019 23:18:28 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-06-14T23:18:28Z</dc:date>
    <item>
      <title>Using DMA in imx6ul SPI client driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-DMA-in-imx6ul-SPI-client-driver/m-p/920304#M138394</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to &lt;A href="https://lore.kernel.org/patchwork/patch/498739/"&gt;this&lt;/A&gt; link, it seems that&amp;nbsp;DMA support can be enabled by setting "dma-names" in dts. Also referring to &lt;A _jive_internal="true" href="https://community.nxp.com/thread/467622"&gt;this &lt;/A&gt;thread and checking it, the&amp;nbsp;DMA related driver code is also integrated in spi-imx.c.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am writing a driver for a SPI SRAM device and&amp;nbsp;am using the 23k256 driver (&lt;SPAN&gt;/drivers/mtd/devices/&lt;/SPAN&gt;&lt;SPAN&gt;mchp23k256.c)&amp;nbsp;as reference. It seems to me that the IMX SPI controller driver is already handling the DMA mappings and requests, and there is no&amp;nbsp;extra configuration needed other than calling standard SPI API as illustrated in the 23k256 driver?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2019 10:36:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-DMA-in-imx6ul-SPI-client-driver/m-p/920304#M138394</guid>
      <dc:creator>uuwen</dc:creator>
      <dc:date>2019-06-13T10:36:57Z</dc:date>
    </item>
    <item>
      <title>Re: Using DMA in imx6ul SPI client driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-DMA-in-imx6ul-SPI-client-driver/m-p/920305#M138395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right, there &lt;SPAN&gt;is no&amp;nbsp;extra configuration needed other than calling standard SPI API&lt;/SPAN&gt;s.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jun 2019 23:18:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-DMA-in-imx6ul-SPI-client-driver/m-p/920305#M138395</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-06-14T23:18:28Z</dc:date>
    </item>
  </channel>
</rss>