<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic QSpi boot mode,  channel 'B' in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/QSpi-boot-mode-channel-B/m-p/920217#M138381</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello &lt;BR /&gt;i am making the acquaintance with MCIMX6SX-SDB kit.&lt;BR /&gt;investigating QSPI boot configuration&lt;/P&gt;&lt;P&gt;i have seen booting from QSPI2 ('A' channel, there is the 32M flash, address 0x70000000),&lt;BR /&gt;likewise QSPI2 channel 'B', there is the 32M flash, address 0x78000000, same.&lt;BR /&gt;My question is:&lt;BR /&gt;is there oportunity to boot from channel 'B' of QSPI2?&lt;BR /&gt;May i place qspi header at address 0x78000400 and&lt;/P&gt;&lt;P&gt;would it acceptable for "boot ROM" or i must use channel 'A' only.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Jul 2019 12:46:48 GMT</pubDate>
    <dc:creator>o_scherbinin</dc:creator>
    <dc:date>2019-07-15T12:46:48Z</dc:date>
    <item>
      <title>QSpi boot mode,  channel 'B'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QSpi-boot-mode-channel-B/m-p/920217#M138381</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello &lt;BR /&gt;i am making the acquaintance with MCIMX6SX-SDB kit.&lt;BR /&gt;investigating QSPI boot configuration&lt;/P&gt;&lt;P&gt;i have seen booting from QSPI2 ('A' channel, there is the 32M flash, address 0x70000000),&lt;BR /&gt;likewise QSPI2 channel 'B', there is the 32M flash, address 0x78000000, same.&lt;BR /&gt;My question is:&lt;BR /&gt;is there oportunity to boot from channel 'B' of QSPI2?&lt;BR /&gt;May i place qspi header at address 0x78000400 and&lt;/P&gt;&lt;P&gt;would it acceptable for "boot ROM" or i must use channel 'A' only.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jul 2019 12:46:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QSpi-boot-mode-channel-B/m-p/920217#M138381</guid>
      <dc:creator>o_scherbinin</dc:creator>
      <dc:date>2019-07-15T12:46:48Z</dc:date>
    </item>
    <item>
      <title>Re: QSpi boot mode,  channel 'B'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/QSpi-boot-mode-channel-B/m-p/920218#M138382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Oleg&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems QSPI 'A' channel is always needed as described in sect.8.6.3 QuadSPI configuration parameters:&lt;/P&gt;&lt;P&gt;The QuadSPI Configuration Parameters Table is built in the boot image at a fixed offset&lt;BR /&gt;of 0x400 from the QSPI NOR A1 base address &lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX6SXRM" target="_blank"&gt;&lt;STRONG&gt;i.MX 6SoloX Applications Processor Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jul 2019 23:18:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/QSpi-boot-mode-channel-B/m-p/920218#M138382</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-07-15T23:18:53Z</dc:date>
    </item>
  </channel>
</rss>