<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Can Serial Downloader be triggered from uboot/userspace?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-Serial-Downloader-be-triggered-from-uboot-userspace/m-p/919585#M138296</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;FYI: fastboot can be used to override say emmc boot and instead jump into the serial-downloader mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Nov 2019 01:03:10 GMT</pubDate>
    <dc:creator>dav1</dc:creator>
    <dc:date>2019-11-21T01:03:10Z</dc:date>
    <item>
      <title>Can Serial Downloader be triggered from uboot/userspace?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-Serial-Downloader-be-triggered-from-uboot-userspace/m-p/919581#M138292</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it possible (on the i.mx8 mini) to override the BOOT_MODE pins (via code/register write) to enable the&amp;nbsp;Serial Downloader (without having to physically change the boot-pins)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Aug 2019 09:44:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-Serial-Downloader-be-triggered-from-uboot-userspace/m-p/919581#M138292</guid>
      <dc:creator>dav1</dc:creator>
      <dc:date>2019-08-29T09:44:07Z</dc:date>
    </item>
    <item>
      <title>Re: Can Serial Downloader be triggered from uboot/userspace?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-Serial-Downloader-be-triggered-from-uboot-userspace/m-p/919582#M138293</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, it is not possible to override the BOOT_MODE[1:0] settings in software without physically switching the BOOT_MODE[1:0] pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Aug 2019 08:45:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-Serial-Downloader-be-triggered-from-uboot-userspace/m-p/919582#M138293</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2019-08-30T08:45:34Z</dc:date>
    </item>
    <item>
      <title>Re: Can Serial Downloader be triggered from uboot/userspace?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-Serial-Downloader-be-triggered-from-uboot-userspace/m-p/919583#M138294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV style="color: #000000; font-size: 12px;"&gt;&lt;/DIV&gt;&lt;P&gt;Hi Artur,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;iMX7's&amp;nbsp;u-boot's bmode usb command writes to gpr9 and gpr10 (general purpose registers). The same register on&amp;nbsp;the imx8m mini's reference manual states these are "reserved for internal use"...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please check with the i.mx8 team if these still exists but are not documented.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Sep 2019 13:24:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-Serial-Downloader-be-triggered-from-uboot-userspace/m-p/919583#M138294</guid>
      <dc:creator>dav1</dc:creator>
      <dc:date>2019-09-04T13:24:29Z</dc:date>
    </item>
    <item>
      <title>Re: Can Serial Downloader be triggered from uboot/userspace?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-Serial-Downloader-be-triggered-from-uboot-userspace/m-p/919584#M138295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The R&amp;amp;D have confirmed that there is no way to override the boot mode settings in software.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Sep 2019 11:28:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-Serial-Downloader-be-triggered-from-uboot-userspace/m-p/919584#M138295</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2019-09-12T11:28:36Z</dc:date>
    </item>
    <item>
      <title>Re: Can Serial Downloader be triggered from uboot/userspace?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-Serial-Downloader-be-triggered-from-uboot-userspace/m-p/919585#M138296</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;FYI: fastboot can be used to override say emmc boot and instead jump into the serial-downloader mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Nov 2019 01:03:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-Serial-Downloader-be-triggered-from-uboot-userspace/m-p/919585#M138296</guid>
      <dc:creator>dav1</dc:creator>
      <dc:date>2019-11-21T01:03:10Z</dc:date>
    </item>
  </channel>
</rss>