<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックUse boot0 and boot1 for primary and secondary bootloader</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Use-boot0-and-boot1-for-primary-and-secondary-bootloader/m-p/919327#M138276</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On IMX7, that has an eMMC with 2 boot blocks/physical partitions, boot0 and boot1, would it be possible to use one or the other as a redundant bootloader?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to flash primary bootloader on boot0 and secondary bootloader on boot1. Both images are signed and verified by HAB. Verified as in I signed/flashed either images individually and made sure the board boots with either image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For my use case I would like that if the primary bootloader gets corrupted, the ROM/HAB should validate the secondary bootloader and boot from there. Is this possible?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have read about the primary and secondary bootloader being flashed on the same boot partition with secondary image table but I really dont want the two bootloader images to reside on the same block. I would like to have it working the way I described above. Please let me know if that is do able?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 May 2019 21:06:45 GMT</pubDate>
    <dc:creator>praveen_bharath</dc:creator>
    <dc:date>2019-05-28T21:06:45Z</dc:date>
    <item>
      <title>Use boot0 and boot1 for primary and secondary bootloader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Use-boot0-and-boot1-for-primary-and-secondary-bootloader/m-p/919327#M138276</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On IMX7, that has an eMMC with 2 boot blocks/physical partitions, boot0 and boot1, would it be possible to use one or the other as a redundant bootloader?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to flash primary bootloader on boot0 and secondary bootloader on boot1. Both images are signed and verified by HAB. Verified as in I signed/flashed either images individually and made sure the board boots with either image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For my use case I would like that if the primary bootloader gets corrupted, the ROM/HAB should validate the secondary bootloader and boot from there. Is this possible?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have read about the primary and secondary bootloader being flashed on the same boot partition with secondary image table but I really dont want the two bootloader images to reside on the same block. I would like to have it working the way I described above. Please let me know if that is do able?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2019 21:06:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Use-boot0-and-boot1-for-primary-and-secondary-bootloader/m-p/919327#M138276</guid>
      <dc:creator>praveen_bharath</dc:creator>
      <dc:date>2019-05-28T21:06:45Z</dc:date>
    </item>
    <item>
      <title>Re: Use boot0 and boot1 for primary and secondary bootloader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Use-boot0-and-boot1-for-primary-and-secondary-bootloader/m-p/919328#M138277</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp; The boot scenario to use the eMMC second boot partition&amp;nbsp; is not supported by i.MX boot ROM,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;at least, directly. Nevertheless, customers can apply the approach, described in section&amp;nbsp;6.6.5.3.5 &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;(Redundant boot support for expansion device) of the i.MX7D RM, assuming that the secondary&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;bootloader, run by the boot ROM, can program properly BOOT_PARTITION_ENABLE field in the &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Ext_CSD[179] and try to reboot the system. Note, "the boot partition can be selected for an MMC4.x &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;card after the card initialization is complete. The ROM code reads the BOOT_PARTITION_ENABLE &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;field in the Ext_CSD[179] to get the boot partition to be set."&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;-------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Note:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 May 2019 08:55:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Use-boot0-and-boot1-for-primary-and-secondary-bootloader/m-p/919328#M138277</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2019-05-29T08:55:31Z</dc:date>
    </item>
  </channel>
</rss>